Frequently Asked Questions (FAQs)
Summary
The Electrical Length of the 16454A has been preset to the E4991A as 0 mm.
Question
What is the Electrical Length Value Defined for the 16454A?
Answer
The electrical length of the 16454A has been preset to the E4991A as 0 mm. Though the 16454A has a low electrical length value for its coaxial connector part, it is less significant error factor than other (major) error sources and is included in the specified measurement uncertainty. Thus, the electrical length is deemed to be 0 mm.
See Also
16454A operation and service guide