Column Control DTX

Medalist VTEP v2.0 Powered!

Flyers

Keysight Technologies, Inc. Medalist VTEP v2.0 Powered! is a comprehensive suite of test tools designed to tackle today’s test challenges.

Technological advances are putting tremendous pressures on manufacturing test. Nearly every segment of the electronics industry is affected by these trends:

  • Shrinking geometries
  • Diminishing test access
  • Increasing PCBA density

High Speed Signal Propagation (HSSP) The VTEP v2.0 Powered! test suite comprises:

  1.  The original VTEP engine – with 4X better sensitivity and 5X better standard deviation
  2.  iVTEP – for testing ultra-small packages (e.g micro-BGAs, lip-chips)
  3.  Network parameter measurement – for testing power and ground pins (essential for HSSP)
  4.  Cover-Extend – The latest addition to the test suite which targets limited-access PCBAs

What is Cover-Extend technology?

Cover-Extend technology is a hybrid between VTEP and boundary scan. It draws the best from what each technology offers and enhances the overall capability of Keysight in-circuit test systems. Here are the key contributions of the constituent technologies:

 VTEP

Simple, robust and fast measurement using VTEP sensors.

Boundary scan

A world-wide standardized test methodology (IEEE 1149.x standard). Limited-access capability – ability to control the I/O functions of individual pins through the use of only four pins of the test access port (refer to Figure 1 overleaf).

Key benefits of Cover-Extend

  •  Test coverage without test access
  • Lower cost of test
  • Improved board quality

Test coverage without test access

Cover-Extend protects your investment in ICT as well as opens up opportunities for access-limited users who have not traditionally considered ICT as part of test strategy to do so now.

Lower cost of test

 With lesser need for physical test access*, there comes significant savings on operational cost like fixturing and ICT test resources. For instance, you can now save on cost of test probes and associated cost like wiring and maintenance. Also, you can minimize your need for ICT pin cards required to test your PCBAs

 How does it work?

The VTEP sensor, which is able to capacitively pick up stimulus signals, is placed on the component to be tested (e.g. a connector).

Traditional VTEP methodology required physical test access (i.e test probes) to deliver this stimulus signal. However, with Cover-Extend, the stimulus signal is delivered via a boundary scan device.

The boundary scan device does not require test probes on every pin.

As per the IEEE 1149.x standard, using only the test access port, users can deliver the necessary stimulus signal to the connector.

A defect (e.g. an open) on the path between the boundary scan device and the VTEP sensor will affect the stimulus signal that is bound for the sensor.

The result is captured and diagnosed by the ICT system and thus, the defect is detected!
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
By clicking the button, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you.

A sales representative will contact you soon.

Column Control DTX