Agilent Technologies
 

Agilent Modular Products VEE Pro 8.5 Customized Menu



 

Table of contents

  1. Revision version
  2. System Requirements
  3. Installing the software
  4. What's New?
  5. Uninstall the software
  6. License Agreement
  7. Product Support


   

1. Revision Version


This Agilent USB Modular Products Reference CD-ROM contains the following installer version.

Agilent Modular Products VEE Pro 8.5 Customized Menu 1.2.0.0
Hardware Driver U2300A/U2802A/U2700A - A.2007.11.05
IVI-COM Driver U2300A/U2800A - 2.0.12.0

top



   

2. System Requirements


Prior to installing the Agilent Modular Products VEE Pro 8.5 Customized Menu software, the PC system needs to meet the following minimum requirements.

Hardware Requirements
Processor 1.6 GHz Pentium IV or higher
Operating system One of the following Microsoft Windows versions:
• Windows XP Professional or Home Edition, Service Pack 1 or later
• Windows 2000 Professional, Service Pack 4 or later
Hard disk space 1 GB
RAM 512 MB or higher recommended
Video Super VGA (800 x 600) 256 colors or more


Software Requirements
Agilent IO Libraries Suite Version 15.0 or above
Agilent VEE Pro Version 8.5

top



   

3. Installing the Software


The following describes the installation procedure of Agilent Modular Products VEE Pro 8.5 Customized Menu.
  1. Verify that your PC meets the minimum requirements as stated in System Requirements. Close all applications on your PC and insert the Product Reference CD-ROM into your CD- ROM drive.
  2. Click Explore Folder on the Agilent Modular Products Installation Menu and goto Utilities > Agilent Modular Products VEE Pro 8.5 Customized Menu, then double click on AgDAQVEEMenu<version>.exe where <version> is the software version.
  3. If the installation menu does not appear after a few seconds, select Start > Run (on the Windows Start menu) and type <drive>:Utilities > Agilent Modular Products VEE Pro 8.5 Customized Menu > AgDAQVEEMenu<version>.exe, where <drive> is your CD- ROM drive and <version> is the software version. Click OK to begin installation.
  4. InstallShield Wizard dialog box will show prerequisite software if your PC does not have IVI-COM Driver installed.
  5. Click OK to begin prerequisite installation. Installer will guide you through the steps.
  6. Once prerequisite installation is done,the installation of Agilent Modular Products VEE Pro 8.5 Customized Menu will proceed. Click Next to begin.
  7. Read the License Agreement and select I accept the terms in the License Agreement to accept the agreement. You may click Print to print out the Agilent License Terms for reference. Click Next to proceed.
  8. Click Install to begin the installation.
  9. Click Finish when the installation is completed.

NOTE
USING THE LICENSED MATERIALS INDICATES YOUR ACCEPTANCE OF THE LICENSE TERMS. IF YOU DO NOT AGREE TO ALL OF THESE TERMS, YOU MAY RETURN ANY UNOPENED LICENSED MATERIALS FOR A FULL REFUND. IF THE LICENSED MATERIALS ARE BUNDLED OR PRE-LOADED WITH ANOTHER PRODUCT, YOU MAY RETURN THE ENTIRE UNUSED PRODUCT FOR A FULL REFUND.

top



   

4. What's New?


Listed below are new features in this release:

  1. U2300A Quick Start Sample Program:
    DIO - Output Digital Data
    Counter - Counter Measurements
    Counter - Totalizer
  2. U2802A Quick Start Sample Program
  3. Release version 1.2 is added into the "What is This Menu?"

top



   

5. Uninstall the Software


The following describes the uninstallation procedure of Agilent Modular Products VEE Pro 8.5 Customized Menu.

  1. Go to Start > Settings > Control Panel and the Control Panel window will appear.
  2. Double-click Add or Remove Programs, the Add or Remove Programs window will appear with the list of currently installed programs.
  3. Select Agilent Modular Products VEE Pro 8.5 Customized Menu and click Remove.
  4. Click Yes to uninstall the software.

Note
Ensure that you have saved your data and work, and close all Agilent VEE Pro version 8.5 application before uninstalling the program.

top



   

6. License Agreement


AGILENT LICENSE TERMS The following License Terms govern your use of the Licensed Materials unless you have a separate written agreement with Agilent, in which case, that written agreement will control and take precedence.

License Grant. Agilent grants you a non-exclusive license to use one copy of the Licensed Materials. With respect to the software portion of the Licensed Materials, “use” means to install, store, display, execute and use the software on the computer or device, or on the class or series of equipment, for which you have paid the corresponding license fee. If no fee is required, you may use the software on one computer or device. If the software is licensed for concurrent or network use, you may not allow more than the maximum number of authorized users to access and use the software concurrently.

License Restrictions. You may make copies or adaptations of the Licensed Materials only for archival purposes or only when copying or adaptation is an essential step in the authorized use of the Licensed Materials. You must reproduce all copyright notices in the original Licensed Materials on all permitted copies or adaptations. Except as provided here, you may not copy, modify or translate the Licensed Materials or disable any of its features. You may not copy the Licensed Materials onto any public or distributed network or service bureau. In addition, you may not lease, rent or sublicense the Licensed Materials without Agilent's prior written consent.

Upgrades. This license does not entitle you to receive upgrades, updates or technical support. Such services may be purchased separately. If the Licensed Materials include an upgrade to previously licensed material, your license in that material automatically terminates and you should destroy the previous content and any copies or adaptations.

Ownership. The Licensed Materials are owned and copyrighted by Agilent or its third party suppliers. Your license confers no title to, or ownership in, the Licensed Materials and is not a sale of any rights in the Licensed Materials. Agilent's third party suppliers may protect their rights in the event of any violation of these License Terms.

No Disassembly. You may not disassemble or decompile the Licensed Materials unless you obtain Agilent's prior written consent. In some jurisdictions, Agilent's consent may not be required for limited disassembly or decompilation. Upon request, you will provide Agilent with reasonably detailed information regarding any such permitted disassembly or decompilation.

High Risk Activities. The Licensed Materials are not specifically designed, manufactured or intended for use in the planning, construction, maintenance or direct operation of a nuclear facility, nor for use in on-line control or fail safe operation of aircraft navigation, control or communication systems, weapon systems or direct life support systems.

Transfer. You may transfer the license granted to you here provided that you deliver all the Licensed Materials to the transferee along with these License Terms. The transferee must accept these License Terms as a condition to any transfer. Your license to use the Licensed Materials will terminate upon transfer.

Termination. Agilent may terminate your license upon notice for failure to comply with any of these License Terms. Upon termination, you must immediately destroy the Licensed Materials, together with all copies, adaptations and merged portions in any form.

Export Requirements. The Licensed Materials may be subject to export control laws, including the U.S. Export Administration Regulations and other export laws and regulations of other countries. You may not export or re-export the Licensed Materials or any copy or adaptation in violation of any applicable laws or regulations. You certify that you are not on the U.S. Department of Commerce’s Denied Persons List, the U.S. Department of Treasury’s Specially Designated Nationals list or other government list prohibiting you from receiving the Licensed Materials.

U.S. Government Restricted Rights. If the Licensed Materials are licensed for use in the performance of a U.S. Government prime contract or subcontract, you agree that they have been developed entirely at private expense. You further agree that they are licensed as "commercial computer software" as defined in DFARS 252.227 7014 (Jun 1995), as a "commercial item" as defined in FAR 2.101(a), or as "Restricted computer software" as defined in FAR 52.227 19 (Jun 1987) (or any equivalent agency regulation or contract clause), whichever is applicable. You agree that you acquire only those rights provided for such Licensed Materials by the applicable FAR or DFARS clause or the Agilent standard license agreement for the product involved. Contractor/Manufacturer is Agilent Technologies, Inc, 395 Page Mill Road, Palo Alto, California 94306.

top



   

7. Product Support


For more information on the products for Agilent Modular Products VEE Pro 8.5 Customized Menu, please visit:

Agilent U2300A Series USB Multifunction Data Acquisition http://www.agilent.com/find/U2300A
Agilent U2802A 31-channel Thermocouple Input Module http://www.agilent.com/find/U2802A


For more information on other related product, visit:

Agilent U2700A Series Modular Instrument Chassis: http://www.agilent.com/find/U2700A
A list of contact information is available on: http://www.agilent.com/find/assist

Microsoft, Windows, MS Windows, and Windows NT are U.S. registered trademarks of Microsoft Corporation.

top



© Copyright Agilent Technologies, Inc. 2006-2008