Choose a country or area to see content specific to your location
Data Sheets
Keysight E5250A
Low Leakage Switch Mainframe
Introduction
The Keysight E5250A low-leakage switch mainframe expands a single measurement station, such as the Keysight B1500A, E5270B, 4155C, or 4156C, to an automated measurement system. Plug-in modules can be configured either as a cross-point matrix for general parametric measurements or as a multiplexer for long-term reliability measurements.
When configured as a 10 x 12 Matrix Switch, the E5250A is ideal for general IV-CV parametric measurements with up to x48 triaxial output configurations.
Because of its 384 channel capability and advanced features that are typically found only on larger, more expensive input devices, the E5250A is ideal for long-term reliability measurements when configured as a 24 (8 x 3) Channel Multiplexer. This enables the use of low-cost power supplies for consistent stressing.
A large number of channels and low-cost stress sources allow the parallel testing of hundreds of devices, saving cost and time and achieving accurate, consistent results.
Unlock Content
Sign up for free
*Indicates required field
Thank you.
Your form has been successfully submitted.
Note: Clearing your browser cache will reset your access. To regain access to the content, simply sign up again.
×
Please have a salesperson contact me.
*Indicates required field
Thank you.
A sales representative will contact you soon.