On the ENA 6 series, can I run a VBA program which is made on the ENA 7 series?
(SUPPORTED MODELS IN BOLD: E5071C E5072A E5070B/71B E5070A/71A E5061A/62A E5061B E5063A E5091A E5092A)
A VBA project for the ENA 7 series doesn't work on the ENA 6 series as is. However, the program is likely to work with only small modifications by "exporting" modules separately from ENA 7 series then "import" them into ENA 6 series, as long as a program doesn't use functions which are not available for ENA 6 series.