Windows login process appears on my ENA every time after power up. Can I skip this?
(SUPPORTED MODELS IN BOLD: E5071C E5070B/71B E5070A/71A E5061A/62A E5061B E5072A)
In default setting, windows login process does not appear and go directly to the NA application after power up.
Required conditions for this are:
- Use welcome screen for login. (default = use welcome screen)
- Only one user account is registered to windows. (default = only "agena" is registered)
- ENA is not attending to a domain. (default = Member of workgroup)
- Password is not active for the account. (default = no password)
Login process will appear if more than one of above setting is changed by user. If such user still requires bypassing windows login process, use windows auto login function:
- Click Start, click Run, and type "control userpasswords2".
- Uncheck the "Users must enter a username and password to use this computer" check box.
- Click Apply.
- Enter the user name and password you wish automatically log on with, and then click OK.
- Click OK again.