When I save a Touchstone file with the ENA / ENA-L, which calculation will be reflected in the Touchstone file?
(SUPPORTED MODELS IN BOLD: E5071C E5070B/71B E5070A/71A E5061A/62A E5061B E5072A)
On save touchstone function, all calculations are reflected in the saved file for Single-Ended calculation (Calibration, Port Extension, Embedding/De-Embedding, Port Reference Impedance Conversion, Matching Circuit Embedding). However, regardless of on/off state, the calculation which includes mixed-mode conversion (Balance-Unbalance conversion, Differential/Common Port Reference Impedance Conversion, Differential Matching Circuit Embedding) is NOT reflected in the Touchstone file.
Same applies to the "save touchstone VBA".