Can the U2300A/U2500A Series Data Acquisition (DAQ) devices that are used with three modular chassis be synchronized?
Yes, the U2300A/U2500A Series Data Acquisition (DAQ) devices that are used with three modular chassis can be synchronized by connecting a reliable 10MHz clock source to these chassis. The connection is made to the 10MHz Reference BNC connector found at the back panel of the chassis. However, the Measurement Manager (AMM) can only connect to one chassis at a time. Controlling multiple chassis can be done in different programming languages through the drivers provided.