For U2300A/U2500A Series Data Acquisition (DAQ) devices, can the Measurement Manager (AMM) display in units other than voltage (v)?
Yes, the Measurement Manager (AMM) can display in units other than voltage (v). The AMM has a feature called the scaling editor which allows you to put in the required scaling and select the engineering units (EUs) for each channel. You can choose to measure in various EUs for current, temperature, vibration and pressure. If the required EU is not displayed in the drop-down list, you can just type the exact format into the editor.