What's new in Command Expert 1.2?
Feature | Description |
---|---|
Additional Supported Enviroments |
Now Supports Windows 8, Visual Studio 2012, MATLAB R2012b and R2013a, and Keysight SystemVue 2013.07 and above. |
Local Variables | Local Variables are like Parameters, but are internal to a Command Expert sequence. They allow you to store the output of one command and use it as the input into another. Example Screenshot |
Running Sequences in .NET Languages | Similar to agRunSequence for MATLAB, you can now play a Command Expert sequence in Visual Studio with a few commands. |
IO Monitor Instrument Simulation |
You can play a sequence using an IO Monitor log capture to simulate real measurement results. |
Copy and Paste |
You can now copy and paste steps between Command Expert sequences. |
Integration with Keysight Connection Expert | In the New Instrument dialog box, you can now easily add instruments that have already been configured in Keysight Connection Expert. Example Screenshot |
No More Auto Connection Delays |
Opening a Command Expert sequence no longer connects automatically to instruments. The connection is now made when the sequence is run. |
Additional LabVIEW Support |
LabVIEW sequence blocks can now use 13 input and 13 output parameter pins instead of the previous limitation of 6 input and 6 output parameter pins. You can now use multiple instruments in one sequence block |
Last Modified: May 3rd, 2013