您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

1-25 / 320

排序:
Signal & Spectrum Analyzer Benchtop/Modular/Handheld Firmware Update Center
To access the most recent version of firmware or software for signal and spectrum analyzer - benchtop and handheld models.

FAQ 2019-10-30

What is Keysight's Windows 7 to Windows 10 Migration Schedule?
We are beginning the transition of our Windows based instruments from Windows Embedded Standard 7 to Windows 10 IoT Enterprise. Click on the link for additional information.

FAQ 2019-08-28

M8000 系列軟體 30 天免費試用授權
M8000 產品系列適用的軟體之試用授權頁面與連結。

FAQ 2019-05-21

FieldFox Manuals, Firmware, Software and Product Support
Manuals, firmware upgrade, software trials & upgrade and support page for FieldFox analyzers

FAQ 2018-11-14

What software and options do I need to access the FPGA sandbox in my high-speed digitizer?
Digitizer option FDK enables programming access to the on-board FPGA. Click on the question for additional information.

FAQ 2018-01-18

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced TDD?
The X-Series upgrade path to LTE-Advanced TDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

Can the PNA-X be configured to install Windows updates as they are pushed out by Microsoft?
Yes, any Windows based machine can be configured to install Windows updates.

FAQ 2017-06-28

Does the noise figure application on the PNA-X (option 029) provide a full noise-parameter system (tuners and software)?
No, we don’t provide a full noise-parameter system. Click on the question for additional information.

FAQ 2017-06-28

Is there a software application for the 8714ES to calculate K factor?
No, there is not a software application to calculate K factor for the 8714ES.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced FDD?
The X-Series upgrade path to LTE-Advanced FDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

Can antivirus programs run on the Windows based PNA-X?
Yes, antivirus programs can run on any Windows based machine.

FAQ 2017-06-28

Is there a software application for the E5062A to calculate K factor?
No, there is not a software application to calculate K factor for the E5062A.

FAQ 2017-06-28

Is calibration included in the 86100DU-WN7 Windows 7 upgrade?
86100DU-WN7 is a return to service center upgrade and does include calibration, in addition to a certificate of calibration and data.

FAQ 2017-06-28

What is the difference of software options between M9485A and PNA/ENA series VNA?
There is no difference for option 007/009/010. There are some differences for options 025, 028, 086 and 551.

FAQ 2017-05-25

FieldFox 有沒有 GPS 接收器?
從 A.05.33 版本韌體開始,FieldFox 分析儀便已添加了 GPS 功能。

FAQ 2017-01-23

30-Day Free Trial for X-Series Measurement Applications for X-Series Modular Instruments
30-day trial license available for the X-Series measurement applications for X-Series modular signal analyzers.

FAQ 2016-06-09

Why 34405A can't be detected in Windows 7?
There are two posibilities causing 34405A couldn't be detected. 1. IO Libraries Suit 15.1 or below...

FAQ 2015-09-21

How to enable 34410A/34411A/L4411A browser web control work in Java 8?
To enable browser web control to work in Java 8, update instrument to firmware version 2.41...

FAQ 2015-09-21

Microsoft 不再支援 Windows XP 對我的 ENA 有何影響?
Microsoft 於 2014 年 4 月 8 日停止對 Windows XP 作業系統的支援。請閱讀此頁面以了解我們對此問題的解答。

FAQ 2015-07-27

Can I recover the E7515A operating system if it fails to start correctly?
Yes, E7515A has an Instrument Image Recovery mode. Click on the question above for a fuller description.

FAQ 2015-05-15

M9290A CXA-m PXIe 信號分析儀是否支援掃描模式以進行頻譜分析?
是,M9290A 支援掃描模式和 FFT 模式,以進行信號的頻譜分析。

FAQ 2014-12-29

適用於具傳統 UI 之 X 系列信號分析儀的量測應用軟體,30 天免費試用
X 系列信號分析儀量測應用軟體提供 30 天免費試用授權。

FAQ 2014-12-19

Is U2700A series USB Modular Instruments supported in Linux environment?
No. U2700A Series are not supportable in Linux environment. The drives for USB Modular only build for Microsoft Windows.

FAQ 2014-11-25

How does the Microsoft end of support for Windows XP affect my M9036A?
In Keysight’s ongoing efforts and commitment to provide the best possible product quality and improve the overall customer experience with our M9036A PXIe Embedded Controller, we would like to inform you that we have made the conscious decision to not migrate the XP version of the M9036A to Windows 7.

FAQ 2014-10-12

X 系列信號分析儀軟體更新
X 系列信號分析儀 (PXA/MXA/EXA/CXA) 軟體更新

FAQ 2014-08-14

1 2 3 4 5 6 7 8 9 10 ... 下一頁