検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

テクニカルサポート

電子計測

製品番号で検索:

26-50 / 72

並べ替え
What do the N7620B upgrade licenses cost?
All N7620B license upgrades are free.

FAQ 2012-10-28

Do I have to upgrade my N7620A licenses?
You may want to upgrade your N7620A licenses to N7620B licenses so that they can be managed using the Keysight License Manager.

FAQ 2012-10-28

How do I install my N7620B licenses?
All N7620B licenses are managed with the Keysight License Manager.

FAQ 2012-10-28

Will the N7620B software recognize my N7620A licenses?
The N7620B software recognizes all N7620A licenses except for the N8241A, N6030A, and N9330A external Arbs.

FAQ 2012-10-28

How do I manage my N7620A licenses?
The N7620A software allows you to view your original N7620A licenses.

FAQ 2012-10-28

I have the basic functionality license for N7620A and I want to get the advanced capability license. What should I do?
Install the N7620B software and get the N7620B-QFP, or N7620B-QTP advanced capability license

FAQ 2012-10-28

How do I upgrade my N7620A licenses?
Contact the customer contact center at Keysight Technologies.

FAQ 2012-10-28

Where can I find Keysight EEsof EDA License Server (FLEXnet) Licensing Software?
On the Keysight EEsof EDA License Server software download page at: http://www.keysight.com/find/eesof-flexnet-downloads

FAQ 2012-10-23

Why doesn't the Keysight License Manager connect to my ESG?
Your ESG needs firmware revision C.04.84 or above...

FAQ 2012-03-02

How do I register for the Keysight EEsof EDA Knowledge Center?
The Knowledge Center is an enhancement to our existing site that provides additional documents and examples. Registration is required.

FAQ 2011-11-08

ENAソフトウェア・オプションの試用ライセンスはありますか?
モデルによって異なります。

FAQ 2011-10-16

Why is my N1918A Power Analyzer USB dongle key not detected by Windows7 64bit OS.
You need to upgrade the sentinel USB system(dongle key) driver to support Windows7 64bit OS.

FAQ 2011-09-12

For waveform 5-pack licenses, can a customer purchase a perpetual or time-based Signal Studio license for one MXG/ESG to evaluate waveforms, and th...
Yes, any licensed MXG/ESG can be used to evaluate the waveforms – not just the MXG/ESG with the waveform 5-pack license option.

FAQ 2010-09-24

What are the Signal Studio License options and configurations for the MXG?

FAQ 2010-09-20

For waveform 5-pack licenses, is there any protection against accidentally overwriting a licensed waveform?
No, we recommend keeping a copy of the licensed waveform for archival purposes.

FAQ 2010-09-19

グラフィカル測定アプリケーション (GMA) N4017Aソフトウェアのライセンスをインストールするにはどうすれば良いでしょうか?
http:///find/softwarelicenseでN4017Aの権利証明書を回復する場合は、ソフトウェアをN4010Aテスト・セットにロックするかPCにロックするかを決める必要があります。

FAQ 2010-09-15

For waveform 5-pack licenses, since a waveform can be copied and renamed, is there protection from a user inadvertently licensing the same signal?
Yes, there is protection against using a license slot on a redundant signal. A unique identifier is associated and stored with each signal created by Signal Studio applications. It is this identifier that is licensed on the MXG or ESG signal gen...

FAQ 2010-09-08

For waveform 5-pack licenses, is there a grace-period where I can still revoke/replace a waveform once it has been licensed?
Once the waveform is licensed, that license is permanent and cannot be revoked or replaced.

FAQ 2010-09-08

For waveform 5-pack licenses, can a customer generate a waveform in Signal Studio software not connected to a MXG/ESG, export to a location on thei...
Yes, this method can be used when customers only want to tweak waveform parameters and not evaluate RF performance beforehand.

FAQ 2010-09-08

For waveform 5-pack licenses, once a waveform is licensed, can it be copied and stored for archival purposes?
Yes, a licensed waveform can be copied and renamed for archival purposes. Be aware that the waveform can still only played on the ESG or MXG to which it has been licensed.

FAQ 2010-09-08

For waveform 5-pack licenses, can the 30-day license attached to each waveform 5-pack license be activated whenever the customer wants –or– do the ...
The 30-day license for the evaluation of waveforms (Option D01) may be activated at anytime, although they must be used one at a time.

FAQ 2010-09-08

For waveform 5-pack licenses, is there a way to have password protection against licensing a 5-pack waveform to prevent someone from inadvertently ...
No, this will be considered as an enhancement request for future releases.

FAQ 2010-09-08

How is a Signal Studio application license installed?
A Signal Studio license is installed using the License Manager software utility available for download and on the CD shipped with the Signal Studio software.

FAQ 2010-09-08

Why do the error messages "1105: Could not connect to License Server. Please restart application" and "1003: Failed to connect …
The error messages appear when the N1918A Power Analysis Manager is launched because the Keysight License Service sometimes does not start….

FAQ 2010-08-09

What should I do when my Power Analyzer (software licensing version) still goes into trial version even though a valid license was installed…
When this situation happens, try the following steps to get this resolved:

FAQ 2010-08-09

前へ 1 2 3 次へ