이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

1-25 / 219

정렬방식:
What Information Should I Collect From FlexDCA Before Asking Keysight For Help?
What Information Should I Collect From FlexDCA Before Asking Keysight For Help?

FAQ 2018-12-10

FieldFox Manuals, Firmware, Software and Product Support
Manuals, firmware upgrade, software trials & upgrade and support page for FieldFox analyzers

FAQ 2018-11-14

지원하기 위해 N4373A LCA를 보낼떄 포함되어야 하는 것은 무엇입니까?
네트워크 분석기, 광 테스트 세트 및 모든 RF 케이블을 포함시켜야합니다.

FAQ 2017-10-31

Is 4338B Adjustment Program still available?
The 4338B adjustment program (04338-65005) that could be found in 4338B Service Manual no longer available…

FAQ 2017-09-26

How to measure output frequency of E4981A Capacitance Meter?
To measure the output frequency of E4981A Capacitance Meter, interface box (Keysight part number: 04294-61002) is required…

FAQ 2017-09-20

What is the service (repair/calibration) support strategy?
The service (repair/calibration) support strategy of the M9485A is the module level. Only defective module can be returned, if it needs repair.

FAQ 2017-05-25

How can I send the modules of M9485A to Keysight?
A recommended procedure to return to Keysight is to remove all cables and send the modules independently. Sending all modules with chassis is an optional.

FAQ 2017-05-25

What is the part number of connector saver for the M9376A, M9378A/B?
The connector saver is an adapter of coaxial straight male-SMA female-SMA on the test port of the M9376A, M9378A/B. This adapter can be replaced easily if the connecter is broken or is worn down.

FAQ 2017-05-24

16008B의 전도성 고무(엘라스토머)의 상태가 나빠졌을 때 교체 할 수 있습니까?
아니요, 전도성 고무(엘라스토머)는 16008B의 주 전극 조립체에서 제거 할 수 없기 때문에 전체 주 전극 조립체를 새 것으로 교체하십시오.

FAQ 2016-12-11

What is the username and password for the E44xxB ESG-A/D?
E44xxB ESG-A/D Service Support Software username and password .

FAQ 2016-07-04

U200xB 파워센서의 감쇠기는 왜 본체에서 분해할 수 없습니까?
U200xB USB 파워센서는 센서 전체에서 50MHz의 기본 보정 작업을 한다.

FAQ 2016-02-17

어떻게 손상으로 부터 파워센서를 보호 할 수 있습니까?
손상으로 부터 파워센서를(예, E4412A, E4413A, N8481A, N8482A, N8485A, U2000B, U2000H, U2001B, U2001H, U2002H 등.)방지하기 위해, 참고하면...

FAQ 2014-09-11

What is the performance test procedure of 4349A?
See the documentation.

FAQ 2014-09-03

PDF PDF 3.71 MB
Why is the Upgrade Assistant not able to detect my instrument?
Upgrade Assistanet가 활성화되지 않으면 Socket SCPI가 ON 되어 있는지 확인하십시오.

FAQ 2014-08-25

E5061A/ E5062A 소스 출력 전력 레벨의 저하 현상을 해결하려면 어떻게 해야 합니까?
소스 출력 전력 레벨 보정(Source Output Power Level Correction) 소프트웨어를 실행해 E5061A/ E5062A의 소스 출력 전력 레벨을 보정하십시오.

FAQ 2014-04-28

교정 키트 토크 렌치를 위한 인증(및 재인증) 프로세스는 무엇입니까?

FAQ 2014-03-24

How can the memory in a 438A Power Meter be erased for security purposes?
This can be done by a sequence of keypresses, or by a sequence of remote commands.

FAQ 2013-11-22

Why does handheld scope’s date/time display disappears or shows hexa characters?
This condition indicates that the internal memory battery level is low.

FAQ 2013-11-22

Are rules execution sequences arrange able? If yes, how to do it?
Yes, expand the Device Navigation tree of the particular device types, select one of the rule, click "Up" or "Down" key to move the rule to your desired location. For example: Moving "Agilent_fi" rule to before "Agilent_Swap_S&I" of the resistor devices.

FAQ 2013-10-16

What calibrations are available on X-Series, PSA, ESA analyzers and X-Series, ESG-C, PSG Signal Generators at time of initial sale from the factory?
Details regarding time of sale calibrations can be found here...

FAQ 2013-10-15

Replacement of Control XTP, Module Control Card
Frequently Asked Questions about XTPA Module Control Card

FAQ 2013-06-11

Can I order the replacement part of 16089E's clips?
When the clip is faulty, please proceed to place a new order on 16089E or purchase the spare Kelvin Clip Leads.

FAQ 2013-03-17

Sample “testplan” for Utility card & FR3070A
Sample “testplan” for Utility card & FR3070A from manufacturing site

FAQ 2013-02-18

Can I use external mixing (Option EXM) with real-time?
Yes, you can use external mixing with real-time. The instrument software must A.14.54 or later.

FAQ 2013-02-07

Can I use noise floor extension (NFE) with real-time?
No, you cannot use noise floor extension with real-time.

FAQ 2013-02-07

1 2 3 4 5 6 7 8 9 다음