Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

126-150 of 332

Sort:
What is the difference between E4438C options 001, 002, 601 and 602?
ARB memory depth, waveform segment and availaiblity of digital I/O port vary.

FAQ 2012-06-07

Are there any known issues when downgrading the VSA firmware?
When downgrading firmware on the E4406A there is an issue with the firmware upgrade program. You must first completely uninstall any previous installation of the upgrade program before installing an older version.

FAQ 2012-05-29

How do I upgrade the E4406A VSA Series 321.4 MHz IF Output Option 300?
This option can be upgraded at your local Keysight Service Center. (Click on this FAQ for more information)

FAQ 2012-05-28

How many options can be loaded into my E4406A with A.06.03 firmware at one time?
With a 48 MB flash memory board, you can fit up to seven measurement personalities. To determine what will fit, add up the memory sizes of the personalities that you want. If the total is less than 19,225 kB then they will fit.

FAQ 2012-05-28

How do I upgrade the E4406A VSA Series Firmware and Measurement Personalities?
The E4406A firmware and measurement personalites can be upgraded via the LAN or crossover cable. (Click on this FAQ for more information)

FAQ 2012-05-28

How do I upgrade the E4406A VSA Series Base Band I/Q Inputs Option B7C?
This option can be upgraded at your local Keysight Service Center. (Click on this FAQ for more information)

FAQ 2012-05-28

How can I upgrade my PSA Series Spectrum Analyzer to add Gated Sweep (Time gating)?
A hardware retrofit will be required before gated sweep can be used in PSA's purchased before September 2003 (Serial Prefix less than US4336 or MY4336 ). Firmware Release A.04.12 or greater is also needed.

FAQ 2012-05-28

How do I upgrade the E4406A VSA Memory Upgrade Option ANE?
The memory for E4406A can be upgrade to 64MB with E4406AU Option ANE. (Click here for more details)

FAQ 2012-05-28

How do I upgrade the E4406A VSA Series iDEN Measurement Personality Option HN1?
This option can be upgraded via the LAN or crossover cable. (Click on this FAQ for more information)

FAQ 2012-05-28

How do I upgrade the E4406A VSA Series cdma2000® Measurement Personality (Option B78) and 1xEV-DV add-on (Option 214)?
This Option can be upgraded via the LAN or crossover cable. (Click on this FAQ for more information)

FAQ 2012-05-26

How do I upgrade the E4406A VSA Series NADC / PDC Measurement Personality Option BAE?
This Option can be upgraded via the LAN or crossover cable. (Click on this FAQ for more information)

FAQ 2012-05-26

How do I upgrade the E4406A VSA Series 1xEV-DO Measurement Personality Option 204?
This option can be upgraded via the LAN or crossover cable. (Click on this FAQ for more information)

FAQ 2012-05-26

How do I upgrade the E4406A VSA Series cdmaOne Measurement Personality Option BAC?
This option can be upgraded via the LAN or crossover cable. (Click on this FAQ for more information)

FAQ 2012-05-26

How do I upgrade the E4406A VSA Series W-CDMA Measurement Personality (option BAF) and HSDPA add-on (option 210)?
This option can be upgraded via the LAN or crossover cable. (Click on this FAQ for more information)

FAQ 2012-05-26

How do I upgrade the E4406A VSA Series GSM measurement personality Option BAH?
This option can be upgraded via the LAN or crossover cable. (Click on this FAQ for more information)

FAQ 2012-05-26

How do I upgrade the ESA or EMC instruments with upgrade Option 230, Web Remote Control Software?
This upgrade is installed via floppy disk using the instrument floppy disk drive.

FAQ 2012-03-16

What is the revision history for the 89601A, VSA software?
New feature list with each software release...

FAQ 2012-03-16

Why do I need to update firmware on the PSA/E4406A VSA for the GSM/EDGE option?
Because you can get the updated test limits to comply the latest 3GPP standards and more flexible test limit or limit mask settings in most measurements.

FAQ 2012-03-11

Do the handheld spectrum analyzers have a built-in GPS receiver?
Yes, the C Series have optional built-in GPS for GPS tagging. The N9340B HSA does not.

FAQ 2012-03-02

How do I update my N9320B firmware?
Please download firmware package from N9320B firmware & software webpage. Unzip the file and copy folder “N9320B” to root directory of a USB stick. Press [System/Preset]->{More 1 of 2}->{Upgrade}

FAQ 2012-03-02

Using Option INM, how many frames can be saved in one spectrogram file? Can the capacity for spectrum monitoring be increased?
The HSA spectrogram can only record 1500 frames in one file.

FAQ 2012-03-02

How do I install the task planner option on my handheld spectrum analyzer?
Refer to the Application Note: Streamlining Field Test with Task Planner

FAQ 2012-03-02

Why doesn't the Keysight License Manager connect to my ESG?
Your ESG needs firmware revision C.04.84 or above...

FAQ 2012-03-02

How do I upgrade my handheld spectrum analyzer?
Most of the upgrades to the HSA can be made by obtaining a license key and do not require hardware installation.

FAQ 2012-03-02

Do the handheld spectrum analyzers offer time-gated spectrum analysis?
The HSAs have an optional time-gated spectrum analysis feature that enables spectral information to be obtained about signals in the frequency domain (Option TMG).

FAQ 2012-03-01

Previous 1 2 3 4 5 6 7 8 9 10 ... Next