이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

상세 분류

주제별

산업/기술

분야별 검색결과

제품 카테고리별

151-175 / 8112

정렬방식:
When using the DIQ application, what happens when I set the internal receiver to measure beyond the frequency range of my instrument?
Data for frequencies beyond the instrument hardware limitations is extrapolated from the hardware’s maximum and minimum limits. Click on the question for additional information.

FAQ 2017-06-28

I want to use multiple 2-port M9371A PXIe VNAs in my system. Is option 551 necessary?
If the modules are used as independent 2-port VNAs, no; however, option 551 is necessary to perform true, calibrated, multiport measurements. Click on the question for additional information.

FAQ 2017-06-28

N9080B SEM measurement defaults seem to be different from 3GPP 36.141 V12.12.0 (2016-06). Is N9080B doing something it shouldn’t?
To make a “True RMS detection”, as requested by the 3GPP conformance testing, based on ITU-R SM.329, for a mix of noise-like & CW-like signals under test, use “Peak Detector with very narrow VBW”. Click on the question for additional information.

FAQ 2017-06-28

Where can I find information on E4980A/AL error messages?
E4980A/AL error messages are described in Appendix B of the Users Guide.

FAQ 2017-06-28

Is it possible to develop specific macros for E5061B to support TRL cal or the unknown thru method under a 9-term calibration method?
Yes, it is possible to perform a user developed 8-term calibration, like TRL, using an external program for the E5061B. Click on the question for additional information.

FAQ 2017-06-28

Can antivirus programs run on the Windows based PNA-X?
Yes, antivirus programs can run on any Windows based machine.

FAQ 2017-06-28

How do I create a Mono FM Signal using N5182B MXG ARB?
You can configure N7611B Signal Studio Broadcast Radio to play a mono/FM signal.

FAQ 2017-06-28

What is the difference between the Integrated true-mode stimulus application (opt 460) and the Differential and I/Q devices application (opt 089)?
The Integrated TMSA and the DIQ both simplify measurements of differential (balanced) devices. The two applications however, are used for different measurements. Click on the question for additional information.

FAQ 2017-06-28

Can the PNA-X support SSLT or SSST calibration techniques?
Yes; however, the Cal Kit must be defined properly to work. The Cal can be modified via Advanced Modify Cal Kit for Definitions under the Calibration menu.

FAQ 2017-06-28

What is the raw jitter tolerance for the N4960A/N4952A?
There is no CDR in the N4960A, so by itself, the JTOL plot will be a flat line somewhere below 1 UI. An external CDR can be used. Click on the question for additional information.

FAQ 2017-06-28

If we use external clocks for both the Pattern Generator and Error Detector parts, can we run them at different data rates?
It would be more straight-forward to provide the PG (TX) with a 10 GHz clock (for 10 Gb/s data) and then use the 1:4 demux and provide the ED (RX) with a 2.5 GHz clock (measuring 2.5 Gb/s data). Click on the question for additional information.

FAQ 2017-06-28

What is the time out limit of response time (2.4) in M8020A Interactive link training?
The LTSSM (Link Training and Status State Machine) implements the timeouts as specified in the PCIe specification. Click on the question for additional information.

FAQ 2017-06-28

최신 벤치 전원 공급기로 시간 절감
키사이트의 새로운 저비용 DC 벤치 전원 공급기는 4개의 독립적 출력 및 내장 데이터 로거가 있습니다. 최신 벤치 전원 공급기가 어떤 도움을 줄 수 있는지 확인하십시오.

FAQ 2017-06-20

5G로 가는 가장 빠른 경로 지원
설계 주기의 모든 단계를 포괄하는 5G 기술과 가용 5G 테스트 솔루션에 대해 자세히 알아보십시오.

FAQ 2017-06-16

How do you know the serial number and calibration date (Last Verification Date) of each module?
See “About NA” in the firmware or Use a tool to check the serial number and calibration date.

FAQ 2017-06-01

Is there any system level specification for the M9485A?
No, there is no system level specification.

FAQ 2017-05-25

How do I install the cables and adapter for the M9485A?
The installation procedure is shown in the M9485A Start Up Guide.

FAQ 2017-05-25

Which power meter is recommended for system power calibration?
U2000 Series USB Average Power Sensors or U8480 Series USB Thermocouple Power Sensors are recommended.

FAQ 2017-05-25

How can I send the modules of M9485A to Keysight?
A recommended procedure to return to Keysight is to remove all cables and send the modules independently. Sending all modules with chassis is an optional.

FAQ 2017-05-25

Which PXI chassis is recommended for M9485A?
M9018A/18B and M9019A are recommended.

FAQ 2017-05-25

What is the service (repair/calibration) support strategy?
The service (repair/calibration) support strategy of the M9485A is the module level. Only defective module can be returned, if it needs repair.

FAQ 2017-05-25

What is the difference of software options between M9485A and PNA/ENA series VNA?
There is no difference for option 007/009/010. There are some differences for options 025, 028, 086 and 551.

FAQ 2017-05-25

How many peripheral modules (M9379A, M9341A/B, M9161D, M9111A) are supported on M9485A?
M9485A supports one M9341A/B and up to 6 M9111A. There is no software limitation for M9379A and M9161D.

FAQ 2017-05-25

Can I use multiple M9485A with one controller?
Yes, but there are some limitations. Please refer to below.

FAQ 2017-05-25

How can I order custom configuration for M9485A?
You can order each module/accessory separately as you like. Please refer to below item list and startup guide for detail.

FAQ 2017-05-24

이전 1 2 3 4 5 6 7 8 9 10 ... 다음