技术支持
缩小范围
按主题
- 校准 (172)
- 配置和安装 (857)
- 显示信息和误差代码 (172)
- 许可 (72)
- 测量和仪器的基础知识 (217)
- 测量技术 (545)
- 操作系统和软件 (320)
- 操作和功能 (1160)
- 其它信息 (310)
- 部件和附件 (303)
- 打印和打印机 (35)
- 产品与固化软件更新及升级 (331)
- 产品操作原理 (282)
- 编程和数据传输 (513)
- 服务和维护 (219)
- 规范和精度 (347)
- 故障诊断 (134)
行业/技术
按内容类型
- FAQ (8121)
按产品类别
1-25 / 8121
Where can I find Signal Integrity, Power Integrity and EMC/EMI resources for high-speed digital designs?
Signal Integrity & Power Integrity Resources are available at http://www.keysight.com/find/eesof-ads-sipi-resources
FAQ 2019-11-15 |
|
How do I upgrade my N9040B UXA Signal Analyzer?
Find Information on Hardware Upgrades, Instrument Software and Measurement Applications, etc....
FAQ 2019-11-13 |
|
Is there a 3D model of the Infiniium 9000 Series oscilloscope?
Yes, see the Step format file download.
FAQ 2019-11-04 |
|
Signal & Spectrum Analyzer Benchtop/Modular/Handheld Firmware Update Center
To access the most recent version of firmware or software for signal and spectrum analyzer - benchtop and handheld models.
FAQ 2019-10-30 |
|
EMPro 许可证常见问题解答
解答关于 EMPro 许可证的常见问题。
FAQ 2019-10-28 |
|
BenchVue 软件是什么?
关于 BenchVue 软件的更多信息。
FAQ 2019-10-18 |
|
CBx_Data_Converter_Installer
M9203A/M9703B Streamed Data Conversion Utility
FAQ 2019-10-17 |
![]() |
What sets DMX apart from the applications that are built into the VNA already?
FAQ for DMX
FAQ 2019-10-16 |
|
What VNA models work with DMX?
FAQ for DMX
FAQ 2019-10-16 |
|
What problem is DMX trying to solve?
FAQ for DMX problem solving
FAQ 2019-10-16 |
|
关于许可证和下载的常见问题解答
关于 Keysight EEsof EDA 软件许可证和下载的常见问题解答
FAQ 2019-10-15 |
|
M980xA PXIe VNA Multi-Module Installation Guide
Y1730A is available as a cable kit. The installation procedure is described in documentation in the link.
FAQ 2019-10-10 |
![]() |
Which version of Visual Studio is working with TestExec SL?
Which version of Visual Studio will work with TestExec SL ?
FAQ 2019-10-08 |
|
What version of TS-5000 is working with TestExec SL?
Which version of TS-5000 will work with TestExec SL 8.1?
FAQ 2019-10-08 |
|
Does Test Exec SL software support backward compatibility?
Can Test Plan Created on TestExec SL 8.1 can run on TestExec SL 7.1?
FAQ 2019-10-08 |
|
How do I upgrade my N9030B PXA Signal Analyzer?
Find Information on Hardware Upgrades, Instrument Software and Measurement Applications, etc....
FAQ 2019-10-08 |
|
Why do OLED (Organic LED) displays dim over time?
OLED makes great contrast but its lifespan is highly dependent on user application: power on hours, contrasts settings, storage environment and operating environment.
FAQ 2019-09-25 |
|
Where do I download the mechanical drawings for M980xA PXI VNA
The M980xA comes with .step files that can be imported into your modelling application.
FAQ 2019-09-19 |
|
Where do I download the mechanical drawings for P50xxA PXI VNA
The P50xxA comes with .step files that can be imported into your modelling application.
FAQ 2019-09-19 |
|
是德科技软件许可证
是德科技软件节点锁定/固定、可转移、浮动/网络/企业级许可证为您提供灵活选择。无论您只是短期需要还是长年累月都需要软件,无论您是单一用户还是多个用户,选择是德科技许可证,一切尽在掌握!
FAQ 2019-09-16 |
|
探索最新版本的 IC-CAP 及其他信息
IC-CAP 特定产品版本信息列表
FAQ 2019-09-13 |
|
Where do I download the mechanical drawings for the M9506A?
Files can be imported into your modeling application.
FAQ 2019-09-10 |
|
Where can I find system requirements and supported platform information for GoldenGate?
For GoldenGate system requirements and supported platform information, refer to the Prerequisites section for your platform at http://www.keysight.comfind/eesof-goldengate-latest-downloads
FAQ 2019-09-06 |
|
RFPro EM Applications
RFPro EM Applications are provided below for RF Module, RFIC, MMIC, or RF Board design.
FAQ 2019-09-04 |
|
What is Keysight's Windows 7 to Windows 10 Migration Schedule?
We are beginning the transition of our Windows based instruments from Windows Embedded Standard 7 to Windows 10 IoT Enterprise. Click on the link for additional information.
FAQ 2019-08-28 |
|