Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

1-25 of 134

Sort:
Recognizing and Reducing Data Acquisition Switching Transients - White Paper
Low impedance sources can produce large and fast current transients when switching; creating problems with adjacent channels, transients in the ground circuit that upset digital logic connected to the DUT, or causing the switch unit to reset or hang. This application note describes several techniques to reduce these switching transients.

Application Note 2019-09-27

Automotive FMCW Analysis with U3851A RF Microwave Courseware
Frequency Modulated Continuous Wave (FMCW) is widely use automotive industry. In this document, we will discuss about FMCW simulation with SystemVue and real-world measurement with the prototyping kit.

Application Note 2019-07-16

PDF PDF 1.47 MB
Drive Down the Cost of Test Using the ENA Series Vector Network Analyzers - Application Note
Discussion of the contributions of the Keysight ENA series vector network analyzer to drive down the cost of test in production lines. Including an in depth analysis of the total cost of ownership.

Application Note 2019-06-04

PDF PDF 2.42 MB
Signal Integrity Analysis Series Part 1: Single-Port TDR, TDR/TDT, and 2-Port TDR - Application Note
This Application Note focuses on part 1: those which use a single-port TDR, those which use TDR/TDT, and those which use 2-port TDR.

Application Note 2019-04-25

Understanding the Fundamental Principles of Vector Network Analysis - Application Note 1287-1
This application note explores the fundamental principles of vector network analysis. The discussion includes the common parameters (S-parameters). RF fundamentals such as transmission lines and the Smith chart will also be reviewed.

Application Note 2019-04-04

Noise Figure Measurement Accuracy - The Y-Factor Method - Application Note
Specific to instruments that use the Y-factor method for noise figure measurements, this app note discusses measurement basics, avoidable errors, loss and temperature corrections, and uncertainties.

Application Note 2019-03-19

Power Handling Capability of Electromechanical Switches
This application note discusses the power handling of the hot switching and cold switching of EM switches.

Application Note 2019-02-13

USB 2.0 Compliance Testing with Infiniium Oscilloscopes - Application Note
This Application Note discusses the solution for the USB 2.0 test suite. The Keysight solution is the only one-box solution that uses the official USB-IF scripts for precompliance ans compliance testing.

Application Note 2019-01-29

Metrology-Grade Measurement Challenges - Application Note
This application note analyzes the sources that contribute to measurement uncertainties and summarizes how to achieve the most accurate measurement results with the Keysight N5531X.

Application Note 2018-12-20

PDF PDF 819 KB
Probe soldering guidelines for Keysight InfiniiMax probes - Application Note
There are various ways to connect test instrumentation probes to devices under test(DUTs). One such method is soldering, which provides a reliable connection and minimizes parasitic probing effects by keeping wire lengths and connections as short as possible. Many of Keysight's high performance oscilloscopes probes utilize soldered connections.

Application Note 2018-10-07

PDF PDF 7.73 MB
EMI Troubleshooting: The Need for Close Field Probes - Application Note
This application note introduces close field probes and explains how specific probes offer distinct advantages in electromagnetic compatibility (EMC) radiated emission pre-compliance test.

Application Note 2018-08-07

An Overview of the Electrical Validation of 10BASE-T, 100BASE-TX, and 1000BASE-T - Application Note
The technology used in these ports, commonly known as “LAN” or “NIC” ports, is usually one of the 10BASE-T, 100BASE-TX, and 1000BASE-T standards or a combination of them.

Application Note 2018-07-25

Probing a Midpoint of a Transmission Line that is Not Load Terminated - White Paper
With the advent of variable on die termination (i.e. ODT) many systems like low power double data rate memory (LPDDR) have the ability to either terminate a line in its characteristic impedance for high speed operation or terminate it with an open for lower speed operation. Many times there is a desire to probe the transmission line to monitor the signals on the line. When the transmission line is terminated in close to its characteristic impedance, the signals can be readily observed. However, if the line is terminated in an impedance that is not close to the characteristic impedance then it may not be possible to accurately measure the signals.

Application Note 2018-07-03

PDF PDF 1.98 MB
Bandwidth Boosting Techniques for the Infiniimax Probe Amp and Probe Head - Application Note
Keysight InfiniiMax differential probes are DSP corrected to have a flat magnitude and phase response to provide the highest possible accuracy. The bandwidth chosen to correct to is typically around 3dB non-corrected bandwidth. Usually, extending the bandwidth much beyond that point will increase the noise floor, and if pushed even further, can cause unrealistic noise artifacts. However, the N5381A/B solder-in probe head in combination with the InfiniiMax 1169A/B probe amp is an excellent candidate for extending the bandwidth beyond the 3dB point because the N5381A/B is peaked past the normal 12 GHz bandwidth, and the peaking of the probe head can help compensate for the roll-off of the probe amp bandwidth.

Application Note 2018-06-21

PDF PDF 4.96 MB
5 Common Mistakes People Make When Buying a Low-cost Oscilloscope – Application Note
Choosing the right oscilloscope can be a difficult task, especially with a small budget. Ensure you’re getting your money’s worth and avoid these 5 common mistakes when buying a low-cost oscilloscope.

Application Note 2018-06-06

Optimizing Dynamic Range for Distortion Measurements - Application Note
This application note covers high dynamic range measurement techniques for the new PSA Performance Spectrum Analyzer Series. The note describes the best way to use the PSA series to make distortion measurements such as ACP, intermodulation, and harmonic distortion.

Application Note 2018-03-12

PDF PDF 2.11 MB
Measuring Frequency Response with E5061B LF Network Analyzer
This application note describes fundamentals on low frequency network analysis by featuring the E5061B LF-RF network analyzer. Here we mainly discuss simple low frequency 2-port device measurements and associated topics.

Application Note 2018-02-22

Signal Analysis Measurement Fundamentals, Optimize Noise Floor, Resolution Bandwidth, and More
Learn measurement fundamentals to optimize your signal analysis for greater insights

Application Note 2017-12-13

Practical Temperature Measurements (AN-290)
This application note explores the more common temperature measurement techniques and introduces procedures for improving their accuracy.

Application Note 2017-12-13

The Application of Handheld Spectrum Analyzers in Interface Testing - Application Note

Application Note 2017-12-05

What is the difference between an equivalent time and a real-time oscilloscope? - Application Note
This document will discuss how each type of oscilloscope samples the incoming waveform and explain the trigger requirements.

Application Note 2017-12-05

Choosing the Best Passive and Active Oscilloscope Probes for Your Tasks - Application note
Selecting the right probe for your application is the first step toward making reliable oscilloscope measurements, and each probe has an application for which it performs best.

Application Note 2017-12-02

Demystifying RCRC and RC probes - Application Note
An ideal probe would provide an exact replica of a signal being probed. However, the probe becomes a part of the circuit under test, because the probe introduces probe loading to the circuit.

Application Note 2017-12-01

PDF PDF 1.27 MB
Optimizing RF and Microwave Spectrum Analyzer Dynamic Range - Application Note
This application note defines the elements of spectrum analyzer measurement speed and shows how to choose solution bandwidth and data output format for fast measurements.

Application Note 2017-12-01

Evaluating High-Resolution Oscilloscopes - Application Note
This application note talks about: . How scope ADC bits and bits of resolution differ . Relationship between vertical resolution and noise . How high-resolution mode works . Average mode

Application Note 2017-12-01

1 2 3 4 5 6 Next