Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

Refine the List

remove all refinements

By Topic

By Type of Content

By Product Category

1-25 of 38

Sort:
What is the dimension and connector location of each modules of the M9485A?

FAQ 2017-05-19

Do you have anti-aliasing filter for U2300A and U2500A ?
No, we do not have anti-aliasing filter for our DAQs

FAQ 2010-09-22

IO Libraries Suite: What interfaces and operating systems are supported?
View the Keysight IO Libraries Support matrices.

FAQ 2010-09-08

IO Libraries Suite: What are the differences between Keysight IO Libraries Suite versions 14.0 and 14.1?
The major enhancement that has been added to version 14.1 is compatibility with National Instruments NI-488.2 API or I/O Library.

FAQ 2010-09-08

What is the clock rate for Digital Inputs(DI) and Digital Outputs(DO) of U23xxA and U25xxA USB Data Acquisition?
The DAQ DIO is not meant to measure DI with clock rate precision or to control frequency of digital output

FAQ 2010-07-18

When will Keysight USB modular instruments and USB Modular DAQs supports Windows 7?
For 32 bit Windows 7, the supportability of modular instruments and DAQs will happen...

FAQ 2010-07-18

No Title
Instead of the ("Counter value"/"48 x 10^6") as the duration in seconds taken to count, it is...

FAQ 2010-05-10

Is number of bits the only factor to look at if I'm measuring at very low voltage say 5mVpp?
No it is not. Often times, you will have to look at the Gain Error and Offset Error as well as...

FAQ 2010-05-10

Is the USB connection of U2300A,U2500A and U2600A optically coupled?
No. It is not.

FAQ 2010-03-22

What does ENOB of 13.3 bit means in the specification sheet?
ENOB = (SINAD-1.76)/6.02 Overall Accuracy = ENOB (Effective Number of Bits)....

FAQ 2009-12-15

How do I know what is the best sampling rate to use for my measurement?
Typically if you follow Nyquist theory, your sampling rate should be 2x the highest frequency of the incoming signal that you are measuring. However, we recommend that you use 5x...

FAQ 2009-09-29

Does the Measurement Manager (AMM) run on Window Vista operating system?
Yes. The Measurement Manager (AMM) rev. 1.8.3.0 and above will able to run on Windows Vista ...

FAQ 2009-06-10

How can I access to the maximum memory depth (32M/16M) as stated in the U2701A/U2702A Modular Oscilloscope's data sheet?
You can see the effects of maximum memory depth 32/16 Mpts in zoom mode….

FAQ 2009-02-04

Do the U2300A Series USB DAQ devices provide opto-isolation of the analog inputs?
No, the U2300A Series USB DAQ devices do not provide opto-isolation of the analog input channels.

FAQ 2009-02-04

How do I calculate the dc vertical gain accuracy of a U2701A/U2702A USB Modular Oscilloscope?
The dc vertical gain accuracy of a U2701A/U2702A USB Modular Oscilloscope depends on the error values in the measured value....

FAQ 2009-02-04

Does the Keysight Measurement Manager (AMM) support regional language settings other than English (US)?
Yes, the Keysight Measurement Manager (AMM) supports regional language settings other than English (US)….

FAQ 2009-01-12

Are the USB data acquisition (DAQ) devices compatible with USB 1.1 or USB 2.0?
The USB data acquisition (DAQ) devices come with Full Speed USB (12Mbps) which is compatible with any USB Host 1.1 and 2.0.

FAQ 2008-09-25

What is the maximum analog output current from the U2300A Series Data Acquisition (DAQ) devices?
The maximum analog output current from the U2300A Series Data Acquisition (DAQ) devices is 5mA.

FAQ 2008-09-25

What is the lowest sampling rate that can be set for the U2300A/U2500A Series USB Data Acquisition (DAQ) devices?
The Keysight U2300A/U2500A Series Data Acquisition (DAQ0 devices can support sampling rates as low as 3Sa/s.

FAQ 2008-09-25

What programming platforms are compatible with the U2300A Series Data Acquisition (DAQ) devices?
Keysight VEE, LabView, Microsoft Visual Studio and C++ are compatible with the U2300A Series Data Acquisition (DAQ) devices.

FAQ 2008-09-24

What are the maximum sampling rates for the U2531A, U2541A and U2542A Data Acquisition (DAQ) devices?
The maximum sampling rates for the U2531A, U2541A and U2542A Data Acquisition (DAQ) devices are:….

FAQ 2008-09-24

Which thermocouple types are compatible with the U2802A Thermocouple input device?
Eight standard thermocouple types defined in the NIST ITS-90 Thermocouple Database are compatible with the U2802A input device….

FAQ 2008-09-24

What is the expected lifetime of the relays used in the Keysight 34970A plug-in modules?
The Keysight 34970A Relay Maintenance System automatically counts the cycles on each relay in the instrument and stores the total count in non-volatile memory on each switch module.

FAQ 2008-01-08

What is the mean time between failures (MTBF) for the 34970A?
20+ years for the 34970A and its module cards.

FAQ 2005-05-11

What are the sizes and weights of the E8401A, E8403A, and E8404A?
Size and weight information is listed in Appendix A of the E8401A, E8403A User and Service manual.

FAQ 2004-06-28

1 2 Next