Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

Refine the List

remove all refinements

By Topic

By Type of Content

By Product Category

1-25 of 52

Sort:
How to measure output frequency of E4981A Capacitance Meter?
To measure the output frequency of E4981A Capacitance Meter, interface box (Keysight part number: 04294-61002) is required…

FAQ 2017-09-20

When automating markers on the ENA is it possible to programmatically query the indicated inductance or capacitance on a Smith Chart?
The inductance / capacitance information cannot be directly queried via the automation interfaces. The inductance (positive reactance, top half of the Smith Chart) or capacitance (negative reactance, lower half of the Smith Chart) is not available as an automation query.

FAQ 2014-08-11

Does the ENA 6 series have the swept sweep mode in the frequency sweep?
No. The E5061A/62A and E5061B have only stepped sweep mode in the frequency sweep.

FAQ 2013-04-25

What is the difference between an "ECal Confidence Check" and a Network Analyzer "System Verification" test?
The ECal Confidence Check is a method to check the accuracy of a calibration performed with either a mechanical cal kit or an ECal module. System verification testing provides network analyzer users a method to verify that the network analyzer is ...

FAQ 2012-12-18

Is it possible on the Keysight ENA series Network Analyzers to over-ride the output source blanking at every sweep end?
Yes, the output source blanking on sweep retrace can be prevented by turning off the Initial Source Port Control function.

FAQ 2012-12-18

On the Keysight E4980A, what is the "DC Source Option 001 (±10 VDC Max)" and how is it utilized?
A summary description of the enhancements provided by E4980A option 001 - 'Power and DC Bias Enhancement Option'

FAQ 2012-12-02

What are the implications of swapping test heads between different Keysight 4287A Impedance Analyzers?
The Keysight 4287A Impedance Analyzer must be used with the furnished test head as a set because it is an indivisible portion of the calibrated 4287A.

FAQ 2012-01-16

How is trace math implemented within the Keysight Technologies Vector Network Analyzers?

FAQ 2012-01-11

Is it possible to change the font size of softkey menu on ENA?
Yes. The font size of softkey menu can be changed with following procedure...

FAQ 2011-10-07

On the ENA, how can I make CW sweep (Fixed frequency) without turning off the ENA's output signal each time a sweep finishes?
Turn off the "Init Src Ctrl" feature, then hold trigger.

FAQ 2011-10-07

What is the difference between Smoothing and Averaging on a Keysight network analyzer?

FAQ 2011-10-07

What is the difference between "sweep speed", "cycle time" and "time per data point" as related to a vector network analyzer?

FAQ 2011-10-07

The "set Zo" function does not appear to affect the displayed S-parameters of my network analyzer. How does this function work?

FAQ 2011-10-07

What are the equations that relate Real and Imaginary data pairs to Log Magnitude, Polar, Phase, and Smith Chart formats?

FAQ 2011-10-07

When I save a Touchstone file with the ENA / ENA-L, which calculation will be reflected in the Touchstone file?
All calculations are reflected in the Touchstone file except for the mixed-mode conversion.

FAQ 2011-10-07

How can I calculate the equivalent phase delay, as a function of frequency, for a given electrical delay as set on Vector Network Analyzer?
Equivalent phase delay, based upon electrical delay is computed as: θ˚ = Ftest * Delay * 360

FAQ 2011-10-07

Using the VBA program, can the ENA / ENA-L control the handler interface to control other peripherals?
Yes.

FAQ 2011-10-07

For Cable Testing should I use a TDR, a network analyzer, or both?
The cable specifications will determine the test equipment requirements...

FAQ 2011-10-07

On the ENA / ENA-L, what occurs if I select "order-based display" in sweep mode?
Measurement points of different segments are plotted in constant intervals.

FAQ 2011-10-07

Does the touchstone file generated by the ENA / ENA-L include the electrical delay?
The touchstone files do not include electrical delay. Please use port extension.

FAQ 2011-10-07

How can I know the stray capacitance and residual inductance values from OPEN A/B and SHORT A/B measurement data displayed on the E4980A LCD?
The E4980A displays the open admittance and the short impedance obtained for Open/Short compensation as OPEN A, OPEN B, SHORT A and SHORT B values on the CORRECTION Setup page.

FAQ 2011-06-07

How can the S21 to transmission impedance (Zt) conversion equation on the 4395A Operation Manual be derived?
The equivalent circuit model of transmission measurement is as follows.

FAQ 2011-06-03

For the 4395A / 4396B combination analyzer in spectrum analyzer mode with the noise format. Are the indicated units in error for this mode?

FAQ 2011-05-06

When measuring a capacitor via a Keysight LCR meter, what is the best circuit mode, Cs or Cp?
To measure L, C, or R, there are two equivalent circuit models.The LCR meter can select the mode by setting the FUNC (function) to Cp, Cs, Lp or Ls.

FAQ 2010-09-30

What are primary differences between the E4991A and 4291B?
The major difference is frequency range. E4991A: 3 GHz, 4291B: 1.8 GHz.

FAQ 2010-07-02

1 2 3 Next