Aqui está a página que achamos que você queria. Veja o resultado da pesquisa ao invés de:

 

Contate um especialista

Suporte técnico

Produtos PXI

Support by Product Model Number:

101-125 de 133

Sort:
Can I put the Keysight Switch cards into a PXIe chassis?
Only a PXIe chassis that has hybrid slots...

FAQ 2010-10-11

What kind of backplane connectors do the PXI switches have?
The M9101A-M9160A PXI switches are PXI1 with a J1 only connector...

FAQ 2010-10-11

Do these products appear in the Keysight connection expert?

FAQ 2010-10-11

Will ExpressVIs work with Keysight hardware?
No. Keysight has VIs available to use with LabView but not ExpressVIs.

FAQ 2010-10-06

Can I run a program that is controlling my PXI instrument while using its soft front panel (SFP)?
Not at this time...

FAQ 2010-10-06

What is the difference between PXIe and AXIe?
The AXIe standard provides the maximum scalability to address a range of platforms...

FAQ 2010-10-06

Can I use the PXIe products over LAN?
If the PXIe chassis has an embedded controller with a LAN port then the PXI system can connect to a LAN port...

FAQ 2010-10-06

Can I replace other vendors' module (for example a digitizer) with a Keysight one?
There are two aspects to consider...

FAQ 2010-10-06

What drivers will be provided with modular products?
IVI-COM, IVI-C and LabVIEW (G), are provided with all Keysight modular products...

FAQ 2010-10-06

What is the compatibility between PXIe chassis and Keysight new PXI/PXIe modules?
Keysight modules come in several varieties, so inspection is required to determine compatibility...

FAQ 2010-10-06

Can I use SCPI to communicate with my Keysight modules?
No. Connectivity is provided through Drivers.

FAQ 2010-10-06

What is the data transfer rate of PXI, PXIe, and AXIe?
PXI-1 has two variants...

FAQ 2010-10-06

Can I use PXI-1 existing cards in the Keysight Card cages and are there any that will no longer work?
Older PXI (PXI-1) modules (which have a J2 present) will not work in Keysight 18-slot PXIe chassis...

FAQ 2010-10-06

Does Keysight have mass interconnect solutions?
There are mass interconnect solutions from MAC panel....

FAQ 2010-10-06

Are all PXIe system modules/controllers compatible with all chassis?
No, the PXIe standard requires the chassis support certain configurations but not all...

FAQ 2010-10-06

How do I find a partner to help develop my modular solution?
Keysight has a number of solution partners that can help define and create your modular solution...

FAQ 2010-10-06

Where can customers download instrument drivers? (LabVIEW, Visual-studio.net,…)
The instrument drivers are provided with each instrument on a CD...

FAQ 2010-10-06

Where can customers find user manuals and example programs for AXIe & PXIe products?
Datasheets of modular products will be included on the CD shipped with every product and will be available on Keysight.com from the product page...

FAQ 2010-10-06

IO Libraries Suite: How do I fix the error message “Missing or Damaged GPIB-32.dll”?
Install NI-488.2 version 2.5 (or later)...

FAQ 2010-09-20

IO Libraries Suite: Is it possible to have both an NI GPIB card and a Keysight GPIB card or converter working in the same system?
Yes, it is possible with many version’s of Keysight IO Libraries.

FAQ 2010-09-08

IO Libraries Suite: Where do I find sample programs for SICL, VISA, and VISA COM?
Sample programs are available using SICL, VISA, and VISA COM in the IO Libraries Suite installation and on Keysight.com

FAQ 2010-09-08

IO Libraries Suite: What interfaces and operating systems are supported?
View the Keysight IO Libraries Support matrices.

FAQ 2010-09-08

IO Libraries Suite: What has changed in IO Libraries Suite 16.0?
PXI/PXIe support, IVI USBTMC driver, industry standards tracking, product enhancement and bugfixes

FAQ 2009-09-01

IO Libraries Suite: What is the VISA 32 Open Report?
The VISA 32 Open Report provides a quick "snapshot" of information about all of the instruments configured on your PC.

FAQ 2009-08-25

IO Libraries Suite: Why does T&M Toolkit’s IO Monitor quit working when I install IO Libraries Suite 15.0, or later?
Keysight IO Libraries Suite 15.0, and later, includes a new, updated version of the IO Monitor tool. Because of this, the older IO Monitor shipped with T&M Toolkit will no longer function.

FAQ 2009-08-25

Voltar 1 2 3 4 5 6 Avançar