이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

DC 전원 공급기 비교

모델 번호 입력:

1-25 / 113

정렬방식:
B2961A/B2962A에서 펄스 신호 출력하려면 어떻게 설정해야 하나요?
아래 링크된 문서참조하세요.

FAQ 2016-07-04

B2961A/B2962A에서 사인파형을 출력하려면 어떻게 설정해야 합니까?
아래 링크된 문서를 참조하십시오.

FAQ 2016-07-04

655XA 시리즈의 내부 메모리타입
내부메모리정보

FAQ 2016-06-07

For an auto-ranging power supply, how do I determine the maximum output current for any operating voltage? | Keysight
You will always obtain rated output power of the unit along any point of the auto-ranging operating curve.

FAQ 2015-09-08

B2900A를 컨트롤할 수 있는 인터페이스 종류는 무엇이 있습니까?
GPIB, USB, LAN이 가능합니다.

FAQ 2015-07-22

Is U2700A series USB Modular Instruments supported in Linux environment?
No. U2700A Series are not supportable in Linux environment. The drives for USB Modular only build for Microsoft Windows.

FAQ 2014-11-25

Why are USB modular instruments (U2700 Series) and USB DAQ modules (U2300, U2500, U2600 Series) not detectable by the E5810B?
Establish the connection between the USB modular Instrument and the PC directly, and then disconnect the device from the PC (while it’s still powered-on), and connect to E5810B.

FAQ 2014-04-17

E363xA, E364xA 파워서플라이는 사용자가 사용 할수 있는 내부메모리의 양은 얼마인가?
E3631A, E3632A, E3633A and E3634A는 출력 파라미터를 위한 3개의 비휘발성 전압, 전류 limit, over voltage protection 세팅을 각각 저장 할 수 있는 리콜 상태를 가집니다.

FAQ 2014-04-15

How can I source an exponential waveform on the B2961A/B2962A?
Click the above link for details.

FAQ 2013-12-24

계측기 Host 정보 확인 방법
계측기 Host 정보 확인하는 방법

FAQ 2013-10-17

What is the difference among data query commands such as ":FETCh?", ":MEASure?", ":READ?", :SENSe:DATA?"?
They have the function to query data similarly but there is some difference among them. Click the above link for details.

FAQ 2013-09-16

What is the difference among Trigger Types on Single View?
Click the above link for details.

FAQ 2013-09-16

What is the equivalent command to "Output after Sweep" parameter on "Sweep" dialog?
It should be [:SOURce]:FUNCtion:TRIGgered:CONTinuous. Once you send it with the parameter "ON", the parameter is set to "END VALUE".

FAQ 2013-09-16

How can I save or load the measurement setups on the B2961A/B2962A?
Click the above link for details.

FAQ 2013-03-11

Quick I/V Measurement Software cannot recognize the B2961A/B2962A.
The B2961A/B2962A is supported by Quick I/V Measurement Software in the revision 2.0 or later. Click the above link for details.

FAQ 2013-03-11

Can B2961A/B2962A connect its output to the ground when the output is switched off?
Yes, the B2961A/B2962A can connect its output to the ground by specifying the output-off state to "ZERO" when the output is switched off.

FAQ 2013-03-11

How can I set up Power-on State of the B2961A/B2962A?
It is possible to store the desired instrument condition as Power-on State. Click the above link for details.

FAQ 2013-03-11

How can I perform a self calibration on B2961AB2962A?
Click the above link for details.

FAQ 2013-03-11

How can I find the sensing type of the channels on the B2961A/B2962A?
If the low terminal state of the channel is set to FLOATING, you can see the status indicator on GUI.

FAQ 2013-03-11

How can I find the low terminal state of the channels on the B2961A/B2962A?
If the low terminal state of the channel is set to FLOATING, you can see the status indicator on GUI.

FAQ 2013-03-11

How can I configure Trigger Output Signals with the B2961A/B2962A?
Click the above link for details.

FAQ 2013-03-11

How to configure the time constant of the output filter with the B2961A/B2962A?
The time constant of the output filter can be configured on the Output Filter dialog box. Click the above link for details.

FAQ 2013-03-11

Can I upgrade from B2961A to B2962A?
No, you cannot upgrade from B2961A to B2962A.

FAQ 2013-03-11

Where can I get LabVIEW Plug and Play Instrument Driver for B2961A/B2962A?
You can get LabVIEW Plug and Play Instrument Driver for B2961A/B2962A from NI.com.

FAQ 2013-03-11

How can I update its firmware on the B2961A/B2962A?
Click the above link for details.

FAQ 2013-03-11

1 2 3 4 5 다음