Aqui está a página que achamos que você queria. Veja o resultado da pesquisa ao invés de:

 

Contact an Expert

Suporte técnico

Medição Eletrônica

Support by Product Model Number:

Refine the List

remove all refinements

Mercado/Tecnologia

By Type of Content

Categoria de Produto

By Other Category

126-150 de 1001

Sort:
TowerJazz Announces New Interoperable PDK for ADS on TPSCo's Advanced 65nm RF CMOS Platform
TowerJazz's new interoperable PDK targets various applications such as WiFi, Transmitters/Receivers (Tx/Rx), cell phones, tuners, and automotive radar, among others.

Materiais para imprensa 2015-12-23

Keysight Expands UXM Multi-Format Test Capabilities with GSM, TD-SCDMA

Materiais para imprensa 2015-12-20

Keysight introduces PAM-4 analysis software for oscilloscope platforms
Keysight Technologies, Inc. (NYSE: KEYS) today introduced measurement application software designed to help engineers quickly and accurately measure and quantify PAM-4 (pulse amplitude modulation with four amplitude levels) signals.

Materiais para imprensa 2015-12-16

Keysight Technologies' Updated MOI Now Supports USB Type-C™ Connector
Keysight Technologies, Inc. (NYSE: KEYS) today announced the availability of a newly updated Method of Implementation (MOI) document for cable and connector assembly compliance tests defined in Rev. 1.1 of the USB Type-C specification and Rev. 1.0 of the USB Type-C Compliance Test Specification (CTS).

Materiais para imprensa 2015-12-10

• MIPI UniPro Interoperability Test Workshops Advance Industry Adoption of High-Speed
Second testing event of the MIPI UniPro(SM) and MIPI M-PHY® specifications demonstrates mature, efficient implementation for industry adopters and highlights UFS-Enabled applications

Materiais para imprensa 2015-12-09

Keysight Technologies Introduces Industry's First DisplayPort 1.3 Source Electrical Performance
Keysight Technologies, Inc. (NYSE: KEYS) today announced the industry's first DisplayPort 1.3 source compliance and validation software. The U7232D DisplayPort 1.3 compliance and validation test software runs on Keysight's industry-leading Infiniium oscilloscopes and provides a complete compliance test suite for the extensive physical-layer tests required for DisplayPort 1.3 source devices.

Materiais para imprensa 2015-12-09

Leti to collaborate with Keysight Technologies to enable expansion of FD-SOI technology
CEA-Leti announces it has signed an agreement with Keysight Technologies, a device-modeling software supplier, to adapt Leti’s UTSOI extraction flow methodology within Keysight’s device modeling solutions for high-volume SPICE model generation.

Materiais para imprensa 2015-12-08

Keysight Technologies Enables 5G Research with Beamforming, Channel Modeling in 5G Software Library
Keysight introduces beamforming and channel modeling capabilities in the Keysight EEsof EDA W1906EP 5G Baseband Verification Library

Materiais para imprensa 2015-12-03

Keysight Technologies Enables 5G Research with Beamforming, Channel Modeling in 5G Software Library
Keysight introduces beamforming and channel modeling capabilities in the Keysight EEsof EDA W1906EP 5G Baseband Verification Library.

Materiais para imprensa 2015-12-03

Keysight Technologies Introduces USB Type-C™ Protocol Trigger, Decode Software
Keysight Technologies, Inc. (NYSE: KEYS) today introduced the industry's first oscilloscope-based USB-PD (Power Delivery) protocol decoder software with real-time triggering and protocol decode performance.

Materiais para imprensa 2015-12-02

UXM enables 600 Mbps data throughput, 4x4 DL MIMO, carrier aggregation, integrated channel emulation

Materiais para imprensa 2015-12-02

Keysight Showcases Communication Test Solutions at GLOBECOM 2015
Keysight had on site demonstrations include: 5G Waveform Generation and Analysis Testbed Reference Solution, 5G Channel Sounding Reference Solution and 5G System-Level simulation software

Materiais para imprensa 2015-12-01

Keysight Technologies to Showcase Communication Test Solutions at GLOBECOM 2015
Keysight announces that it will demonstrate its latest test solutions in 5G, IoT and LTE-Advanced along with hosting a workshop and participation in panel discussions at GLOBECOM 2015, Hilton San Diego Bayfront Hotel, Booth 207, Dec. 6–10.

Materiais para imprensa 2015-12-01

Keysight Technologies, UCSD, Demonstrate World's First 5G, 100 to 200 Meter Communication Link up to
In collaboration with the University of California, San Diego, Keysight demonstrated 64 (8x8) and 256-element (16x16), 60 GHz silicon wafer-scale phased array transmitter.

Materiais para imprensa 2015-11-30

University Relations
Keysight takes an active role in supporting higher education and research around the world. This Keysight for Universities home page provides an index to the programs of greatest interest to university faculty, students and staff. Learn more about our latest research collaborations, research tools, education support, recruiting of top university tale

Materiais para imprensa 2015-11-17

Keysight Technologies Introduces PAM-4 Capability for its Advanced Design System Channel Simulator
Keysight announces a four-level PAM-4 capability for the ADS Channel Simulator. The introduction of this capability further advances Keysight's leadership position in IBIS-AMI SerDes channel simulation.

Materiais para imprensa 2015-11-17

Keysight Technologies Introduces PAM-4 Capability for its Advanced Design System Channel Simulator
Keysight Technologies, Inc. (NYSE: KEYS) today announced a four-level pulsed amplitude modulation (PAM-4) capability for the Keysight EEsof EDA Advanced Design System (ADS) Channel Simulator. The introduction of this capability further advances Keysight's leadership position in IBIS-AMI SerDes channel simulation.

Materiais para imprensa 2015-11-17

Keysight Selects Fraunhofer EMFT as its First Low-Frequency Noise Reference Center for EMEAI
Keysight announces that Fraunhofer Research Institution for Microsystems and Solid State Technologies EMFT (Fraunhofer EMFT) is the first low-frequency noise measurements reference center able to demonstrate the Keysight EEsof EDAs E4727A Advanced Low-Frequency Noise Analyzer in Europe, the Middle East, Africa and India (EMEAI).

Materiais para imprensa 2015-11-04

Keysight Technologies Collaborates with China Southeast University on 5G Massive MIMO Research
New Research Designed to Accelerate Progress in 5G Massive MIMO Implementation

Materiais para imprensa 2015-10-29

Keysight Technologies Introduces MIPI® Receiver Test Software for PHY-Layer Standards
New Software Enables Automated Testing According to Conformance Test Suite for MIPI C-PHY 1.0 Standard

Materiais para imprensa 2015-10-26

Keysight Technologies Introduces MIPI® Receiver Test Software for PHY-Layer Standards
New Software Enables Automated Testing According to Conformance Test Suite for MIPI C-PHY 1.0 Standard

Materiais para imprensa 2015-10-26

Keysight Technologies to Demonstrate Advances in Hardware, EDA Software Solutions at EPEPS 2015
Keysight announces it will demonstrate its latest hardware and electronic design automation (EDA) software solution releases at EPEPS 2015, DoubleTree by Hilton Hotel, Booth 3, San Jose, Calif., Oct. 25-28.

Materiais para imprensa 2015-10-22

Keysight Technologies Introduces Industry's Highest-Data-Rate, Deepest-Memory Logic Analyzer
Instrument Enables LPDDR4, DDR4 Protocol Validation and Debugging at Data Rates Proven to 4 Gb/s

Materiais para imprensa 2015-10-13

Keysight Technologies Introduces Software Tool that Enables Deeper, Easier Debugging of DDR4, LPDDR4
Oscilloscope-Based Software Helps Designers Pinpoint Root Cause of Problems

Materiais para imprensa 2015-10-12

Keysight Technologies to Demonstrate Latest Simulation Software Solutions at CSICS
Keysight announces it will demonstrate its latest RF circuit, system and 3-D electromagnetic design and electro-thermal simulation software solutions at the Compound Semiconductor IC Symposium (CSICS 2015), Sheraton New Orleans, Booth 601, New Orleans, Oct. 11-14.

Materiais para imprensa 2015-10-08

Voltar 1 2 3 4 5 6 7 8 9 10 ... Avançar