Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

Refine the List

remove all refinements

By Industry/Technology

By Type of Content

1-25 of 1809

Sort:
Using a Waveform Generator to Create a Pseudorandom Binary Sequence Signal
Learn how to simulate noise in a variety of frequency bandwidths and perform acoustic testing of a structure. Overcome test challenges using a waveform generator to create pseudorandom binary sequence signals.

Case Study 2020-02-14

PDF PDF
IQ Signal Generation Made Easy
This white paper will cover how to generate both ideal and non-ideal IQ signals. We will use the Keysight 33500B and 33600A Trueform Series waveform generators with the IQ Signal Player option to show you how to do this.

Case Study 2020-02-06

PDF PDF
Using Simulation to Overcome 3 Millimeter-Wave Design Challenges
Radio designers are embracing system simulation to reduce design time and ensure their devices meet the 5G NR specification. We explore 3 simulation techniques to overcome mmWave design challenges.

Case Study 2020-02-01

PDF PDF
Three Best Practices for Optimizing EVM Measurements for Wideband Signals
Learn three best practices for accurately making and optimizing EVM measurements.

Case Study 2020-01-31

PDF PDF
Automotive Ethernet: Enabling the Future of Autonomous Driving
Autonomous vehicles and advanced driver assistance systems (ADAS) need higher bandwidth and lower latency. Automotive Ethernet is the new backbone for faster onboard networking.

Case Study 2020-01-31

PDF PDF
4 Ways to Efficiently Generate Complex Waveforms
Generating the signals to characterize, test or troubleshoot electrical designs or systems can be tedious and time=consuming. So, our experts came up with four ideas to help you more efficiently generate simple or complex waveforms.

eBook 2020-01-31

PDF PDF
Automotive ECU Designer Reduces Power Consumption by 10%
An automotive chipmaker solved large peak current issues, reducing power consumption and heat generation while ensuring reliability of its products for advanced driver assistance systems.

Case Study 2020-01-29

Engineering the 5G World
This book provides an overview of 5G technology, focusing on test and measurement and its role in the development of 5G. This book delivers the collective distilled wisdom of Keysight 5G experts. It summarizes the fundamentals of 5G across the entire ecosystem and introduces best practices for testing 5G solutions across the entire 5G workflow.

eBook 2020-01-29

PDF PDF
The Blueprint to a Successful Industrial Internet of Things
This white paper addresses device reliability, adherence to industry standards, regulations, and interoperability for a successful Industrial Internet of Things (IIoT).

Case Study 2020-01-29

PDF PDF
Automotive ECU Designer Reduces Power Consumption by 10%
An automotive chipmaker solved large peak current issues, reducing power consumption and heat generation while ensuring reliability of its products for advanced driver assistance systems.

Case Study 2020-01-29

PDF PDF
Designing for DDR4 and Beyond
High-speed digital standards are evolving to keep pace with emerging technologies such as 5G, the Internet of Things (IoT), artificial intelligence, and autonomous vehicles. While each technological advancement certainly raises the bar for innovation, each step forward brings forth new obstacles, particularly for hardware engineers designing memory systems. It's critical that memory designers employ the right simulation-based design and analysis workflow solution. Here's how.

Case Study 2020-01-26

PDF PDF
Five Strategies to Accelerate 5G Device Development
Designing and implementing 5G devices in new mmWave operating bands present new challenges. New technologies and evolving standards increase design complexity. Here are five strategies to help you address these challenges and get your designs to market faster.

Case Study 2020-01-23

PDF PDF
PCIe 5.0 – The Next Generation of Peripheral Component Interconnect
This application note describes breakthrough technologies that have transformed the way systems can be tested in the field while providing higher performance, improved accuracy, capability and frequency coverage to 50 GHz

Case Study 2020-01-21

PDF PDF
PCIe 5.0 - The Next Generation of Peripheral Component Interconnect
Learn about the next generation of PCI Express. PCI Express 5.0 doubles the data rate from the PCIe 4.0

Case Study 2020-01-21

PDF PDF
Four Channel Power Measurement Must-Haves for Your Field Kit
Modern communications systems have complex modulation formats. This white paper covers four channel power measurements you should make in the field to ensure the performance and compliance of these systems.

Case Study 2020-01-19

PDF PDF
Test Teams Gain Competitive Advantage by Embracing a Platform-Based Approach
Electronics are getting more sophisticated and complex every day. Chips, boards, and the systems they make up are increasingly difficult to design. Companies engaged in electronic product development are regularly employing platform-based approaches in their design projects. Benefits of a platform-based approach include faster time-to-market, increased engineering productivity and cost-efficiency, improved design and test reuse, and faster analysis and insight that supports better decision-making.

Case Study 2020-01-16

PDF PDF
DDR Memory Test Challenges from DDR3 to DDR4 and DDR5
This whitepaper will discuss the progression of the technology, how tests have had to evolve accordingly, the test equipment that can help combat challenges presented by current and future generations of DDR.

Case Study 2020-01-15

PDF PDF
Modulation Techniques for Satellite Communications
Focuses on modulation techniques for modern satellite communications from generating and analyzing the signals to the impacts of phase noise on modulation quality.

Case Study 2020-01-11

PDF PDF
Put Technical Support Front and Center: Pave the Way for a Smooth Transition to 5G

Case Study 2020-01-08

PDF PDF
Put Technical Support Front and Center: Pave the Way for a Smooth Migration to 5G
This white paper examines frequently overlooked challenges in the design and development of 5G devices and networks and the role value-added support services play in addressing them. It also outlines the specific challenges wireless product designers face as they migrate to 5G and explores how improved management and support of test assets can play a pivotal role in overcoming them.

Case Study 2020-01-08

PDF PDF
PCBA Manufacturer Shifts Gears for Autonomous Driving with Keysight ICT
Leading printed circuit board assembly manufacturer tests 15 million automotive boards with almost no downtime, exceeding its test target.

Case Study 2020-01-07

PDF PDF
Three Steps to Overcome Signal Integrity Challenges
Tackling signal integrity issues in today’s complex boards is challenging. Common challenges for signal integrity engineers include crosstalk, signal loss or distortion, and bandwidth degradation. Overcome common signal integrity challenges with these three steps.

Case Study 2020-01-07

PDF PDF
PCBA Manufacturer Shifts Gears for Autonomous Driving with Keysight ICT
Leading printed circuit board assembly manufacturer tests 15 million automotive boards with almost no downtime, exceeding its test target.

Case Study 2020-01-07

PCBA Manufacturer Shifts Gears for Autonomous Driving with Keysight ICT
Leading printed circuit board assembly manufacturer tests 15 million automotive boards with almost no downtime, exceeding its test target.

Case Study 2020-01-06

PDF PDF
Comparisons: DAQ970A/DAQ973A to 34970A/34972A Data Acquisition System
This paper provides a comparison of the next generation DAQ970A / DAQ973A and, the 34970A / 34972A Data Acquisition Systems.

Case Study 2020-01-06

PDF PDF

1 2 3 4 5 6 7 8 9 10 ... Next