这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

缩小范围

去除所有优化

行业/技术

按内容类型

1-25 / 1258

排序:
4 个实际应用电磁仿真
4 个实际应用电磁仿真

电子书 2019-11-19

PDF PDF 17 MB
High-Speed Digital Design Success Demands a Modern Workflow
A simulation and measurement-based workflow enables Power Integrity engineers to design resonant-free power delivery and avoid rogue voltage waves.

案例分析 2019-11-08

PDF PDF
Four Tips Protect Against Power -Related Damage
High power devices that store energy or contain reactive components are notorious for damaging themselves and the surrounding equipment. Get four tips to help protect your devices and equipment. The first tip provides a way to not only protect against over-power, and not just overvoltage or overcurrent. The second tip helps protect your supply when working with more than one power source. To reduce inrush current, tip 3 provides a method to slow the rate of output voltage change. Lastly, some devices can handle a tremendous surge of current and tip four addresses how to keep the power supply active during a surge.

电子书 2019-11-07

PDF PDF 2.02 MB
GISTDA National Space Agency Captures CubeSat Opportunity - Case Study
By setting up an RF satellite lab that leveraged a handheld spectrum analyzer, Thailand’s space agency overcame the testing challenges facing its new SmallSat program.

案例分析 2019-11-04

PDF PDF 3.49 MB
Production Throughput Doubles with Keysight i3070 Advanced Throughput Multiplier - Case Study

案例分析 2019-11-01

PDF PDF 1.48 MB
The Blueprint to a Successful Industrial Internet of Things (IIoT)
This white paper will address each of the individual components within a device, as well as the finished product, and offer guidance for creating an effective test matrix outline. Developers can use these concepts as a foundation on which to build a complete test plan to deploy industrial IoT devices with a greater degree of confidence.

案例分析 2019-11-01

PDF PDF
First Steps in 5G: Overcoming New Radio Device Design Challenges - Part 4
This white paper explains the need for over-the-air (OTA) testing and the related challenges.

案例分析 2019-10-30

PDF PDF
First Steps in 5G: Overcoming New Radio Device Design Challenges - Part 1
This white paper provides an overview of the 5G New Radio standard.

案例分析 2019-10-30

PDF PDF
First Steps in 5G: Overcoming New Radio Device Design Challenges - Part 3
This white paper provide an overview of MIMO and beamforming and related challenges.

案例分析 2019-10-30

PDF PDF
Four Tips for Powering and Testing Higher Current Devices
High current systems share several challenges for a dc power supply. The first challenge is to measure not only the large active current but also the small standby currents used by the control logic. A second challenge is to mimic a battery and supply large amounts of current when the voltage or load suddenly changes. The third challenge is to speed device characterization by changing output voltages quickly. Finally, understanding the effect that wiring has on power supplies ability to react to a change in voltage or the load.

电子书 2019-10-27

PDF PDF 8.84 MB
Antenna Module Manufacturer Accelerates 5G mmWave Development by More than 50%
A global antenna module manufacturer uses Keysight's 5G R&D Test Bed and PNA network analyzer to accelerate the development time for its 5G mmWave products based on beamforming technologies.

案例分析 2019-10-25

PDF PDF
X-Apps 藏宝图 能够加速测试的信号分析仪必备测量软件
X-Apps 藏宝图 能够加速测试的信号分析仪必备测量软件

电子书 2019-10-25

PDF PDF 4 MB
Antenna Module Manufacturer Accelerates 5G mmWave Development by More than 50%
A global antenna module manufacturer uses Keysight's 5G R&D Test Bed and PNA network analyzer to accelerate the development time for its 5G mmWave products based on beamforming technologies.

案例分析 2019-10-25

PDF PDF 5.70 MB
Signal Integrity Fundamentals
Learn signal integrity fundamentals from simulation to measurement to help you design your high-speed digital devices with higher reliability and lower costs.

案例分析 2019-10-23

PDF PDF
The Case for Integrated Design Software
Design World article presenting the case for integrated design software by Lee Teschler.

文章 2019-10-22

Four Tips to Achieve More with a Multiple Output Power Supply
Get four tips to get the most out of your multiple output power supply.

电子书 2019-10-21

PDF PDF
Signal Integrity Measurement Analysis
Learn how to address signal integrity problems early, to ensure optical circuit design and development that works reliably at a reasonable cost.

案例分析 2019-10-17

PDF PDF
Improving the Battery Life of Implantable Medical Devices
Battery drain analysis is crucial to ensure that implantable medical devices have maximum battery life and preditable battery charge and replacement cycles.

案例分析 2019-10-16

PDF PDF
Implantable Medical Devices Customer
A Keysight application engineer worked with the design engineering team at an implantable medical device manufacturer to recommend a solution consisting of hardware and software for battery drain analysis. The key solution components are the N6705C DC Power Analyzer, the N6781A 2-quadrant SMU for battery drain analysis and Keysight's 14585A control and analysis software.

案例分析 2019-10-16

PDF PDF 2.79 MB
The Power of Emulation - Part 1: Understanding the Impact of Emulation Tests on the Connected Car
Car makers are reducing design cycle time by emulating components and subsystems to ensure design and functional integrity for Connected Car and ADAS applications.

案例分析 2019-10-15

PDF PDF
相干光通信元器件测试推动实现 1.2 Tb 应用
相干光通信元器件测试推动实现 1.2 Tb 应用

案例分析 2019-10-14

PDF PDF 3 MB
Saving Lives by Saving Time with eCall
All new cars will come equipped with eCall by 2025 as mandated by the European Union. Keysight eCall test solution helps save time and money for original equipment manufacturers (OEMs).

案例分析 2019-10-09

PDF PDF
ASE Reduces Antenna-in-Package Test Time by 20% with Keysight’s PNA - Case Study
Learn how Keysight's PNA Vector Network Analyzer helped Advanced Semiconductor Engineering, Inc. accurately test its high frequency antenna-in-package designs, and reduce overall test time by 20%.

案例分析 2019-10-08

PDF PDF 3.18 MB
X-Apps Marks the Spot - Essential Signal Analyzer Measurement Apps for Saving Test Time
Learn how measurement applications increase both the capability and functionality of signal analyzers, while reducing your time to measurement insights.

电子书 2019-10-08

PDF PDF
ASE Reduces Antenna-in-Package Test Time by 20% with Keysight’s PNA
This case study describes how ASE increased measurement accuracy and reduced test time by 20% for its new AiP designs using the PNA.

案例分析 2019-10-08

PDF PDF

1 2 3 4 5 6 7 8 9 10 ... 下一页