Aqui está a página que achamos que você queria. Veja o resultado da pesquisa ao invés de:

 

Contact an Expert

Suporte técnico

Medição Eletrônica

Support by Product Model Number:

1-15 de 15

Sort:
Pushing the Boundaries to Achieve Ultra-broadband Communications at True Terahertz Frequencies
See how researchers at the University at Buffalo achieved the first ever system to transmit and receive communications at 1.025 terahertz.

Publicação 2018-12-10

PDF PDF 23 KB
The Difference Between Digitizers and Oscilloscopes for Wideband Measurements

Artigo 2017-09-20

Full Function Oscilloscopes for ATE Systems

Artigo 2017-09-20

Make accurate and fast design decisions with data analytics
Make accurate and fast design decisions with data analytics

Artigo 2017-08-25

2015 Global Digital Oscilloscopes Growth Award
Understand how Frost & Sullivan evaluates and decides on the winner for this award

Artigo 2016-01-05

PDF PDF 1.06 MB
Jitter Analysis: The Dual-Dirac Model, RJ/DJ, and Q-Scale - Application Note
This paper provides a complete description of the dual-Dirac model, how it is used in technology standards and a summary of how it is applied on different types of test equipment.

Artigo 2014-06-14

PDF PDF 515 KB
2014 Global PXI Instrumentation Growth Excellence Leadership Award - Article Reprint
Frost & Sullivan honors Agilent as a growth leader in the PXI modular instrumentation market in 2014.

Artigo 2014-05-22

PDF PDF 598 KB
Digital Oscilloscope
What is a digital oscilloscope? See the main characteristics of digital oscilloscopes.

Artigo 2013-07-25

What is waveform update rate and why does it matter?
Explore this often overlooked oscilloscope performance specification to learn how to determine an oscilloscope’s update rate and what a fast update rate can mean for you.

Artigo 2013-06-03

Caution: MIMO Test Challenges Ahead
Article published by Wireless Design & Development on MIMO testing challenges and methods to achieve higher data rates such as two0 and four-channel MIMO.

Artigo 2010-09-20

PDF PDF 70 KB
The Fifth Harmonic: Tradeoffs Between Sampling and Real-Time Oscilloscopes
When determining the required system bandwidth some vendors will use a “fifth harmonic” rule of thumb; however it is important to understand typical conditions at the receiver to accurately determine the amount of bandwidth you will need.

Artigo 2009-01-19

Validating the Physical and Protocol Layers in DDR Memory Interfaces

Artigo 2009-01-06

Eye-Diagram Analysis Speeds DDR SDRAM Validation

Artigo 2009-01-06

Is the 5th Harmonic Still Useful for Predicting Data Signal Bandwidth?
This article, published in High Frequency Electronics, compares using the 5th harmonic to using the system rise/fall times to determine the required bandwidth for your system. The article begins on page 18.

Artigo 2009-01-01

Simplify DDR Validation with SI Methods

Artigo 2008-01-06