Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

1-25 из 36

Упорядочить:
RF GaN Device Models and Extraction Techniques
This presentation was recorded at IMS 2019. The Workshop covers the market trends, technology and challenges in using Gallium Nitride (GaN) devices.

Демонстрация 2019-08-30

IIT Kanpur Develops ASM-HEMT Model for GaN Transistors Using Parametric and Device Characterization
The India Institute of Technology Kanpur creates an accurate and simple compact SPICE model and introduces an industry-grade model for power electronics and RF applications.

Пример реального применения 2019-07-10

PDF PDF 1.90 MB
PathWave Design Software
Accelerate your design cycle with integrated design and simulation software. Know your performance under simulated real-world conditions before you build.

Брошюра 2019-07-01

PDF PDF 13.23 MB
Transforming Engineering Education with Cutting-Edge Keysight Labs
Keysight is committed to continue with innovation that will enable researchers, educators, and students.

Пример реального применения 2019-06-25

PDF PDF 2.03 MB
Keysight Technologies Accelerates Design Workflows with New PathWave Design 2020 Software Suite
Keysight announces PathWave Design 2020, which includes the latest releases of Keysight's electronic design automation software to accelerate design workflows for radio frequency (RF) and microwave, 5G, and automotive design engineers.

Материалы для прессы 2019-06-03

Improved Data Sharing Across Product Development Workflow Would Improve Time to Market
Keysight Survey Reveals Improved Data Sharing Across the Entire Product Development Workflow Would Improve Time to Market for Electronic Devices.

Материалы для прессы 2019-04-08

The Future of Design and Simulation Workflows
While design engineers are facing many challenges, the most pressing are in the areas of data sharing and analysis. This report underscores the need for a new way to connect design and test data across the workflow.

Руководство по применению 2019-02-22

Simplifying the Economics of Test and Repair in Both the Factory and Depot - White Paper
This paper explores how to calculate the cost-of-test.

Руководство по применению 2019-02-21

PDF PDF 1.97 MB
Introduction to Wafer-level Measurement Solutions (WMS) – WMS Series Part 1 of 6
In this video we present an overview of the hardware and software used for making wafer level measurements up to 110 GHz.This is part of a 6 part video series on wafer level measurements.

Демонстрация 2018-05-09

Set up a measurement project with WaferPro Express – WMS Series Part 6 of 6
In this video, we will set up a new project in WaferPro Express, defining our measurements on our desired devices.

Демонстрация 2018-05-09

Configure WaferPro Express for measurements and probing – WMS Series Part 3 of 6
In this video, we will show you how to connect WaferPro Express to the instruments and then to the Velox prober control software.

Демонстрация 2018-05-09

Perform on-wafer RF calibration – WMS Series Part 5 of 6
In this video, we demonstrate an on wafer network analyzer calibration to 50 GHz.

Демонстрация 2018-05-09

Automated on-wafer millimeter wave measurements demo – WMS Series Part 2 of 6
In this demo, we measure S-parameters on a GaAs MESFET and capacitor structure in an automated fashion across the wafer. This leverages a lot of pieces together that will be explained in later videos: • configuring the WaferPro Express software to drive other instruments and wafer prober software • wafer alignment • RF S-parameter calibration • WaferPro Express project set up

Демонстрация 2018-05-09

Align wafer probes and create a wafer map – WMS Series Part 4 of 6
In this video, we demonstrate how to align a wafer to the reference plane of our probing system using the auto align feature in Velox. We will then generate a wafer map.

Демонстрация 2018-05-09

Power Electronics Device Modeling
Power Electronics Model Generator (PEMG) software provides a comprehensive modeling solution for discrete power electronics devices, with an intuitive UI and the latest, most powerful models.

Обзор технических характеристик 2018-03-23

Keysight Collaborates with Leading Research Centers to Reach Milestone in Low-Freq. Noise Measurment
Keysight announces it has reached a new milestone in low-frequency noise measurements through its work with leading research centers in Europe, Middle East, Africa and India (EMEAI). Using the new Advanced Low-Frequency Noise Analyzer (A-LFNA) and WaferPro Express software, designers can now measure noise more accurately in an even broader range of electronic devices.

Материалы для прессы 2018-02-05

IMECAS uses MBP to Create a PDSOI PN Junction Model
Researchers from the Institute of Microelectronics of Chinese Academy of Sciences (IMECAS) have proposed a new simulation model for the PN junction based on SOI.

Пример реального применения 2017-11-01

PDF PDF 391 KB
Why Get an ADS Service Support Contract?
The ADS service support contract is a key part of Keysight’s commitment to increasing your engineering productivity and advancing your long-term success. Learn more with this helpful flyer.

Брошюра 2017-10-30

PDF PDF 940 KB
Hangzhou Dianzi University Uses IC-CAP to Extract a Novel, Small-Signal Model for Bulk FinFETs
Case study on how Hangzhou Dianzi University created a novel compact model for bulk FinFETs that accommodates self-heating behaviors.

Пример реального применения 2017-10-10

PDF PDF 1.12 MB
Customizing Tables Just Got Easier with a New Python Module for MQA Software
Working with data tables is a basic skill every engineer learns early on in their career. When organized properly, tables can summarize a great deal of device data into a helpful information format, and that makes them extremely useful.

Статья 2017-07-12

How to Simplify Device Model Extraction using an Open Source User Interface
This video shows an example of an IC-CAP custom user interface (UI) for device modeling. In the selected modeling application, the DC modeling of a Zener diode is intentionally kept simple in order to demonstrate the features of the UI.

Видеоролики, демонстрирующие решение прикладных задач 2017-06-26

Static Random Access Memory (SRAM) Cell Modeling in MBP 2017
This video introduces a new turnkey solution for SRAM modeling now available in Keysight’s Model Builder Program 2017. The video describes the concept of SRAM cell modeling and highlights the major challenges of that process.

Демонстрация 2017-06-12

Extending the Power of IC-CAP Software with Python—PyVISA Instrument Control
Learn how to access the full capabilities of PyVISA from IC-CAP 2016 and create transforms for instrument control and data acquisition over any supported interface.

Статья 2017-05-31

How to Extract a BSIM4 DC Model
This video introduces a general DC modeling and characterization flow for the BSIM4 model, which is one of the most popular models used by the industry today for bulk CMOS.

Видеоролики, демонстрирующие решение прикладных задач 2017-05-24

SRAM Cell Model Generation and Modeling Efficiency Take Center Stage in New Software Releases
Accurate and efficient modeling is critical to successful design, especially when it comes to the Static Random Access Memory (SRAM) cell, the minimum geometry devices in integrated circuit technology.

Статья 2017-05-04

1 2 Следующие