这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

1-25 / 214

排序:
Improving Reliability of Semiconductor Devices - Case Study
Automation of random telegraph noise measurement (RTN) is now possible using the B1500A's waveform generator/fast measurement unit (WGFMU) module and WaferPro Express.

案例分析 2019-09-13

PDF PDF 2.49 MB
Powering E-Bikes and Battery Energy Storage Systems with Cell-Formation Solution - Case Study
E-Mobility manufacturer saves time and money with new cell formation solution to meet growing orders and stricter test criteria.

案例分析 2019-08-15

PDF PDF 2.89 MB
New PXIe Multiport Network Analyzer Speeds Multiport Active Antenna Development - Case Study
Learn how a leading global defense contractor accelerated development of a complex antenna, comprised of multiple Transmit Receive (TR) modules. The use of a multiport PXI Vector Network Analyzer characterized this multiport active antenna without relying on switches.

案例分析 2019-08-05

PDF PDF 2.18 MB
5G 射频设计初创公司以最快速度推出尖端的 GaN/GaAs 器件
5G 射频设计初创公司以最快速度推出尖端的 GaN/GaAs 器件

案例分析 2019-07-17

PDF PDF 3 MB
IIT Kanpur Develops ASM-HEMT Model for GaN Transistors Using Parametric and Device Characterization
The India Institute of Technology Kanpur creates an accurate and simple compact SPICE model and introduces an industry-grade model for power electronics and RF applications.

案例分析 2019-07-10

PDF PDF 1.90 MB
执行 5G 元器件表征和 测试的五大策略
5G 给整个移动生态系统带来了巨大的创收前景。这个生态系统涵盖了芯片和元器件制造商、器件制造商、网络设备制造商和服务提供商。5G 的技术复杂程度也呈指数增长。例如,大规模多路输入多路输出(MIMO)天线要求对每个天线元件进行多次传输和反射测量。

案例分析 2019-06-28

PDF PDF
Transforming Engineering Education with Cutting-Edge Keysight Labs
Keysight is committed to continue with innovation that will enable researchers, educators, and students.

案例分析 2019-06-25

PDF PDF 2.03 MB
生成相位相干射频信号的三种 配置方法
测试多天线系统时,要求测试系统必须能够提供多个信号,并且信号之间要有恒定的相位关系。生成相位相干信号时,不同的配置方法会导致不同的测量结果。

案例分析 2019-06-18

PDF PDF
迎接 5G NR 一致性测试的挑战
随着 5G 商用步伐的加快,针对预兼容性测试和一致性测试的准备工作变得极其重要。由于 5G NR 还没有提出完整的测试要求,并且使用了新的毫米波工作频段、更复杂的测试和持续演进的标准,因而在测试方面带来了许多新的挑战。

案例分析 2019-06-17

PDF PDF
High-Speed Interface Testing Made Simple with a Modern DMM - Case Study
Learn from this article how a computing company solves its testing challenges in validating high-speed interfaces, monitoring voltage changes, and accessing data fast with a modern digital multimeter.

案例分析 2019-06-13

PDF PDF 1.55 MB
利用数据分析加速准确、 快速的设计决策
设计工程师们都在争相打造最佳产品,抢占市场先机。为此,他们必须超前做出明智的设计决策。然而,这其中存在许多挑战,譬如工程资源短缺、预算受限,以及需要筛选大量数据来确保他们的设计符合行业和公司的要求。

案例分析 2019-06-11

PDF PDF
利用无线能量采集电路 延长物联网设备的运行寿命
利用无线能量采集电路 延长物联网设备的运行寿命

案例分析 2019-06-11

PDF PDF 2 MB
直流 - 直流转换器测试
直流 - 直流转换器测试

案例分析 2019-06-11

PDF PDF 5 MB
Global EMS Manufacturer Reduces Time to Market Using PathWave Manufacturing Analytics - Case Study
The real time automated result analysis and anomaly detection in Keysight’s PathWave Manufacturing Analytics reduce engineering time and effort significantly, empowering the EMS company to release the product into the market sooner.

案例分析 2019-06-04

PDF PDF 2.09 MB
Quadruples throughput with i3070 4-Module In-Circuit Inline in Automotive Electronics Manufacturing
An Automotive Electronics Manufacturing increases the test throughput more than 50% by using i3070 4-Module Inline In-Circuit System with Dual Board Staging and Throughput Multiplier feature.

案例分析 2019-05-22

PDF PDF 4.96 MB
车载雷达便携式雷达测试节省装配时间
车载雷达便携式雷达测试节省装配时间

案例分析 2019-05-16

PDF PDF 3 MB
5G RF Design Startup Delivers Cutting-Edge GaN/GaAs Devices on Day One
To achieve success in the growing wireless industry, a company must deliver cutting-edge devices at competitive speeds. Doing so requires powerful design and simulation tools that can accurately measure the high frequencies that 5G demands.

案例分析 2019-05-10

PDF PDF 1.97 MB
汽车制造商实现 360º 全方位的雷达设计与测试验证,同时节省 50% 的人力
汽车制造商实现 360º 全方位的雷达设计与测试验证,同时节省 50% 的人力

案例分析 2019-04-25

PDF PDF 2 MB
汽车制造商实现 360º 全方位的雷达 设计与测试验证,同时节省 50% 的 人力
一家领先的豪华汽车制造商最近发现自己面临一个挑战:在设计和测试验证上投入的资源已经达到极限。随着该汽车制造商推出具有自动驾驶功能的新车型,他们需要不断满足日益增长的射频测试要求,以便按照内部设定的时间期限完成任务,同时与行业标准保持一致。

案例分析 2019-04-04

PDF PDF
NTT DOCOMO Gains a Go-to-Market Advantage in 5G with Flexible Channel Sounding - Case Study
As one of the industry’s leading innovators, NTT DOCOMO is working to deploy its 5G mobile network in time for a major athletic event in the summer of 2020 in Tokyo. To define and optimize a network that fulfills on the promise of 5G - without being overdesigned - NTT DOCOMO needed an accurate, reliable and repeatable way to characterize channel propagation.

案例分析 2019-04-01

PDF PDF 2.36 MB
5G 制造商将测试时间缩 短 20 倍
通过与是德科技合作,他们的测试速度提高了 20 倍,资产利用率提高了 10 倍,并且能够轻松地对测试站进行更造。

案例分析 2019-03-26

PDF PDF
Probe Heatmap Visualization Tool Helps EMS Company Pinpoint a Costly Issue - Case Study
This case study demonstrate the success of PathWave Manufacturing Analytics helpung EMS company pinpoint and resolve a costly low first pass yield issue.

案例分析 2019-03-20

PDF PDF 1.97 MB
TestOps 宣言 一个敏捷连贯的设计与测试蓝图
通用数据交换原则、开放 API、卓越的测量技术、可扩展的“随处运行”体系结构 和综合的分析与可视化能力,这一切为我们采用革命性的新方法实现设计与测试紧密配合的工作流程奠定了基础。

案例分析 2019-03-19

PDF PDF
Ericsson and Freiburg U. Design High-Q Power Harvesting Circuit Using ADS
ADS HB was used to explore the design space around the innovative impedance transformation using a high Q quartz crystal resonator to transform the low voltage from the low impedance antenna.

案例分析 2019-03-14

PDF PDF 2.37 MB
University Uses ADS to Create an Impedance Matching Method for Wireless Battery Charging
Learn how NCKU created an impedance matching method for wireless battery charging using Keysight ADS.

案例分析 2019-03-14

PDF PDF 2.27 MB

1 2 3 4 5 6 7 8 9 下一页