Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

1-25 of 407

Sort:
New PXIe Multiport Network Analyzer Speeds Multiport Active Antenna Development - Case Study
Learn how a leading global defense contractor accelerated development of a complex antenna, comprised of multiple Transmit Receive (TR) modules. The use of a multiport PXI Vector Network Analyzer characterized this multiport active antenna without relying on switches.

Case Study 2019-05-20

PDF PDF 2.25 MB
3 Key Challenges Implementing and Testing MIMO and Beamforming in 5G Base Stations and Components
Learn the 3 key challenges that designers must overcome while implementing and testing MIMO and beamforming on 5G base stations and components.

Case Study 2019-05-13

PDF PDF
5G RF Design Startup Delivers Cutting-Edge GaN/GaAs Devices on Day One
To achieve success in the growing wireless industry, a company must deliver cutting-edge devices at competitive speeds. Doing so requires powerful design and simulation tools that can accurately measure the high frequencies that 5G demands.

Case Study 2019-05-10

PDF PDF 1.97 MB
Integrated Photonics Revolutionize Data Center Interconnects
Compared with conventional electrical systems, PICs and silicon photonics technologies enable optical communications at higher volumes with lower costs, greater energy efficiency, and smaller sizes.

Case Study 2019-05-09

PDF PDF
Coherent Optical Transforms Data Center Interconnects
Integrated photonics and new standards such as 400ZR and IEEE 802.3ct drive next-generation data center interconnects.

Case Study 2019-05-02

PDF PDF
Fundamentals of MilCom Digital Modulation Format
Adding complex modulation schemes to military systems boosts scalability, security, and data rates.

Case Study 2019-04-24

PDF PDF
With Data Analytics, Accurate and Faster Design Decisions Follow
The secret to making more informed design decisions comes down to using integrated data analytics software. It allows engineers to work in shorter design cycles, reduce the number of redesigns, and benefit from an integrated design and test workflow that increases productivity and minimizes risk.

Case Study 2019-04-15

PDF PDF
How TestOps Speeds Electronic Design and Test
This white paper highlights the ways that TestOps speeds the design and testing of electronic products thanks to PathWave's connected workflow.

Case Study 2019-04-11

PDF PDF
3 Tactics for Configuring Phase-Coherent RF Signal Generation
Testing multi-antenna systems such as MIMO, beamforming requires a test system capable of providing multiple signals and a constant phase relationship between the signals. This white paper will help you understand phase coherence and why it matters, and offer tactics for generating phase-coherent signals.

Case Study 2019-04-10

PDF PDF
Beyond Operational: LTE and WLAN Boost Military and First Responder Networks
Enabling military and public safety networks to access and share data across enhanced coverage zones

Case Study 2019-04-09

PDF PDF
Prepare for 5G New Radio Conformance Test Challenges
Passing conformance and device acceptance tests is the biggest challenge device and base station companies need to overcome. This white paper provides information that helps when preparing for 5G NR conformance tests.

Case Study 2019-04-08

PDF PDF
NTT DOCOMO Gains a Go-to-Market Advantage in 5G with Flexible Channel Sounding - Case Study
As one of the industry’s leading innovators, NTT DOCOMO is working to deploy its 5G mobile network in time for a major athletic event in the summer of 2020 in Tokyo. To define and optimize a network that fulfills on the promise of 5G - without being overdesigned - NTT DOCOMO needed an accurate, reliable and repeatable way to characterize channel propagation.

Case Study 2019-04-01

PDF PDF 2.36 MB
NTT DOCOMO Gains a Go to Market Advantage in 5G with Flexible Channel Sounding
As one of the industry’s leading innovators, NTT DOCOMO is working to deploy its 5G mobile network in time for a major athletic event in the summer of 2020 in Tokyo. To define and optimize a network that fulfills on the promise of 5G – without being overdesigned – NTT DOCOMO needed an accurate, reliable and repeatable way to characterize channel propagation.

Case Study 2019-04-01

PDF PDF
Evolution of the Connected Healthcare System
Technology in the healthcare industry has evolved tremendously over the last five years. Technology is now compact, faster, and more affordable. It is an expectation that all new healthcare devices and tools are intelligent — with multiple sensors connected wirelessly to each other and the internet. The combination of advances like the internet of things (IoT), artificial intelligence (AI), machine learning (ML), and cloud services impact the changes you see in healthcare today. Learn about four critical technology changes in the healthcare industry today in this white paper.

Case Study 2019-04-01

PDF PDF
First Steps in 5G: Overcoming New Radio Device Design Challenges Series – Part 2
This white paper series explores the issues designers face when working in the millimeter-wave spectrum.

Case Study 2019-03-27

PDF PDF
Probe Heatmap Visualization Tool Helps EMS Company Pinpoint a Costly Issue - Case Study
This case study demonstrate the success of PathWave Manufacturing Analytics helpung EMS company pinpoint and resolve a costly low first pass yield issue.

Case Study 2019-03-20

PDF PDF 1.97 MB
The TestOps Manifesto. A Blueprint for Connected, Agile Design and Test
Explore how TestOps improves design and test workflows. Read about the five key principles for connected, agile design and test, a critical understanding in realizing the full potential and benefits of this powerful new approach.

Case Study 2019-03-19

PDF PDF
Four Measurements on the Go
Learn about four important measurements you can make on the go with the FieldFox Handheld Analyzer, including Noise Figure, Real-Time Spectrum Analysis (RTSA), Cable and Antenna Testing (CAT), and Over-the-Air (OTA).

Case Study 2019-03-14

PDF PDF
Ericsson and Freiburg U. Design High-Q Power Harvesting Circuit Using ADS
ADS HB was used to explore the design space around the innovative impedance transformation using a high Q quartz crystal resonator to transform the low voltage from the low impedance antenna.

Case Study 2019-03-14

PDF PDF 2.37 MB
Automaker Gets a 360 View of Radar Design and Test Validation with 50 Percent Less Manpower
A car maker saved 50% manpower by automating their tracking and fine-tuning systems for autonomous driving radio frequency (RF) tests with the Keysight PathWave laboratory management software.

Case Study 2019-03-14

PDF PDF
University Uses ADS to Create an Impedance Matching Method for Wireless Battery Charging
Learn how NCKU created an impedance matching method for wireless battery charging using Keysight ADS.

Case Study 2019-03-14

PDF PDF 2.27 MB
Ericsson and Freiburg U. Design High Q Power Harvesting Circuit Using ADS
The Internet of Things (IoT) fulfills a promise of a more efficient and connected world. But with dozens of devices per household, battery management must become wireless and autonomous. This problem is now being solved through power harvesting, which enables a circuit to power itself from energy in the environment.

Case Study 2019-03-14

PDF PDF
Automaker Gets a 360 View of Radar Design and Test Validation with 50% Less Manpower - Case Study
A car maker saved 50% manpower by automating their tracking and fine-tuning systems for autonomous driving radio frequency (RF) tests with the Keysight PathWave laboratory management software.

Case Study 2019-03-14

PDF PDF 2.22 MB
University Uses ADS to Create an Impedance Matching Method for Wireless Battery Charging
Learn how NCKU created an impedance matching method for wireless battery charging using Keysight ADS.

Case Study 2019-03-14

PDF PDF
Key Building Blocks of the Internet of Things
Understanding how IoT ecosystems work together to achieve success in the industrial IoT and beyond.

Case Study 2019-03-13

PDF PDF

1 2 3 4 5 6 7 8 9 10 ... Next