这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

缩小范围

去除所有优化

按主题

按内容类型

按产品类别

1-17 / 17

排序:
What is Keysight's Windows 7 to Windows 10 Migration Schedule?
We are beginning the transition of our Windows based instruments from Windows Embedded Standard 7 to Windows 10 IoT Enterprise. Click on the link for additional information.

FAQ 2018-05-07

Can the B01 bundle for the M9703B digitizer support 1 GHz of bandwidth?
No, the AXIe carrier board in the B01 bundle contains different assemblies than the standard M9703B board. Click on the link for additional information.

FAQ 2017-08-01

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced TDD?
The X-Series upgrade path to LTE-Advanced TDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced FDD?
The X-Series upgrade path to LTE-Advanced FDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

M9290A CXA-m PXIe 信号分析仪是否配置跟踪发生器?
M9020A 目前不提供跟踪发生器功能。

FAQ 2014-10-27

我能否升级 M9290A CXA-m PXIe 信号分析仪的频率范围?
不能,M9290A 不支持频率范围升级。

FAQ 2014-10-27

M9330A 有哪些工厂升级选件?
M9330A 工厂升级选件列表。

FAQ 2014-05-18

IO Libraries Suite: How do I obtain a license for the Keysight IO Libraries Suite?
Keysight now allows you to use the IO Libraries Suite, whether or not you have Keysight equipment...

FAQ 2012-10-10

IO Libraries Suite: Can a customer shipped the current version of the Keysight IO Libraries Suite use a previous version?
Yes.

FAQ 2012-10-10

34970A: How do I add a DMM to a 34970A that does not have one installed?
Order the customer installable retrofit kit 34970-80100.

FAQ 2010-10-12

Transferring the license from an older version to version 3.00
Before updating to a new revision of Data Logger on the SAME computer, be certain to save all data and configuration files that you wish to keep.

FAQ 2010-09-19

IO Libraries Suite: What are the differences between Keysight IO Libraries Suite versions 14.0 and 14.1?
The major enhancement that has been added to version 14.1 is compatibility with National Instruments NI-488.2 API or I/O Library.

FAQ 2010-09-08

I see spikes at the U2351A/U2353A's Analogue Output when Analogue Input is turned on and its frequency changes according to the AI sampling.
There is a spike on the U2351A/U2353A's Analogue Output when Analogue Input is turned on because....

FAQ 2010-08-09

Why is my acquired data for U2300A and U2500A shifted? eg. Column 2 data is in column 1, column 3 data is in column 2, and so on.
Install DAQ hardware driver version 1.05 and above.

FAQ 2010-08-09

When I sent commands using VISA (Both Keysight VISA and NI VISA), why must i put '\n' or '\r' after the commands for U2600A…
Please upgrade your U2600A firmware to version 1.05 or above

FAQ 2010-08-09

如何才能将34980A更新到固化软件版本2.19?

FAQ 2007-11-04

Are the E840x mainframes both deeper and taller than the E8401B?
The E8401B is 631mm (24.9") deep compared to the E1401B which is 602mm (23.7") deep.

FAQ 2002-08-14