Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

Уточнить список

убрать все фильтры

По теме

По типу содержания

По типу оборудования

1-25 из 50

Упорядочить:
What is the phase noise sensitivity of the E5052B with E5053A and 11970 Mixers?
Please refer to this document.

FAQ 2016-03-29

Where can I find manuals for discontinued and obsolete Hewlett-Packard, Agilent and Keysight test equipment?
Most Keysight products have PDF manuals that can be found on product pages. Other vendors also supply old manuals.

FAQ 2014-08-01

How can I get correct Log Frequency Scale Trace Data Using IntuiLink or BenchVue with my ESA Series Spectrum Analyzer?
Save the trace as a .csv file

FAQ 2014-03-13

How often does the system user alignment for the PSA EMI Measurement Receiver need to be run?
30 days or 3° C temperature change. See contents for details...

FAQ 2012-12-11

Do I need to perform a periodic front panel instrument alignment on my N9039A RF Preselector?
No, but there is a system alignment that needs to be periodically run. See FAQ content for details...

FAQ 2012-12-11

Is the N9068A phase noise application supported by N9030A PXA Option EXM external mixing?
Yes, the N9068A phase noise application is supported when using N9030A PXA Option EXM external mixing. In addition, Option EXM supports normal spectrum analyzer applications, including PowerSuite one-button measurements.

FAQ 2012-10-25

Why does my PSA EMI Measurement Receiver tell me that I need to run the user alignment everyday?
There are a couple of reason why this could be hapening. See FAQ contents for details...

FAQ 2012-03-16

Why does my signal go off the top of the screen when I select either the Quasi-Peak or EMI Average detectors in my EMC or ESA analyzer?
Your instrument firmware may need to be updated to fix an auto ranging problem....

FAQ 2012-03-16

Why don't the Measure at Marker or Auto Measure peak detector values match the peak trace marker values on my EMC analyzer?
Your instrument firmware may need to be updated....

FAQ 2012-03-16

How do I erase/clear the user data in an ESA or EMC series spectrum analyzer for security reasons?
Follow this link for further information....

FAQ 2012-03-16

What does the system user alignment of my PSA EMI Measurement Receiver do?
See contents for details...

FAQ 2012-03-16

What should I do if the system user alignment of my PSA EMI Measurement Receiver fails?
This could be caused by a few different reasons. See contents for details...

FAQ 2012-03-16

How long does the system user alignment of my PSA EMI Measurement Receiver take to run?
A full system alignment takes approx. 30 minutes. See FAQ content for further details...

FAQ 2012-03-16

How do I transfer the time capture buffer data from my 89441A or 89410A VSA to a PC?
There are several ways to transfer the data in the time capture buffer after a recording has been made. The easiest way is to use FTP over LAN, but there are other programmatic ways too.

FAQ 2012-03-02

What is the frequency range of the N5532A Sensor Module?
100 kHz to 4.2 GHz, 10 MHz to 18 GHz, 30 MHz to 26.5 GHz, and 30 MHz to 50 GHz.

FAQ 2012-02-26

Why do spurious signals appear in my spectrum analyzer span when I apply a clean signal to the RF input?
Overdriving the input mixer of the analyzer may cause the spurs.

FAQ 2012-02-26

What is the frequency coverage of the N5532A/N5532B sensor module? What options would my PSA Analyzer require to operate in an N5531S?
The N5532A/N5532B is offered in four optional frequency ranges. All models can measure power from -20 dBm to +30 dBm.

FAQ 2012-02-26

What is the frequency range of the N5532B Sensor Module?
100 kHz to 4.2 GHz, 10 MHz to 18 GHz, 30 MHz to 26.5 GHz, and 30 MHz to 50 GHz.

FAQ 2012-02-26

How can I transfer trace data from the 89400 VSA to my PC?
The VSA always saves data in standard data format; the utility is run from the DOS prompt.

FAQ 2012-02-25

What is the relationship between the Error Vector Magnitude and the Signal to Noise Ratio for a 64-QAM signal?
EVM is a voltage ratio of the error signal to the peak state voltage and SNR is a ratio of the signal power to the error power. The equation relating them is...

FAQ 2012-02-25

How does the 89400 series vector signal analyzer (VSA) lock to the symbols when it demodulates a vector-modulated signal?
There is no coherent carrier or symbol clock timing signal required for demodulation. The actual demodulation algorithm is proprietary, but...

FAQ 2012-02-25

How do I save my trace data in a comma-separated variable (.csv) file format on an ESA, PSA or EMC spectrum analyzer?
On the front panel of the analyzer, press [File]{Save} and select either the A: (floppy) or C: (internal) drive...

FAQ 2012-02-24

What are the differences between an E7400A Series EMC Analyzer and an ESA Series Spectrum Analyzer with Option AYQ - EMI Detectors & FM Demod?
See table provided....

FAQ 2011-07-07

What signal sources are support for use as an alignment source for the PSA / N9039A RF Preselector based system?
8648B / N5181A / N5182A / N5183A/ N5161A / N5162A / E4438C / E8257D

FAQ 2010-09-08

Why is the marker Count Accuracy on the on the ESA Series Spectrum Analyzer only specified when using resolution bandwidths >1KHz?
If more that one signal is present in the 1kHz span, the marker count will be incorrect.

FAQ 2010-09-08

1 2 Следующие