이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

상세 분류

상세분류 제거

주제별

분야별 검색결과

제품 카테고리별

1-25 / 50

정렬방식:
Is it possible to get an error log of incorrectly sent remote commands to my PSA, E4406A, EMC, or ESA Series Spectrum Analyzer?
Yes. PSA, E4406A and the ESA Series (with firmware A.08.00 and later) support this. You may turn Verbose error logging on through the front panel or remotely, SYST:ERR:VERBOSE ON

FAQ 2016-07-05

E5053A 및 11970 믹서를 포함한 E5052B의 위상 노이즈 감도란 무엇입니까?
이 문서를 참조하십시오.

FAQ 2016-03-29

키사이트, 애질런트 및 휴렛팩커드의 단종된 테스트 장비에 대한 매뉴얼은 어디에서 확인할 수 있습니까?
대부분의 키사이트 제품의 PDF 매뉴얼은 제품 페이지에서 확인하실 수 있습니다. 다른 벤더들도 예전 매뉴얼을 제공합니다.

FAQ 2014-08-01

How can I get correct Log Frequency Scale Trace Data Using IntuiLink or BenchVue with my ESA Series Spectrum Analyzer?
Save the trace as a .csv file

FAQ 2014-03-13

How often does the system user alignment for the PSA EMI Measurement Receiver need to be run?
30 days or 3° C temperature change. See contents for details...

FAQ 2012-12-11

Do I need to perform a periodic front panel instrument alignment on my N9039A RF Preselector?
No, but there is a system alignment that needs to be periodically run. See FAQ content for details...

FAQ 2012-12-11

PXA의 External Mixing Mode에서 Phase Noise 측정이 가능합니까?
예, 가능합니다.

FAQ 2012-10-25

Why does my signal go off the top of the screen when I select either the Quasi-Peak or EMI Average detectors in my EMC or ESA analyzer?
Your instrument firmware may need to be updated to fix an auto ranging problem....

FAQ 2012-03-16

Why don't the Measure at Marker or Auto Measure peak detector values match the peak trace marker values on my EMC analyzer?
Your instrument firmware may need to be updated....

FAQ 2012-03-16

How do I erase/clear the user data in an ESA or EMC series spectrum analyzer for security reasons?
Follow this link for further information....

FAQ 2012-03-16

How long does the system user alignment of my PSA EMI Measurement Receiver take to run?
A full system alignment takes approx. 30 minutes. See FAQ content for further details...

FAQ 2012-03-16

Why does my PSA EMI Measurement Receiver tell me that I need to run the user alignment everyday?
There are a couple of reason why this could be hapening. See FAQ contents for details...

FAQ 2012-03-16

What does the system user alignment of my PSA EMI Measurement Receiver do?
See contents for details...

FAQ 2012-03-16

What should I do if the system user alignment of my PSA EMI Measurement Receiver fails?
This could be caused by a few different reasons. See contents for details...

FAQ 2012-03-16

How do I transfer the time capture buffer data from my 89441A or 89410A VSA to a PC?
There are several ways to transfer the data in the time capture buffer after a recording has been made. The easiest way is to use FTP over LAN, but there are other programmatic ways too.

FAQ 2012-03-02

Why do spurious signals appear in my spectrum analyzer span when I apply a clean signal to the RF input?
Overdriving the input mixer of the analyzer may cause the spurs.

FAQ 2012-02-26

What are the differences between an E7400A Series EMC Analyzer and an ESA Series Spectrum Analyzer with Option AYQ - EMI Detectors & FM Demod?
See table provided....

FAQ 2011-07-07

PSA 와 N9039A alignment 를 지원할수 있는 시그날제너레이터는 무엇인가요?
8648B/N5181A/N5182A/N5183A/N5161A/N5162A/E4438C/E8257D 입니다.

FAQ 2011-04-26

다양한 네트워크 분석기 및 임피던스 분석기에 대한 호환 가능한 프린터의 마스터 목록이 있습니까?

FAQ 2010-09-27

Why is the marker Count Accuracy on the on the ESA Series Spectrum Analyzer only specified when using resolution bandwidths >1KHz?
If more that one signal is present in the 1kHz span, the marker count will be incorrect.

FAQ 2010-09-08

N5532B 센서 모듈의 주파수 범위는?
100kHz~4.2GHz, 10MHz~18GHz, 30MHz~26.5GHz 및 30MHz~50GHz.

FAQ 2010-04-29

N5532A 센서 모듈의 주파수 범위는 어떻게 됩니까?
100kHz~4.2GHz, 10MHz~18GHz, 30MHz~26.5GHz 및 30MHz~50GHz.

FAQ 2010-04-13

N5532A/N5532B 센서 모듈의 주파수 범위는 어떻게 됩니까? 내가 구입한 PSA 시리즈 스펙트럼 분석기가 N5531S 측정 수신기에서 작동하려면 어떤 옵션이 필요합니까?
자세한 내용을 보려면 여기를 클릭하십시오.

FAQ 2010-04-13

How do I enter my own antenna correction factors on the ESA or EMC Series Analyzer?
Access the AMPLITUDE, More, Corrections menu.

FAQ 2008-11-21

Is it OK to connect both AC and DC power sources to my ESA Series Spectrum Analyzer simultaneously?
No, damage to the instrument or the 12Vdc source may occur!!

FAQ 2008-11-21

1 2 다음