検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

テクニカルサポート

電子計測

製品番号で検索:

1-25 / 51

並べ替え
E5053Aおよび11970ミキサーと組み合わせて使用した場合のE5052Bの位相雑音感度とは?
このドキュメントを参照してください。

FAQ 2016-03-29

既に販売が完了したKeysight、AgilentおよびHewlett-Packard(HP)のテスト機器のマニュアルはどのように入手できますか?
ほとんどのKeysight製品にPDFマニュアルがあり、製品ページで入手することができます。Keysightのベンダも古いマニュアルを提供しています。

FAQ 2014-08-01

IntuiLinkまたはBenchVueをESAシリーズ スペクトラム・アナライザと組み合わせて使用して、正しいログ周波数スケール・トレース・データを得るには?
トレースを.csvファイルで保存します

FAQ 2014-04-23

How often does the system user alignment for the PSA EMI Measurement Receiver need to be run?
30 days or 3° C temperature change. See contents for details...

FAQ 2012-12-11

Do I need to perform a periodic front panel instrument alignment on my N9039A RF Preselector?
No, but there is a system alignment that needs to be periodically run. See FAQ content for details...

FAQ 2012-12-11

N9068A位相雑音アプリケーションは、N9030A PXAオプションEXM外部ミキサによってサポートされますか?
はい。N9068A位相雑音アプリケーションは、N9030A PXAオプションEXM外部ミキサの使用時にサポートされています。オプションEXMは、PowerSuiteワンボタン測定などの一般的なスペクトラム・アナライザ・アプリケーションもサポートしています。

FAQ 2012-10-25

Why does my signal go off the top of the screen when I select either the Quasi-Peak or EMI Average detectors in my EMC or ESA analyzer?
Your instrument firmware may need to be updated to fix an auto ranging problem....

FAQ 2012-03-16

Why don't the Measure at Marker or Auto Measure peak detector values match the peak trace marker values on my EMC analyzer?
Your instrument firmware may need to be updated....

FAQ 2012-03-16

How long does the system user alignment of my PSA EMI Measurement Receiver take to run?
A full system alignment takes approx. 30 minutes. See FAQ content for further details...

FAQ 2012-03-16

Why does my PSA EMI Measurement Receiver tell me that I need to run the user alignment everyday?
There are a couple of reason why this could be hapening. See FAQ contents for details...

FAQ 2012-03-16

What does the system user alignment of my PSA EMI Measurement Receiver do?
See contents for details...

FAQ 2012-03-16

What should I do if the system user alignment of my PSA EMI Measurement Receiver fails?
This could be caused by a few different reasons. See contents for details...

FAQ 2012-03-16

Why do spurious signals appear in my spectrum analyzer span when I apply a clean signal to the RF input?
Overdriving the input mixer of the analyzer may cause the spurs.

FAQ 2012-02-26

How do I save my trace data in a comma-separated variable (.csv) file format on an ESA, PSA or EMC spectrum analyzer?
On the front panel of the analyzer, press [File]{Save} and select either the A: (floppy) or C: (internal) drive...

FAQ 2012-02-24

What signal sources are support for use as an alignment source for the PSA / N9039A RF Preselector based system?
8648B / N5181A / N5182A / N5183A/ N5161A / N5162A / E4438C / E8257D

FAQ 2010-09-08

Why is the marker Count Accuracy on the on the ESA Series Spectrum Analyzer only specified when using resolution bandwidths >1KHz?
If more that one signal is present in the 1kHz span, the marker count will be incorrect.

FAQ 2010-09-08

N5532Bセンサ・モジュールの周波数レンジは?
100 kHz~4.2 GHz、10 MHz~18 GHz、30 MHz~26.5 GHz、30 MHz~50 GHzです。

FAQ 2010-04-29

N5532Aセンサ・モジュールの周波数レンジはどれ位ですか?
100 kHz~4.2 GHz、10 MHz~18 GHz、30 MHz~26.5 GHz、30 MHz~50 GHzです。

FAQ 2010-04-25

N5532A/N5532Bセンサ・モジュールの周波数レンジは?PSAシリーズ・スペクトラム・アナライザをN5531S測定レシーバで使用するには、どのオプションが必要ですか?
詳細はこちらをクリックしてください。

FAQ 2010-04-25

How do I enter my own antenna correction factors on the ESA or EMC Series Analyzer?
Access the AMPLITUDE, More, Corrections menu.

FAQ 2008-11-21

Is it possible to get an error log of incorrectly sent remote commands to my PSA, E4406A, EMC, or ESA Series Spectrum Analyzer?
Yes. PSA, E4406A and the ESA Series (with firmware A.08.00 and later) support this. You may turn Verbose error logging on through the front panel or remotely, SYST:ERR:VERBOSE ON

FAQ 2008-11-21

Is it OK to connect both AC and DC power sources to my ESA Series Spectrum Analyzer simultaneously?
No, damage to the instrument or the 12Vdc source may occur!!

FAQ 2008-11-21

When should I press "Discharge DC Block Capacitor" softkey of the E5052B?
It is recommended to press this softkey when reconnecting the DUT at the baseband input port of the E5052B.

FAQ 2008-10-22

Why does the built-in speaker of my E7400A EMC and ESA Analyzer appear to cut out while demodulating signals?
This is due to the internal auto alignment routine...

FAQ 2008-10-09

Is there any way to reduce the intensity of the display on an ESA or EMC spectrum analyzer if it must be left on for long periods of time?
Not via the Front Pannel but can be done using a SCIPI command. See text...

FAQ 2008-10-09

1 2 3 次へ