您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

1-25 / 104

排序:
What is Keysight's Windows 7 to Windows 10 Migration Schedule?
We are beginning the transition of our Windows based instruments from Windows Embedded Standard 7 to Windows 10 IoT Enterprise. Click on the link for additional information.

FAQ 2019-08-28

FieldFox Manuals, Firmware, Software and Product Support
Manuals, firmware upgrade, software trials & upgrade and support page for FieldFox analyzers

FAQ 2018-11-14

Does the noise figure application on the PNA-X (option 029) provide a full noise-parameter system (tuners and software)?
No, we don’t provide a full noise-parameter system. Click on the question for additional information.

FAQ 2017-06-28

Is there a software application for the 8714ES to calculate K factor?
No, there is not a software application to calculate K factor for the 8714ES.

FAQ 2017-06-28

Is there a software application for the E5062A to calculate K factor?
No, there is not a software application to calculate K factor for the E5062A.

FAQ 2017-06-28

Can the PNA-X be configured to install Windows updates as they are pushed out by Microsoft?
Yes, any Windows based machine can be configured to install Windows updates.

FAQ 2017-06-28

Can antivirus programs run on the Windows based PNA-X?
Yes, antivirus programs can run on any Windows based machine.

FAQ 2017-06-28

What is the difference of software options between M9485A and PNA/ENA series VNA?
There is no difference for option 007/009/010. There are some differences for options 025, 028, 086 and 551.

FAQ 2017-05-25

FieldFox 有沒有 GPS 接收器?
從 A.05.33 版本韌體開始,FieldFox 分析儀便已添加了 GPS 功能。

FAQ 2017-01-23

Microsoft 不再支援 Windows XP 對我的 ENA 有何影響?
Microsoft 於 2014 年 4 月 8 日停止對 Windows XP 作業系統的支援。請閱讀此頁面以了解我們對此問題的解答。

FAQ 2015-07-27

CPU / 儲存類型 / Windows OS 歷史紀錄
表格中列出過去的CPU類型/記憶體容量、儲存類型/容量、windows OS。

FAQ 2014-04-28

能否使用 USB 記憶體來更新 ENA 的韌體?
此支援能力因機種而異

FAQ 2012-12-28

是否可在 ENA 中關閉或開啟 Windows 的自動登錄功能?
有, 為了在無域系统中關閉或開啟Windows 的自動登錄功能,請執行以下步驟:

FAQ 2012-12-27

How can I check for the computer viruses on the ENA?
It depends on the model...

FAQ 2012-12-11

Can I install extra applications on the ENA?
It depends on the model...

FAQ 2012-12-11

How Can I Find What I Need in a Signal Analyzer Recording Faster?
If you have a very long Signal Analyzer recording, it is sometimes difficult to find the area of interest. There is no really good tool for this problem at this time, but here are some suggestions.

FAQ 2012-08-17

Why won't my Signal Analyzers Display Pulse Type Signals Properly?
These signals may be missed if the Sweep Acquisition setting is on Auto. We recommend using a Sweep Acquisition setting of 50 or 100 for GSM signals.

FAQ 2012-08-15

Which is Most Accurate: CalReady, QuickCal (Without Load), or 2 Port Calibration?
When nothing connected at the end of RF port, CalReady is the most accurate calibration method at test port.

FAQ 2012-08-15

Opt.100 VBA utility programs do not run properly. What is wrong?

FAQ 2012-08-09

Keysight ENA-L是否支援類似871x系列的內建網頁?

FAQ 2011-10-07

常見問答集 (FAQ)
常見問答集 (FAQ)

FAQ 2011-10-07

The ENA / ENA-L was infected with the virus. What should I do?
Remove the LAN cable and perform system recovery.

FAQ 2011-10-07

Firmware Upgrades via the Web

FAQ 2011-02-15

8720的升級

FAQ 2010-11-20

ENA/ENA-L does not go directly to the instrument mode after power on, but shows the password dialog box or the windows desktop. How do I fix it?
This is because the user registration was improperly done when the first time the power was turned on. Performing system recovery is recommended to fix it.

FAQ 2010-07-02

1 2 3 4 5 下一頁