検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

テクニカルサポート

電子計測

製品番号で検索:

1-25 / 246

並べ替え
What is Keysight's Windows 7 to Windows 10 Migration Schedule?
We are beginning the transition of our Windows based instruments from Windows Embedded Standard 7 to Windows 10 IoT Enterprise. Click on the link for additional information.

FAQ 2020-09-08

What software and options do I need to access the FPGA sandbox in my high-speed digitizer?
Digitizer option FDK enables programming access to the on-board FPGA. Click on the question for additional information.

FAQ 2020-02-06

What is the CPU / Storage / Windows OS history?
The history of CPU type/memory size, storage type/size, windows OS is listed in the table.

FAQ 2018-08-21

Xシリーズ モジュール計測器用のXシリーズ測定アプリケーションの30日間無料試用ライセンス
Xシリーズ モジュラー・シグナル・アナライザ用Xシリーズ 測定アプリケーションの30日間無料試用ライセンス。

FAQ 2018-07-25

ベンチトップ/モジュラー/ハンドヘルドモデルのシグナル・アナライザ/スペクトラム・アナライザのファームウェア・アップデート・センター
ベンチトップ/モジュラー/ハンドヘルドモデルのシグナル/スペクトラム・アナライザのファームウェア/ソフトウェアの最新バージョンを利用するために。

FAQ 2018-05-17

Is there a software application for the 8714ES to calculate K factor?
No, there is not a software application to calculate K factor for the 8714ES.

FAQ 2017-06-28

Is there a software application for the E5062A to calculate K factor?
No, there is not a software application to calculate K factor for the E5062A.

FAQ 2017-06-28

Is calibration included in the 86100DU-WN7 Windows 7 upgrade?
86100DU-WN7 is a return to service center upgrade and does include calibration, in addition to a certificate of calibration and data.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced TDD?
The X-Series upgrade path to LTE-Advanced TDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

Does the noise figure application on the PNA-X (option 029) provide a full noise-parameter system (tuners and software)?
No, we don’t provide a full noise-parameter system. Click on the question for additional information.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced FDD?
The X-Series upgrade path to LTE-Advanced FDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

Can antivirus programs run on the Windows based PNA-X?
Yes, antivirus programs can run on any Windows based machine.

FAQ 2017-06-28

Can the PNA-X be configured to install Windows updates as they are pushed out by Microsoft?
Yes, any Windows based machine can be configured to install Windows updates.

FAQ 2017-06-28

What is the difference of software options between M9485A and PNA/ENA series VNA?
There is no difference for option 007/009/010. There are some differences for options 025, 028, 086 and 551.

FAQ 2017-05-25

M8000シリーズの30日間の無料試用ライセンス
M8000製品シリーズのすべての試用ライセンスへのリンクおよび概要

FAQ 2017-01-30

【VSA】【SG】RF信号をキャプチャして信号源で再生することはできますか?
はい。ベクトル・シグナル・アナライザを使用することで、RFキャプチャ信号を信号源から再生することが可能です。

FAQ 2016-02-03

Why 34405A can't be detected in Windows 7?
There are two posibilities causing 34405A couldn't be detected. 1. IO Libraries Suit 15.1 or below...

FAQ 2015-09-21

How to enable 34410A/34411A/L4411A browser web control work in Java 8?
To enable browser web control to work in Java 8, update instrument to firmware version 2.41...

FAQ 2015-09-21

Microsoft社によるWindows XPのサポート終了は、ENAにどのような影響を及ぼしますか?
Microsoft社は、2014年4月8日にWindows XPオペレーティング・システムのサポートを終了しました。このドキュメントは、いくつかの重大な疑問に答えます。

FAQ 2015-07-27

Is U2700A series USB Modular Instruments supported in Linux environment?
No. U2700A Series are not supportable in Linux environment. The drives for USB Modular only build for Microsoft Windows.

FAQ 2014-11-25

M9290A CXA-m PXIeシグナル・アナライザは、スペクトラム解析用の掃引モードをサポートしていますか?
はい。M9290Aは、スペクトラム解析用の掃引モードとFFTモードをサポートしています。

FAQ 2014-09-11

Xシリーズ・シグナル・アナライザ・ソフトウェア・アップデート
ソフトウェア・アップデート、Xシリーズ・シグナル・アナライザ(PXA/MXA/EXA/CXA/MXE)

FAQ 2014-08-14

Microsoft社によるWindows XPのサポート終了は、E5052Bにどのような影響を及ぼしますか?
Microsoft社は、2014年4月8日にWindows XPオペレーティング・システムのサポートを終了しました。このドキュメントは、いくつかの重大な疑問に答えます。

FAQ 2014-08-01

従来のUIを備えたX-シリーズ シグナル・アナライザ用X-シリーズ 測定アプリケーションの30日間無料試用版
X-シリーズ シグナル・アナライザ用X-シリーズ 測定アプリケーションの30日間無料試用ライセンス。

FAQ 2014-08-01

Microsoft社によるWindows XPのサポート終了は、E4982Aにどのような影響を及ぼしますか?
Microsoft社は、2014年4月8日にWindows XPオペレーティング・システムのサポートを終了しました。このドキュメントは、いくつかの重大な疑問に答えます。

FAQ 2014-05-23

1 2 3 4 5 6 7 8 9 10 次へ