这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

1-25 / 72

排序:
FlexDCA: What Licenses Do I Have, And What Features Do They Enable?
FlexDCA: What Licenses Do I Have, And What Features Do They Enable?

FAQ 2018-12-10

What software and options do I need to access the FPGA sandbox in my high-speed digitizer?
Digitizer option FDK enables programming access to the on-board FPGA. Click on the question for additional information.

FAQ 2018-01-18

Why has Keysight changed the N9069C licensing structure model?
The N9069C licensing structure model has been collapsed as a customer ordering convenience. Click on the question for additional information.

FAQ 2017-06-28

Is Option RTS a license key or hardware upgrade?
Option RTS is a hardware and license key upgrade. Therefore, this upgrade requires the analyzer to be returned to Keysight.

FAQ 2017-06-28

Is it possible to add the N9080B-2TP with the N9080B-1FP installed on the X-Series Analyzer? Should the N9080B-2FP be used instead?
Yes, this is possible. A combination of fixed and transportable licenses can be used.

FAQ 2017-06-28

Where can I get current and previous software versions as well as updates of MBP and/or MQA?
Current and previous software versions of Model Builder Program (MBP) and/or Model Quality Assurance (MQA) can be found in the Knowledge Center.

FAQ 2017-04-03

Where can I find product documentation for MBP and MQA?
Product documentation for Model Builder Program (MBP) and/or Model Quality Assurance (MQA) can be found in the Knowledge Center.

FAQ 2017-04-03

How do I renew an expired MBP or MQA license?
General information on renewing an expired Model Builder Program (MBP) or Model Quality Assurance (MQA) license.

FAQ 2017-04-03

如何找到免费试用?
免费试用设计和测试软件。为您的应用寻找免费试用的软件。

FAQ 2014-08-14

How does the 89601BU "update and subscription service" work?
Option 200 is mandatory and you cannot use the 89600 VSA software without having Option 200 installed. Software version.....

FAQ 2014-01-27

什么是 Keysight EEsof EDA 知识中心?
知识中心是对是德现有网站的一大改进,可提供更多的文档和实例。

FAQ 2013-11-10

如何辨别我的 N9030A PXA 信号分析仪是否获得了选件 B1X、B1Y 和 MPB 的许可证?
您可以检查在仪器上安装了哪些选件,首先按下 [System] 硬件,再按下 {Show} 功能键,最后按下 {System} 功能键。

FAQ 2013-08-07

什么是 30 天免费试用许可证?如何使用?
30 天免费试用期可以让用户在购买前试用最新的 Signal Studio 软件产品

FAQ 2013-03-28

激活 30 天试用许可证后,是否可以暂停试用期以备将来使用?
不可以。试用许可证激活后仅在连续的 30 天内有效。试用结束后,您必须购买永久许可证才能继续使用该软件。

FAQ 2013-03-28

试用许可证是否可以在 30 天试用期满后续期或延长有效期?
仪器的试用许可证到期后不可以续期或延长有效期。

FAQ 2013-03-28

如果我已经为一台信号发生器购买了许可证,此许可证是否可以在信号发生器之间转移?
可以,是德新的许可证模式目前提供可转移许可证。

FAQ 2013-03-28

如何跟踪试用许可证的剩余时间?
要跟踪试用许可证的剩余时间,您可以在 ESG/PSG 前面板依次按下 Utility(实用工具) > Instrument Adjustments(仪器调节)> Instrument Options(仪器选件)> Waveform Licenses(波形许可证)。

FAQ 2013-03-28

如何启用 30 天免费试用许可证?
若要获取 Signal Studio B 型(例如 N7615B)的试用许可证,请下载 Signal Studio 软件并访问该型号对应的是德软件许可证试用许可证申请页面。

FAQ 2013-03-28

Why do I need to pay installation/calibration charges for N4010A license-only upgrades?
The N4010A has several license-only upgrade paths, most of which enhance the base technology options that are already enabled in the unit. Click on the question above for a fuller description.

FAQ 2013-02-06

When I use the 30-day trial license of the Signal Studio for WiMAX™, how can I check the number of days remaining on temporary license?
Press the front panel keys: Utility > Instrument Adjustments > Instrument Options > Waveform Licenses

FAQ 2013-01-28

I lost my E5500 Phase Noise System license key. How do I obtain a permanent replacement license key?
In order to obtain a permanent replacement phase noise system license key the phase detector test set (70420A or N5500A) serial number is required.

FAQ 2012-12-20

For waveform 5-pack licenses, what alternatives are available for customers that require additional waveform evaluation time after the initial 30-d...

FAQ 2012-12-13

For waveform 5-pack licenses, can the customer download a waveform generated with the 30-day license?
Yes, if a waveform was created using the 30-day trial, it can be downloaded to any MXG/ESG with unused waveform 5-pack license slots.

FAQ 2012-12-11

Is there a 30-day trial license for this application?
Only selected Signal Studio software applications have the 30-day free trial license available, while others allow a free evaluation of the software interface only.

FAQ 2012-12-11

What do the N7620B upgrade licenses cost?
All N7620B license upgrades are free.

FAQ 2012-10-28

1 2 3 下一页