这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

1-25 / 513

排序:
FieldFox Manuals, Firmware, Software and Product Support
Manuals, firmware upgrade, software trials & upgrade and support page for FieldFox analyzers

FAQ 2018-11-14

Where can I find the user documentation for the U5340A FPGA Development Kit (FDK)?
The user documentation is installed on your computer with the software.

FAQ 2018-01-18

Can the U4431A MIPI M-PHY protocol analyzer be controlled from an external PC via the AXIe mainframe's USB port?
Yes, the USB connected chassis option (M9502A-U20/M9505A-U20) is a viable connection strategy when using the U4431A M-PHY Protocol Analyzer instrument.

FAQ 2016-07-08

Why isn’t the unit being discovered by VSA software hosted inside the instrument itself?
Check to see if Keysight Technologies is returned from the analyzer as part of the *IDN query.

FAQ 2016-07-08

Does FieldFox support data-based cal kits?
FAQ for FieldFox support of Cal Kits

FAQ 2015-09-09

When automating markers on the ENA is it possible to programmatically query the indicated inductance or capacitance on a Smith Chart?
The inductance / capacitance information cannot be directly queried via the automation interfaces. The inductance (positive reactance, top half of the Smith Chart) or capacitance (negative reactance, lower half of the Smith Chart) is not available as an automation query.

FAQ 2014-08-11

How can I get correct Log Frequency Scale Trace Data Using IntuiLink or BenchVue with my ESA Series Spectrum Analyzer?
Save the trace as a .csv file

FAQ 2014-03-13

How can I save my log plot data to a CSV file type when using the option 226 Phase Noise personality on the PSA or ESA?
In the Phase Noise personality, the log plot data can only be saved as a binary file with the .lpt extension.

FAQ 2014-01-31

On the Keysight NFA Series of Noise Figure Analyzers, is it possible to query the RF attenuator range while in the auto range mode?
The command to query the Keysight NFA RF attenuator while in the auto ranging mode is: DIAG:BLU:RF:RANG?

FAQ 2014-01-31

Which currently available power meters are compatible with the 8753E network analyzer?
In order to work with the 8753E network analyzer, your power meter must emulate either the 436A, 437B, 438A E4418A or the E4419A power meter. Keysight is no longer selling those power meters. However, the E4418B (formerly named the EPM-441A) and E4...

FAQ 2013-11-17

Does Keysight VEE 9.0 support Windows 7?
Yes. A Keysight VEE patch is currently in development and is tentatively scheduled for release on 2nd quarter of 2010.

FAQ 2013-11-17

Can I use a normal USB cable for datalogging with the U1250A Series Handheld Digital Multimeters?
No, you cannot use a normal USB cable for datalogging with the U1250A Series Handheld Digital Multimeters…..

FAQ 2013-11-17

Can HyperTerminal be used with the 34405A Digital Multimeter?
No, HyperTerminal cannot be used with the 34405A Digital Multimeter….

FAQ 2013-11-17

Can I export the data saved in the U1602A/U1604A Handheld Oscilloscope's internal memory to my PC?
No, you cannot export the data saved in the U1602A/U1604A Handheld Oscilloscope's internal memory to your PC....

FAQ 2013-11-17

Can HyperTerminal be used with the U1251A/U1252A Handheld Digital Multimeter?
No, HyperTerminal cannot be used with the U1251A and U1252A Digital Multimeter….

FAQ 2013-11-17

Can I save the image of Meter or Logger mode to the internal memory of my U1602A/U1604A Handheld Oscilloscope?
No, you cannot save your Meter or Logger data to the internal memory nor the USB Flash Memory (for option-001) of your U1602A/U1604A....

FAQ 2013-11-17

How do I use the Service Request method (SRQ) to determine if the X-Series, ESA and PSA Signal Analyzers measurement is complete or has an error me...
Click here for information on the Service Request query to determine when a measurement is complete.

FAQ 2013-06-25

如何对频谱或矢量信号分析仪进行远程编程?
下面的信息可能会给您对是德频谱分析仪进行远程编程提供有益的帮助。

FAQ 2013-05-16

What USB storage devices are compatible with the MXG?
The MXG is now compatible with most USB storage devices.

FAQ 2013-03-13

怎样在53131/32A或53181A计数器上配置RS-232、以进行交互?
没有一种计数器能在RS-232上通信。

FAQ 2013-02-07

怎样把迹线图像捕获到Keysight 8712ES/ET和8714ES/ET矢量网络分析仪的软盘上?
8712ES/ET和8714ES/ET矢量网络分析仪支持使用软盘驱动器保存HPGL、PCX、PCL5和GIF图像。

FAQ 2013-01-04

Is it possible to programmatically receive the displayed low/high stimulus values when using the "CALC1:MARK:BWID:DATA?" bandwidth query results?
When manually configuring the ENA network analyzer via the Marker – Marker Search – Bandwidth ON, the manual process results in low and high stimulus values as displayed on the analyzer’s front panel.

FAQ 2012-12-20

Where is the cfunc.h header file called for in the 33120A Users Guide example program?
Some older versions of the IB Libraries provided this header file during installation. This file was required to access commands from the IB command library.

FAQ 2012-09-05

当进行 TME 软件调整时,如何才能避免“缓冲区溢出”?
在 FieldFox 分析仪和 PC 之间使用交叉电缆直接进行连接。

FAQ 2012-06-01

我能在 FieldFox 上使用局域网连接吗?
可以。请阅读情景介绍。

FAQ 2012-06-01

1 2 3 4 5 6 7 8 9 10 ... 下一页