Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

Refine the List

remove all refinements

By Topic

By Type of Content

By Product Category

176-200 of 418

Sort:
Does 6000L Series oscilloscope require extra rack mount kit?
No. There are front-panel brackets and rack rails included as part of the product to attach it to the rack securely.

FAQ 2007-11-02

Can I use the oscilloscope while the battery is being charged?
Yes, the battery automatically recharges when the scope is connected to AC line power.

FAQ 2007-11-02

Is the battery option retrofitable to previously purchased oscilloscope?
No. The battery option for the 6000 Series is a factory-installed option which is not retrofitable to previously purchased oscilloscopes.

FAQ 2007-11-02

What digital probe cables and accessories are available for Keysight mixed-signal oscilloscopes (MSOs)?
The digital probe kit for all Keysight 6000-series and 54620/40-series MSOs is P/N 54620-61801. The digital probe kit for all 8000-series and 54830-series MSOs is P/N 54826-68701.

FAQ 2007-08-10

What probes are available for my logic analyzer?
Keysight offers the following four basic categories of logic analyzer probes...

FAQ 2007-06-01

How do I update the Scope Connect software and 3000 Series oscilloscope firmware?
Follow these instructions.

FAQ 2007-04-26

Why won't my LaserJet printer print from the oscilloscope's USB port?
Connect the oscilloscope to the printer's parallel port using a USB to Parallel Port adapter.

FAQ 2007-02-20

My Infiniium scope application is not running properly. Is there a way to reset it?
My Infiniium scope application is not running properly. Is there a way to reset it?

FAQ 2007-01-05

Why do I see more noise on my oscilloscope when a probe is connected?
When a probe is connected, the scope changes its attenuation setting so that it correctly displays the voltage coming from the probe.

FAQ 2006-12-04

When using TV trigger mode with a Keysight oscilloscope, can I trigger only on even or odd fields?
Yes. All current Keysight scopes with TV triggering are capable of exclusively triggering on odd or even fields.

FAQ 2006-12-04

How often should I send in my oscilloscope for calibration?
Please consult your instrument's Service Guide or contact your local Keysight service center.

FAQ 2006-12-04

Frequently Asked Questions N5433A and N5434A Keysight MSO FPGA Dynamic Probe for Altera
Keysight’s FPGA dynamic probe provides greater real-time measurement productivity for MSO- based validation of FPGAs and the surrounding system.

FAQ 2006-11-28

What is the Keysight part number for the CR2032 3V Lithium battery used on the CPU board in the 5483x, 5485x, MSO8000, and DSO80000 Series Infiniium...
The Keysight part number is 1420-0356. However, this is a very common battery and may be available at camera shops, electronic suppliers, etc.

FAQ 2006-11-13

Does the 1152A active probe work on the DSO80000 Series Infiniium Oscilloscopes?
Yes, the 1152A active probe works with Infiniium oscilloscopes up to and including the new DSO80000B Series oscilloscopes.

FAQ 2006-11-06

Why doesn’t my oscilloscope display the + and - signals from my differential probe separately?

FAQ 2006-11-04

Can my 54600-series or 6000-series scope use channels 3 and 4 for XY mode or math functions?
These oscilloscopes can perform math functions such as FFT, integration, and differentiation on any analog channel or even on another math function. But they cannot use channel 3 or 4 for XY mode, addition, subtraction, or multiplication.

FAQ 2006-11-04

What is the amplitude accuracy of my oscilloscope?
When oscilloscope manufacturers specify vertical accuracy, they typically only mention bandwidth and DC accuracy. The bandwidth specification addresses the AC accuracy. Tighter AC accuracy specifications are very uncommon.

FAQ 2006-11-04

Which Infiniium probes are compatible with the 6000 Series and which are not?
Infiniium probes supported by the 6000 Series oscilloscopes include ...

FAQ 2006-11-04

What does the scope decimate large amount of acquisition data to fit into the display?
The 6000 Series oscilloscopes do not decimate the acquired waveform for display.

FAQ 2006-11-04

My Infiniium oscilloscope with the removable hard drive will no longer boot up, why?
Make sure the removable drive key lock is in the locked position.

FAQ 2006-10-20

Why does the DC Gain Error formula in the DC Gain Accuracy procedure have factors of 0.60 and 0.75 in the DSO80000 Series Infiniiums but not the ot...
These factors are used in the DSO80000 Series Infiniiums because the DC gain is measured with input voltages that are less than full scale, but the spec is relative to a full scale input.

FAQ 2006-10-20

How do I fix the "Can't Connect to USB Device" problem when connecting to a DSO3000 series oscilloscope?
You must remove the device driver from Device Manager and cycle power on the oscilloscope so that the proper USB driver is installed.

FAQ 2006-10-20

Keysight 54600 Scopes: How Hard is it to Upgrade the Software?
Upgrading software for the 54620/40-series Oscilloscopes is easy.

FAQ 2006-10-18

How do I determine or adjust the sample rate of my 54620- or 54640-series oscilloscope?
To determine the sample rate, press the Main/Delayed button. The scope will display the current sample rate in the lower left portion of the display.

FAQ 2006-10-18

54600 Series: What Is the Difference between Run/Stop and Single on the Front Panel?

FAQ 2006-10-18

Previous 1 2 3 4 5 6 7 8 9 10 ... Next