Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

Refine the List

remove all refinements

By Topic

By Type of Content

By Product Category

101-125 of 415

Sort:
How do the :MEASure:SENDvalid and :MEASure:STATistics commands affect my Infiniium's measurement results?

FAQ 2010-05-16

Keysight Infiniium Oscilloscopes: Why does the display go off screen when I lower the V/Div?

FAQ 2010-05-16

Can I program a waveform captured by my oscilloscope into a Keysight arbitrary waveform generator?
Yes. The free IntuiLink Waveform Editor software will download waveform data from Keysight Infiniium, 6000 series, and 54600 series oscilloscopes and send the data to the a Keysight 33120A, 33210A, 33220A, or 33250A generator.

FAQ 2010-05-14

What is the equivalent circuit for the 1161A 10:1 passive probe for Infiniium scopes?
The following is an approximation of the equivalent circuit.

FAQ 2010-03-17

My InfiniiMax probe fails calibration or does not accurately pick up the cal signal when I use the E2655A test fixture. What could be wrong?
The first step in troubleshooting a failed probe calibration should be to compare the actual signal and the probed signal. If the probed signal does not track the actual signal well, it is most likely due to a poor connection.

FAQ 2010-03-09

Keysight Infiniium Oscilloscopes: Programming the Oscilloscope
Use the example programs and programming manual available for download from this web site.

FAQ 2009-12-11

How do I get the maximum available memory depth from my Infiniium oscilloscope?
The various Infiniium models offer between 32K and 128M points of memory per channel. The following guide shows you how to get the maximum available memory from your particular scope.

FAQ 2009-11-19

VEE 9.0 has SCPI completion. How do I make my own SCPI command built-in with VEE?
Please refer to the attached Microsoft Word document for a step by step explanation...

FAQ 2009-11-12

I've written my own text format for SCPI in *.txt. How do I use these for SCPI completion within VEE 9.0. What tool should I use?
You can use the tool found within Keysight.com. Just search using the keyword "Keysight VEE SCPI...

FAQ 2009-11-12

How to measure temperature with the AUXILIARY METER function of the U1602A/U1604A handheld Oscilloscope?
The humidity can be measured with U1586A Temperature Adaptor connected to the U1602A/U1604A handheld Oscilloscope

FAQ 2009-09-29

Where to find the USB modular scopes IVI-COM programming guide?
download the programming guide.

FAQ 2009-09-29

Can I use the Quick Print button to quickly save my waveforms into the USB thumbdrive?
Yes, but with software version 5.10 and above you have to enable the feature...

FAQ 2009-08-17

How do I control my InfiniiVision oscilloscope from a web browser?
Connect to LAN, type scope's IP address in browser, select Browser Web Control, Remote Front Panel.

FAQ 2009-08-17

How can I save comma separated variable (CSV) data to my USB thumb drive?
Set this up in Utility -> Print Config.

FAQ 2009-08-17

What is the update rate for U1600A series handheld scope?
update rate is 14 waveforms per second

FAQ 2009-08-06

Why does handheld scope’s DMM measurement frequently stall after one hour of continuous operation?
This condition indicates that the internal memory battery level has dropped to 1.4V or lower.

FAQ 2009-07-16

Is there any communication between the DCA mainframe and the 1169A probe via the N1022A adapter?
You have to select the probe model number in the graphical user interface (GUI) of the 86100X mainframe ...

FAQ 2009-06-22

How do you connect a 12GHz probe with a solder-in probe tip to the BNC port?
For best accuracy use the E2655B kit to perform the probe calibration on the DCA ...

FAQ 2009-06-22

The N1021B kit contains shorts and loads. Why would I need an N1024A TDR Calibration kit?
The N1024A is a complete set of premium male and female shorts, male and female loads, a pair of broadband cables and a torque wrench ...

FAQ 2009-06-18

Does the Measurement Manager (AMM) run on Window Vista operating system?
Yes. The Measurement Manager (AMM) rev. 1.8.3.0 and above will able to run on Windows Vista ...

FAQ 2009-06-10

How to measure current with the AUXILIARY METER function of the U1602A/U1604A handheld Oscilloscope?
The current can be measured with connect a current adaptor (current probe) to the U1602A/U1604A handheld Oscilloscope...

FAQ 2009-06-10

Why can’t my PC connect to my InfiniiVision oscilloscope via its LAN/USB/GPIB interface?
There are many possible reasons for this, but a very common problem is that the interface has not been enabled on the scope.

FAQ 2009-05-25

What type of USB cable do the U1602A and U1604A Handheld Oscilloscopes use?
The U1602A and U1604A Handheld Oscilloscopes use the USB type-A to mini-B cable….

FAQ 2009-05-03

How do I save deep memory waveform data from my InfiniiVision oscilloscope to a USB storage device?
Use half-channel mode and ASCII XY, ALB, or BIN format. Within the "Save" menu, press Settings and select the max number of points. Make sure you are at a slow enough time/div setting that all the points are on screen, and then ...

FAQ 2009-05-03

Will the "Auto Power Off" function work when the U1602A/U1604A Handheld Oscilloscope is connected to the AC adaptor?
No, the "Auto Power Off" function only works when the U1602A/U1604A Handheld Oscilloscope is operating with the battery pack....

FAQ 2009-05-03

Previous 1 2 3 4 5 6 7 8 9 10 ... Next