这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

76-100 / 166

排序:
Does E5805A or E5813A driver supports Linux operating systems?
No, E5805A or E5813A does not support Linux operating systems

FAQ 2009-10-20

Why am I not able to update my E5810A firmware via Keysight FTP at ftp://ftp.keysight.com/pub/e5810/ ?
Firmware revision A.01.07 and above are able to update via ftp

FAQ 2009-09-29

IO Libraries Suite: Can software written from other vendors specific to their devices that utilize NI-488.2 as an I/O Library work with a Keysight ...
Yes, it is possible with Keysight IO Library version 14.1 and greater.

FAQ 2009-08-25

IO Libraries Suite: Is there any other software that needs to be installed when I am using an application that utilizes NI-488.2 and Keysight IO Lib...
It depends if there is third party connectivity hardware or software installed.

FAQ 2009-08-25

可否在 ENA 上使用嵌入式 GPIB 接口来控制和执行功率计校准?
需要使用Keysight 82357A/B USB/GPIB 接口。

FAQ 2009-08-16

How to update E5810A firmware?
The firmware update instructions can be found on the User's Guide and E5810A Web Access Help......

FAQ 2009-08-06

How do I configure the E5813A Event Logging features in the E5813A LAN/USB Gateway Configuration Utility?
The E5813A Event Logging features are for internal diagnostic/troubleshooting of the device......

FAQ 2009-08-06

MWA 软件在评测模式下有何限制?
MWA 后台应用程序在评测模式下的测量数量受到限制。

FAQ 2009-07-15

如何将 ENA 上的 MWA 软件更新到最新版本?
MWA 软件的最新版本可从是德网站下载。

FAQ 2009-07-15

如何确认选定 的E5092A 配置能否执行测量?
用于 ENA 的 MWA 软件可以识别 E5092A 的体系结构,并自动检测使用选定的切换配置无法执行的测量路径。

FAQ 2009-07-15

我们可否通过外部 PC 控制 MWA 软件?
可以,MWA 的某些功能支持远程控制。

FAQ 2009-07-15

在不使用多端口测试仪的情况下,还可以在 ENA 上使用 MWA 软件吗?
可以,在不使用测试仪的情况下,4 端口 ENA 仍然可以使用 MWA 软件控制。

FAQ 2009-07-15

如何确定我的 ENA 是否安装了 MWA 软件?
MWA 的注册密钥代码存储在 ENA 目录中。

FAQ 2009-07-15

What are the replacement parts of the accessories furnished with the 41800A?

FAQ 2009-07-15

我可否改变 E5091A 多端口测试仪的 MWA 文件,将其用于 E5092A 可配置的多端口测试仪吗?
可以,您可以通过选择与 E5091A 等效的配置,将 MWA 文件于用于 E5092A。

FAQ 2009-07-15

我们可否使用 MWA 软件设置一组不同的测试(即不同的极限测试)?
可以。您可以使用 MWA 软件在同一设备上进行多达十种不同的测量设置。

FAQ 2009-07-15

有没有 MWA 软件的示例文件可供我定制自己的被测件?
有,某些示例器件的 MWA 文件可通过是德网站下载。

FAQ 2009-06-22

I'd like to make my own fixture to hold the N1021B probe. What do I need to know?
The N1021B probe body has two holes spaced 6.35 mm (1/4") apart and threaded for M2.5 screws. Maximum torque is 0.56 Newton-meter (5 lbf-in).

FAQ 2009-06-18

How does Keysight specify the bandwidth of the N1021B probe?
The one-way bandwidth of the probe can be estimated using a simplified equation ...

FAQ 2009-06-18

How does the angle between the N1021B probe and the target affect measurements?
It is best to hold the probe perpendicular to the DUT ...

FAQ 2009-06-18

Why should I calibrate the N1021B differential TDR probe at its connector side as opposed to its tips?
Calibration requires a short to ground for each single-ended portion of a differential signal. Because the differential probe does not have ground at the tips, it is not possible to calibrate to the tips of the probe ...

FAQ 2009-06-18

Can the N1021B differential TDR probe be ordered outside of the kit by itself?
Keysight decided to offer new differential TDR probes only as part of the N1021B probe kit ...

FAQ 2009-06-18

What happens if I probe somewhere in the middle of differential traces? (N1021B differential TDR probe)
The net effects of probing in the middle of traces are (1) you will greatly attenuate the transmitted signal, (2) you will cause a big discontinuity in the line that will send a reflection back to the source, and (3) the signal viewed using the TD...

FAQ 2009-06-18

The N1021B kit contains shorts and loads. Why would I need an N1024A TDR Calibration kit?
The N1024A is a complete set of premium male and female shorts, male and female loads, a pair of broadband cables and a torque wrench ...

FAQ 2009-06-18

能否使用一台 ENA 来控制多台 E5092A 以增加测试端口数?
可以,您能够使用一台 ENA 控制多达两台 E5092A。

FAQ 2009-05-25

以前 1 2 3 4 5 6 7 下一页