这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

26-50 / 166

排序:
是否为3.5mm插座高精度无插槽连接器(PSC)提供了连接器修理套件?
是。修理套件的部件编号是85052-60049。

FAQ 2012-05-04

ENA 是否为有源探头提供探头电源连接?

FAQ 2012-04-17

Which Connector Types Can Be Safely Connected, and Which Types May Cause Damage to the Interface?

FAQ 2012-04-05

What Options would my PSA Series Spectrum Analyzer require to operate in an N5530S / N5531S Measuring Receiver system?
It is highly recommended that your PSA have with Option 1DS (100 kHz to 3 GHz Preamplifier) or Option 110 (10 MHz to 26.5 GHz / 50 GHz preamplifier) for improved dynamic range.

FAQ 2012-03-15

How do I recover my PSA Spectrum Analyzer after a secure erase memory sanitization?
A secure erase memory sanitization clears all of the user writable instrument memory. Firmware and measurement personalities must be reinstalled.

FAQ 2012-02-26

Does the ENA support 87050E / 87075C series multiport test sets?
Unlike the E5061A and E5062A, the E5061B, E5071C and E5072A (ENA) does NOT support full functions of 87050E / 87075C. But it is possible to change switch state of 87050E-Hxx / 87075C-Hxx via GPIB.

FAQ 2012-01-11

如何为是德产品找到附件?
对于特定仪器附件(例如,用于示波器的探头),您首先应该访问产品页面,然后再查阅相关附件。 对于通用附件(例如,射频和微波测试)

FAQ 2011-10-07

85033E 30kHz至9GHz校准套件中的适配器是不是相位匹配的?
是。

FAQ 2011-10-07

85039B F型校准套件的延迟/直通定义值是否有错误?
定义值没有错误,但测量可插入的被测件时必须修改定义值。

FAQ 2011-10-07

Why i can't find other languages help file setting in U160X A/B series HH oscilloscope?
In order to access to other language, please go to respective product support page in www.Keysight.com. Go to Driver & Software page, select Firmware Update.

FAQ 2011-09-12

What is the shielding type used by Keysight GPIB cable?
Keysight GPIB cable is double shielded standard cable

FAQ 2011-09-12

PSA系列频谱分析仪允许直流电压输入吗? 如果允许那么最大直流输入电压是多少?
E4440A, E4443A和E4445A具有交流和直流耦合功能,但E4446A,E4447A和E4448A只有直流耦合功能。

FAQ 2011-06-27

怎样将失配不确定度计入 N5531S 测量接收机绝对幅度精度?
点击此处获得更多信息

FAQ 2011-06-27

N5532A/N5532B 传感器模块的频率范围是多少?PSA 系列频谱分析仪需要安装哪些选件才能在 N5531S 测量接收机上运行?
点击此处获得更多信息

FAQ 2011-06-24

能否保存早先的 TDR 测量波形,并载入与当前的 TDR 测量结果进行比较?
可以保存早先的 TDR 测量波形,并载入到示波器上与当前的 TDR 测量结果进行比较。

FAQ 2011-06-22

为什么我的示波器通过差分探头不能独立 显示“+”信号和“–”信号?

FAQ 2011-06-22

能否保存多条 TDR 迹线并在示波器上显示其波形,以便与当前的测量进行比较?
可以将多条 TDR 迹线保存为内部格式,供以后参考……

FAQ 2011-06-06

E5810A: Can I use the E5810A without installing the Keysight IO Libraries Suite?
Yes, the following instructions show you how to do this in NI-MAX with NI-VISA 2.6 or later installed.

FAQ 2011-04-12

如何获得 ENA 与 E5092A 测量设置中所用的附件(电缆和适配器)?
所有附件均包含在 E5092A 的选件中。

FAQ 2011-01-20

Can U1602A/B and U1604A/B measure capacitance of 0.13nF?
Based on the datasheet, for 0.13nF, it falls in the range of 60nF. To calculate the range of fluctuation of the reading,…

FAQ 2010-12-20

For the InfiniiMax probes, what effect does the "Signal being probed" setting have? Why do I have to specify single-ended or differential?
Infiniium scopes and InfiniiMax differential probe amplifiers have a unique method of applying DC offset which considers whether the signal being probed is single-ended or differential...

FAQ 2010-10-06

How do I control instruments such as 82357A, E5810A, and 82350B using the GPIB interface?
There are several approaches to control instruments via the GPIB interface...

FAQ 2010-10-04

86100A/B/C Infiniium DCA Firmware Upgrades
86100A/B/C Infiniium DCA Firmware Upgrades

FAQ 2010-09-23

I lost some of the small parts of the N1021B probe kit. Can I get them without buying a whole kit?
The following items will be available from www.keysight.com ...

FAQ 2010-09-19

How do I install the driver for the E5805A 4-port RS-232/USB adapter?
To install the driver for the E5805A 4-port RS- 232/USB adapter, follow the steps here:….

FAQ 2010-09-14

以前 1 2 3 4 5 6 7 下一页