这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

101-125 / 166

排序:
E5092A 能否为多端口被测件提供直流控制电压?
可以,E5092A 具有内部直流电源,能够为被测件供电。

FAQ 2009-05-25

86100C DCA-J - TDR/TDT模式
86100C DCA-J - TDR/TDT模式

FAQ 2009-04-29

Why when using the parallel interleave mode and 1 clock per sample, the data seems to be clocked on the opposite clock edge than what the GUI state...
This is a known issue and has been noted for future consideration. The workaround is...

FAQ 2009-02-12

Why doesn't Windows® detect new hardware when I plug the E5813A USB Hub into the computer?
The new hardware is not detected when you plug the E5813A USB Hub into the computer because the PC driver may not be installed properly....

FAQ 2009-01-12

Is it possible to get an error log of incorrectly sent remote commands to my PSA, E4406A, EMC, or ESA Series Spectrum Analyzer?
Yes. PSA, E4406A and the ESA Series (with firmware A.08.00 and later) support this. You may turn Verbose error logging on through the front panel or remotely, SYST:ERR:VERBOSE ON

FAQ 2008-11-21

On the Keysight PNA Series Network Analyzers, is it possible to create an ASCII text based data file from a memory trace?
Yes, it is possible to save a Keysight PNA memory trace to an ASCII text file such as a PRN file.

FAQ 2008-11-20

I need information on Keysight Instrument Security and memory sanitization.
Use the Keysight Instrument Security page to look up the security and memory sanitization procedures for your instrument. Use this link view security information by model number or product type.

FAQ 2008-11-20

What are the part numbers for the 2 m DC power cable and the 1 m RF cable (SMA (m) to SMA (m)) that comes together with the OML Inc. millim...
These parts are not available separately from Keysight.

FAQ 2008-10-17

IVI Instrument Drivers Overview
Learn more about IVI-COM and IVI-C instrument drviers.

FAQ 2008-10-01

How do I configure the E5810A LAN/GPIB Gateway web access when updating firmware from the local FTP server?
When updating firmware from the local FTP server, follow the steps below to configure the E5810A LAN/GPIB Gateway web access:….

FAQ 2008-09-25

What will happen to the E5810A LAN/GPIB Gateway (with firmware revision A.01.05) when it is powered ON for 5 minutes without a LAN connection?
When the E5810A (with firmware revision A.01.05) is powered ON for 5 minutes without a LAN connection, a static IP will be assigned….

FAQ 2008-09-25

What is the maximum torque force allowable on the 82350B GPIB card connector?
The maximum torque force allowable when attaching a GPIB cable to the 82350B GPIB card connector is 8 in. lbs.

FAQ 2008-09-24

可以把U1241A/U1242A连接到PC上吗?
不行,U1241A/U1242A不带任何PC接口。

FAQ 2008-09-22

可以使用U1241A或U1242A保存测量数据吗?
U1242A带有内部存储器,可以保存测量数据。您可以手动保存高达100个数据点或记录高达200个数据点的数据。U1241A无此能力。

FAQ 2008-09-22

可以使用U1241A/U1242A测量温度吗?
可以,事实上U1242A可以同时测量两个温度。

FAQ 2008-09-22

U1241A或U1242A手持式数字多用表的电池可以用多久?
U1241A或U1242A附带的电池在正常使用状态下可持续供电200小时以上。

FAQ 2008-09-22

U1241A和U1242A可以使用普通AAA电池吗?
可以,U1241A和U1242A手持式数字多用表可以使用普通AAA电池。取决于所用电池,供电时间可能有所变化。

FAQ 2008-09-22

可以对保存的波形进行测量吗?

FAQ 2008-08-03

What is the meaning of P1dB and Psat as stated in amplifier specifications?

FAQ 2008-07-15

我们要多久给4294A做一次性能检测?
我们建议每年一次,当然也视客户的具体使用次数和使用环境不同而不同。

FAQ 2008-01-31

Test Set Files

FAQ 2008-01-28

如何将NI Labview和82357A USB/GPIB接口连接起来?
安装IO 程序库并配置82357A

FAQ 2008-01-14

How do I configure Keysight I/O cards and converters to work with the National Instruments software?
There are a few, simple steps that you need to take to make National Instruments software work with Keysight I/O cards and converters.

FAQ 2007-12-09

是否存在一个用于各种网络分析仪和阻抗分析仪的兼容打印机主清单?

FAQ 2007-07-10

How do I recalibrate the N5531S Measuring Receiver when performing the Tuned RF Level (TRFL) measurement?
Click here for additional information.

FAQ 2007-06-22

以前 1 2 3 4 5 6 7 下一页