这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

缩小范围

去除所有优化

按主题

按内容类型

按产品类别

1-22 / 22

排序:
Where can I find software downloads for PathWave Test?
Go to http://www.keysight.com/find/pathwave-test-latest-downloads

FAQ 2018-06-12

30-Day Free Trial for X-Series Measurement Applications for X-Series Modular Instruments
30-day trial license available for the X-Series measurement applications for X-Series modular signal analyzers.

FAQ 2016-06-09

如何找到免费试用?
免费试用设计和测试软件。为您的应用寻找免费试用的软件。

FAQ 2014-08-14

What is the RF Test Blog?
RF engineers know that making good measurements is a challenge. The RF Test Blog was created as a resource for RF engineers to find ways to make better RF measurements.

FAQ 2013-12-17

Does Keysight VEE 9.0 support Windows 7?
Yes. A Keysight VEE patch is currently in development and is tentatively scheduled for release on 2nd quarter of 2010.

FAQ 2013-11-17

N6171A MATLAB Software - Keysight Compatible Instruments
N6171A MATLAB software can be purchased along with a new Keysight instrument or purchased as software to add to an existing instrument.

FAQ 2013-04-29

How to report a VEE bug, serious error or submit an enhancement request effectively?
1. Go to the VEE Help menu and select Customer Feedback option...

FAQ 2012-10-16

Is the Instrument Control Toolbox required for all versions of Download Assistant?
Download Assistant V2.0 requires you to have MATLAB’s Instrument Control Toolbox installed.

FAQ 2012-08-09

Which signal generators are compatible with the Download Assistant for MATLAB?
Download Assistant V2.0 requires you to have MATLAB’s Instrument Control Toolbox installed. MATLAB supports instrument control, instrument configuration, and data transfer with its Instrument Control Toolbox, which allows a wide variety of Keysight instruments to be programmed from within the MATLAB environment.

FAQ 2012-08-09

What type of connection is required in order to transfer data from PC to signal generator for MATLAB?
Data transfer from the PC to the signal generator requires a GPIB or Ethernet (TCP/IP) connection.

FAQ 2012-08-09

Do I need Instrument Control Toolbox if I already have MATLAB installed?
If you already have MATLAB installed, type “ver” at the MATLAB command line to see if you already have Instrument Control Toolbox installed.

FAQ 2012-08-09

What types of files are installed on my machine when I download the Download Assistant for MATLAB?
During installation, the Download Assistant software installs a series of MATLAB functions as MATLAB files, including two MATLAB file examples, into your directory of choice. To learn how to use these functions,see ...

FAQ 2012-08-09

VEE Pro 文档
下载旧版 Keysight VEE Pro 软件。

FAQ 2012-07-23

Why can't I connect to my instrument?
You need to find the instrument in Keysight Connection Expert....

FAQ 2010-05-07

What support will Keysight provide for the example programs at /find/matlab_sa ?
You have the royalty-free right to use and distribute......

FAQ 2010-05-07

Why after using the binblockread() function in MATLAB, all subsequent data transfers return bad data/info?
The binblockread() function doesn't read the terminating character.

FAQ 2010-05-07

I do not understand how to use a particular MATLAB function. Who can help me?
Contact The MathWorks

FAQ 2010-05-03

Is VEE able to interpret "," as decimal point in Formula box running under German Windows?
No. Please use "." as decimal point as per international standard.

FAQ 2009-11-17

VEE 9.0 has SCPI completion. How do I make my own SCPI command built-in with VEE?
Please refer to the attached Microsoft Word document for a step by step explanation...

FAQ 2009-11-12

I've written my own text format for SCPI in *.txt. How do I use these for SCPI completion within VEE 9.0. What tool should I use?
You can use the tool found within Keysight.com. Just search using the keyword "Keysight VEE SCPI...

FAQ 2009-11-12

Why is the binblockread() function returning bad data?
Need to check the byte order of the computer

FAQ 2009-03-09

IVI Instrument Drivers Overview
Learn more about IVI-COM and IVI-C instrument drviers.

FAQ 2008-10-01