您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

1-13 / 13

排序:
Why is readback voltage/current different from actual value when the recall function is used after power cycling the unit?
Users may encounter incorrect voltage/current readback reading under the following conditions

FAQ 2019-02-27

我在哪裡可以找到過時的HP測試儀器的使用手冊?
有一些公司可能還會提供這些使用手冊…

FAQ 2013-05-29

66xxA: Calibration Certificates
Criteria have been established to determine which products get or do not get a calibration from the factory. A product with a product number does not automatically qualify for a calibration certificate.

FAQ 2008-09-22

66xxA: Re-Calibration Date
There are no components used in Power Products which have a specific shelf life. Therefore, the calibration period of this instrument begins on the date that the product is first put into service by the customer. The recommended calibration interv...

FAQ 2008-09-22

66xxA, 68xxB, N330A and E36xxA: Determining the Correct Line Voltage Option to Order for a Power...
Some power products use lots of power, far beyond the range of typical electronic products with which we are familiar. This makes choosing the correct line voltage option more challenging.

FAQ 2008-09-22

What types of memory are installed into Keysight N3302A, N3303A, N3304A, N3305A, N3306A, and N3307A DC electronic load mainframes?
Please refer to the document linked to this page for a comprehensive listing of internal memory information for Keysight N3302A, N3303A, N3304A, N3305A, N3306A, and N3307A DC electronic load products.

FAQ 2006-11-15

605xxB 與 N330xA:串聯及並聯的電子負載
605xxB 與 N330xA:串聯及並聯的電子負載

FAQ 2006-04-11

What are the units used when setting the current slew rate in the electronic loads from the front panel and over the GPIB?
For the N3300A series electronic loads, all slew rate entries from the front panel or over the GPIB are done in the units of amperes per second (A/s).

FAQ 2006-04-11

How do I get my N3300/01A to output a negative going trigger pulse?
The trigger out of the N3300/01A electronic load mainframes is a positive pulse. Many electronic instruments require a negative pulse for a trigger in signal. The workaround is to use the digital port functionality of the electronic load. The d...

FAQ 2006-04-10

Keysight 66xxA, 605xB 與 N330xA:含增益的電壓編程
是的,許多是德電源供應器都有遠端電壓設定或類比設定功能的特性。然而...

FAQ 2005-08-25

66xxA, 68xxA, N330xA 與 E36xxA:我該如何偏移因長纜線所造成的電壓降情形?

FAQ 2005-08-08

Keysight 66xxA、E435xB、605xB、N3300A 和 E36xxA:地面上電源供應器的「浮接」輸出
Keysight 66xxA、E435xB、605xB、N3300A 和 E36xxA:地面上電源供應器的「浮接」輸出

FAQ 2005-07-13

66xxA: Synchronize Different System Power Supply Outputs

FAQ 2003-06-04