Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

176-200 of 526

Sort:
How wide range of resistivity can the 4339B measure when used with the 16008B?
The 4339B can measure surface resistivity up to 7 x 1017 Ω and volume resistivity up to 8 x 1018 Ω-cm, but it depends on the electrodes of the 16008B used.

FAQ 2010-07-02

The marker list function in the NA mode of the 4395A/4396B displays "EXTRA" value in the list below Smith chart. What does this value stand for?
It stands for equivalent capacitance or inductance.

FAQ 2010-07-02

How can I get DC bias current resolution of 20 mA in the 1 A to 2 A range when the E4980A-002 is used with 2 units of the 42841A?
The bias current resolution has been improved on the E4980A with firmware revision 2.12 and above. If your E4980A has firmware revision 2.10 or below, upgrade the firmware to revision 2.12 or above.

FAQ 2010-07-02

Do the coaxial Short and 50 Ω Load terminations for the 42941A have accuracy specifications?
No, both the coaxial Short and 50 Ω Load standard terminations for the 42941A do not have accuracy specifications.

FAQ 2010-07-02

What are primary differences between the E4991A and 4291B?
The major difference is frequency range. E4991A: 3 GHz, 4291B: 1.8 GHz.

FAQ 2010-07-02

Why is there a step (discontinuity) on the trace of noise floor around 10 MHz in 4395A's SA mode even when no signal is input into the test port?
This phenomenon is caused by a change in circuit operation of the 4395A at 10 MHz.

FAQ 2010-07-02

Why does the DC resistance measurement function of the 4287A require to be calibrated at the same time with Open/Short/Load calibration?
The specified accuracy for the DC resistance measurement is applied when the Open/Short/Load calibration for the DC resistance measurement is performed.

FAQ 2010-07-02

The 4339B with 16339A test fixture: The insulation resistance of a high value ceramic C (≥1000 pF) is very noisy even after 60 sec. charging time.

FAQ 2010-07-02

Error message "PHASE LOCK LOOP UNLOCKED" could be displayed, when the 4294A using an external ref. osc (opt.1D5 or other 10 MHz output) is ON.
The message is removed when any key of the front panel except [Preset]. In this case, the unit works properly.

FAQ 2010-07-02

Why don't the E4991A and 4287A have Load compensation function?
Performing Load compensation in addition to Open/Short compensation is equivalent to performing Open/Short/ Load calibration at DUT contacts of test fixture (by using the working standard devices).

FAQ 2010-07-02

Can 4263B preserve Open/Short/Load correction data by using Save/Recall function?
No.

FAQ 2010-07-02

Is there any effective way to measure the impedance of a pressure sensitive SMD component (ex. a ferrite bead) with the 16196 series or 16197A test...
In order to measure a pressure sensitive device, the pressure applied to the DUT by the test fixture needs to be carefully controlled.

FAQ 2010-07-02

The E4980A/4284A display much lower resistance values than DUT's DC resistance when measuring high-value resistors in Mega-ohms region.
Set the measurement function to Cp - Rp mode to measure high resistance properly.

FAQ 2010-07-02

Can the E4980A perform open/short/load correction at user-specified spot frequency points while open/short correction at all frequency points is OF...
No, open/short/load correction at user-specified spot frequency points can be activated only when open/short correction at all frequency points is set to on.

FAQ 2010-07-02

Can the 4294A measure a grounded DUT?
The 4294A can measure the grounded DUT when used with the 42941A Impedance Probe.

FAQ 2010-07-02

Can I separately order the heat-resistant cable without ordering E4991U-007 Upgrade Kit?
No. The heat-resistant cable cannot be ordered separately from the E4991U-007.

FAQ 2010-07-02

Why does measurement data exhibit a discontinuity at 5 MHz or 15 MHz and how can the 4294A get rid of this phenomenon?
The 4294A extends its measurement frequency range up to 110 MHz by terminating each measurement terminal with 50 ohm in order to eliminate the resonance of test leads (including leads inside the 4294A).

FAQ 2010-07-02

How should I define or select the residual inductance values of Shorting Bars when performing Short compensation on the E4991A or the 4287A?
Nowadays, the authorized standards stipulate the dimensions of shorting devices and the Short Compensation method which uses the defined inductance values of the shorting devices. It is recommended to consider these authorized standards.

FAQ 2010-07-02

Can the 4338B measure internal resistance of a battery?
Yes, the 4338B can directly measure internal resistance of a battery.

FAQ 2010-06-14

How low resistance can the 4338B measure and resolve?
The effective resistance measurement range and resolution of the 4338B is down to 10 micro-ohms. The minimum display resolution of the 4338B is 0.1 micro-ohms.

FAQ 2010-05-14

Is the E4991A option 010 needed only when a specific probe station is used with the E4991A?
No, the E4991A-010 is generally needed when a probe station is used with the E4991A.

FAQ 2010-05-12

What are the precautions when using the 4284A LCR Meter with the 42841A Bias Current Source and the 42842A/B Fixtures?

FAQ 2010-05-12

What is max. DC output voltage when two 42841A units are used as a 40A system?

FAQ 2010-05-12

When fabricating a custom test fixture for the Keysight 4339B, what are the recommendations to extend the measurement and interlock cables?

FAQ 2010-05-11

Can I perform real time measurement with Keysight U1731B & U1732B Data Logger Software?
The Data Logger Software is to provide an indicative check on the unit and not intended for high timing accuracy measurement…

FAQ 2010-05-05

Previous 1 2 3 4 5 6 7 8 9 10 ... Next