这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

76-100 / 525

排序:
On the ENA I am receiving the message "Continuous switching may damage source attenuator". What corrective actions should I pursue?

FAQ 2012-03-16

针对 Keysight ENA 系列矢量网络分析仪,建议使用哪种运输箱?
目前还没有针对 ENA 和 ENA-L 系列而专门定制的运输箱。不过,是德的 9211-2658 运输箱足以容纳一台 ENA-A、ENA-B、ENA-C 或 ENA-L 系列矢量网络分析仪。

FAQ 2012-02-28

Can I hide the softkey menu when I perform "Dump Screen Image" on the ENA / ENA-L?
Yes.

FAQ 2012-02-02

What are the implications of swapping test heads between different Keysight 4287A Impedance Analyzers?
The Keysight 4287A Impedance Analyzer must be used with the furnished test head as a set because it is an indivisible portion of the calibrated 4287A.

FAQ 2012-01-16

What is an alternative solution to the 87075C / 87050E replacement?
Build your home-made switch box using the L4491A RF/MW switches. Refer to the application note for details.

FAQ 2012-01-11

如何在是德矢量网络分析仪中进行迹线数学运算?
是德网络分析仪中的迹线数学运算适用于复数实部和虚部数据对。

FAQ 2012-01-11

Does the ENA support 87050E / 87075C series multiport test sets?
Unlike the E5061A and E5062A, the E5061B, E5071C and E5072A (ENA) does NOT support full functions of 87050E / 87075C. But it is possible to change switch state of 87050E-Hxx / 87075C-Hxx via GPIB.

FAQ 2012-01-11

While programming the ENA I am receiving the error, "-128, Numeric data not allowed". Why?
For many analyzers the data transfer format is adjustable when outputting data...

FAQ 2011-10-07

When I save a Touchstone file with the ENA / ENA-L, which calculation will be reflected in the Touchstone file?
All calculations are reflected in the Touchstone file except for the mixed-mode conversion.

FAQ 2011-10-07

Anti-Virus FAQ for ENA

FAQ 2011-10-07

Keysight ENA-L是否与871x系列类似,支持内置网页?
不。ENA-L包括型号E5061A和E5062A,与前身871x不同的是,它们没有内置网页服务器。

FAQ 2011-10-07

ENA系列网络分析仪上的"1.#QNB"和"1.#QNAN"代表什么意思?

FAQ 2011-10-07

What are the benefits of the built-in VBA?

FAQ 2011-10-07

我的模拟软件不能用*.s1、*.s2等扩展名输入标准文件,有解决这个问题的办法吗?

FAQ 2011-10-07

85033E 30kHz至9GHz校准套件中的适配器是不是相位匹配的?
是。

FAQ 2011-10-07

如果在是德矢量网络分析仪上设定了电延迟,如何通过频率计算等效相位延迟?
根据电延迟,等效相位延迟可通过公式: θ˚ = Ftest * Delay * 360计算

FAQ 2011-10-07

Windows login process appears on my ENA every time after power up. Can I skip this?
Yes.

FAQ 2011-10-07

使用用户定义的校准套件执行校准后,所有记录幅值会显示为-200dB,这是什么原因?

FAQ 2011-10-07

ENA 和 ENA-L 的编程指令可以互相兼容吗?
是的

FAQ 2011-10-07

Is it possible to improve the print speed of my ENA?
Yes

FAQ 2011-10-07

On the ENA, how can I make CW sweep (Fixed frequency) without turning off the ENA's output signal each time a sweep finishes?
Turn off the "Init Src Ctrl" feature, then hold trigger.

FAQ 2011-10-07

Does the touchstone file generated by the ENA / ENA-L include the electrical delay?
The touchstone files do not include electrical delay. Please use port extension.

FAQ 2011-10-07

What is the difference between Smoothing and Averaging on a Keysight network analyzer?

FAQ 2011-10-07

有没有Keysight VEE示例程序概括说明如何使用SRQ通过程序来检测ECal校准过程是否完成?
有。

FAQ 2011-10-07

On the ENA / ENA-L, what occurs if I select "order-based display" in sweep mode?
Measurement points of different segments are plotted in constant intervals.

FAQ 2011-10-07

以前 1 2 3 4 5 6 7 8 9 10 ... 下一页