这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

226-250 / 525

排序:
Can the E4980A make a list sweep measurement at regular time intervals and save the measurement data with time stamp?
Yes. You can make a List Sweep measurement and save the measurement result with time data using Time Stamp function.

FAQ 2009-08-19

E4980A/4284A LCR 表显示“ALC 不能调整”的错误消息时,应执行哪些纠正措施?

FAQ 2009-08-13

16047A 与 16047D 之间存在哪些差异?

FAQ 2009-08-13

如何订购 4285A 选件 201、202 和选件 301 的操作指南?
4285A 选件 201/202 处理器接口和选件 301 扫描仪接口的操作指南列在 4285A 操作手册(序列号 04285-90010)结尾部分的附录中。

FAQ 2009-08-13

How to calculate the accuracy for U1731A/U1732A Capacitance Measurements?
The accuracy is calculated using the formula in the data sheet...... The Example......

FAQ 2009-07-16

How to calculate the accuracy for U1731A/U1732A Inductance Measurements?
The accuracy is calculated using the formula in the data sheet...... The Example......

FAQ 2009-07-16

How can I order 10 µF Standard Capacitor to retrofit the 16380C with Option 001?
The 16380V-001 Upgrade Kit for adding 10 µF capacitor is available.

FAQ 2009-07-07

与 Keysight 85070E 介电探头套件连用时,各种探头的频率限制及其原因是什么?
通过 3 GHz E4991A 阻抗分析仪,85070E 介电探头选件 020、030 和 050 可拥有最大的频率。

FAQ 2009-06-26

Is calibration report included in the 16380V-001 Upgrade Kit which adds the 10 µF standard capacitor to the 16380C?
Yes, the 16380V-001 Upgrade Kit includes the 10 µF standard capacitor and its calibration report.

FAQ 2009-06-23

Can the U1731A/U1732A Handheld LCR Meter measure a battery's internal resistance?
No, the U1731A and U1732A Handheld LCR meters cannot measure active parts like batteries etc.....

FAQ 2009-03-25

Is the Rdc measurement accuracy of the 4287A better than that of the 4286A?

FAQ 2009-03-13

What is the DC open/short/load calibration used for?

FAQ 2009-03-11

Do the 4284A GPIB commands comply with SCPI?
Yes. The GPIB programming language of the 4284A is SCPI.

FAQ 2009-03-11

What should I perform when the 4287A displays an “OVLD” message?
First, check if the DUT has properly contacted the test fixture’s electrodes. If no contact error is found, check for a possible failure of the 4287A.

FAQ 2009-03-11

Can I use any instrument driver software for the 4284A?
National Instrument’s LabVIEW driver supports the 4284A.

FAQ 2009-03-11

Is there a 16060A-like transformer test fixture usable with the 4284A?
No transformer test fixture for the 4284A is available.

FAQ 2009-03-11

Is there a 16060A-like transformer test fixture usable with the E4980A?
No transformer test fixture for the E4980A is available.

FAQ 2009-03-11

Is it possible to create a VBA, LabVIEW or any control program for application and run it on the 4287A?

FAQ 2009-03-11

Can the Rdc measurement function of the 4287A be used instead of a digital multimeter to measure the DC resistance of an inductor?
No, it is not recommended to measure DC resistance of inductors with the Rdc measurement function. This function is provided for contact check.

FAQ 2009-03-11

When is the contact check of the 4287A performed?
The contact check (Rdc measurement) is performed prior to each impedance measurement after a trigger.

FAQ 2009-03-11

What are the dimensions of the working standards supplied with the option 4287A-004?

FAQ 2009-03-11

Are the GPIB commands of the 4287A compatible with the 4286A?

FAQ 2009-03-11

How should I make Rdc measurements with the 4287A to improve measurement stability for low DC resistance below 1 ohm?
It is recommended to set the averaging factor of the 4287A to 4 or above in order to make as stable Rdc measurements as the 4286A does.

FAQ 2009-03-11

How can I order the upgrade kit of the 4287A?

FAQ 2009-03-11

What is the output impedance of the 4287A?
Nominal output impedance is 50 ohms.

FAQ 2009-03-11

以前 1 2 3 4 5 6 7 8 9 10 ... 下一页