这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

201-225 / 526

排序:
将两个 42841A 单元作为一个 40A 系统使用时,最大直流输出电压是多少?
将两个 42841A 单元作为一个 40A 系统使用时,最大直流输出电压是多少?

FAQ 2010-05-24

有没有适用于扩展 E4991A 测试端口的选件或附件?
除了 E4991A-007 温度特征测试套件,不需要安装任何选件或附件来扩展 E4991A 的测试端口。

FAQ 2010-05-24

4338B 可以测量的最小电阻是多少?分辨率如何?
4338B有效测量的最小值为10微欧姆。显示分辨率是0.1微欧.

FAQ 2010-05-14

4284A LCR 表和 42841A 偏置电流源及 42842A/B 夹具一起使用时,需要注意哪些问题?

FAQ 2010-05-12

When fabricating a custom test fixture for the Keysight 4339B, what are the recommendations to extend the measurement and interlock cables?

FAQ 2010-05-11

Can I perform real time measurement with Keysight U1731B & U1732B Data Logger Software?
The Data Logger Software is to provide an indicative check on the unit and not intended for high timing accuracy measurement…

FAQ 2010-05-05

How to calculate the accuracy for U1731B/U1732B Inductance Measurements?
The accuracy is calculated using the formula in the data sheet...... The Example......

FAQ 2010-05-05

Does the 4294A have the ALC (Auto Level Control) function?
No, the 4294A doesn't have the ALC. I-Basic program can be used to achieve the test signal ALC.

FAQ 2010-05-03

How to calculate the accuracy for U1731B/U1732B Capacitance Measurements?
The accuracy is calculated using the formula in the data sheet...... The Example......

FAQ 2010-05-03

Can the 41951A Impedance Test Kit be used with the 4395A/ 4396B?
No, the 41951A cannot be used with the 4395A or 4396B.

FAQ 2010-04-13

Is there any simple method of having the E4980A start up with a low test signal voltage?
You can have the E4980A start up with a low test voltage by saving a test level setting in memory and starting up with the recalled setting.

FAQ 2010-03-31

如何订购 Keysight 42941A 阻抗探头的替换探针?
订购部件编号为 42941-60004 的是德产品

FAQ 2010-03-16

Can the U1731B/U1732B Handheld LCR Meter measure a battery's internal resistance?
No, the U1731B and U1732B Handheld LCR meters cannot measure active parts like batteries etc.....

FAQ 2010-02-21

Are there any programming commands for the U1731B/U1732B Handheld Capacitance and LCR Meter?
No, it only offers datalogging with Keysight U173xB GUI Data Logger Software.

FAQ 2010-02-21

Are there any programming commands for the U1701B Handheld Capacitance Meter?
No, it only offers datalogging with Keysight U1701B GUI Data Logger Software…

FAQ 2010-02-21

4287A 进行接触点检测时显示的 Rdc 测量值不准确,怎样做才能提高其准确度?
执行开路/短路/负载校准和开路/短路补偿。

FAQ 2010-01-26

当显示“警告,ALC 不能调整”时,E4980A / 4284A 能否测量被测件?
能,虽然无法将测试信号电平控制在 ALC 设置值上,但 E4980A/ 4284A 仍能测量被测件。

FAQ 2010-01-26

42841A 关闭时,为什么直流电流偏置系统指示的测量值不正确?

FAQ 2010-01-26

按下 RF OUT On/Off(射频输出打开/关闭)键时,4396B 是否会立即关闭射频信号源?
这要视 4396B 固化软件版本而定。

FAQ 2010-01-26

What is the recommended calibration period of the 16380C?
The recommended calibration period is every 12 months.

FAQ 2009-11-17

What is the recommended calibration period of the 42030A?
The recommended calibration period is every 12 months.

FAQ 2009-11-17

What is the recommended calibration period of the 16380A?
The recommended calibration period is every 12 months.

FAQ 2009-11-17

What is the recommended calibration period of the 16190B?
The recommended calibration period is every 12 months.

FAQ 2009-11-17

Are there any programming commands for the U1731A/U1732A Handheld Capacitance and LCR Meter?
No, it only offers datalogging with Keysight U173xA GUI Data Logger Software.

FAQ 2009-10-26

Are there any programming commands for the U1701A Handheld Capacitance Meter?
No, it only offers datalogging with Keysight U1701A GUI Data Logger Software…

FAQ 2009-10-22

以前 1 2 3 4 5 6 7 8 9 10 ... 下一页