这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

151-175 / 525

排序:
When measuring a capacitor via a Keysight LCR meter, what is the best circuit mode, Cs or Cp?
To measure L, C, or R, there are two equivalent circuit models.The LCR meter can select the mode by setting the FUNC (function) to Cp, Cs, Lp or Ls.

FAQ 2010-09-30

Can I read a list sweep measurement data by operating the soft-panel of the E4980A on Web Browser?
Yes, you can read a list sweep measurement data using Web-server control mode.

FAQ 2010-09-19

External test, 26 TRD LOSS test fails. How do I execute?
In the 26 TRD LOSS test, use 2 m N(m)-N(m) cable for the connection between S and R on the 4291B front panel. If it fails even using the 2m cable, troubleshoot the test station.

FAQ 2010-09-19

Why isn't calibration option (UK6) available for the 42941A?
The 42941A does not have calibration option because the 4294A specifies total measurement accuracy including the 4294A accuracy.

FAQ 2010-07-12

When utilizing Save/Recall on the E4991A file names are limited to six characters. Is there a method to save/recall files with longer names?

FAQ 2010-07-12

Can I separately order the heat-resistant cable without ordering E4991U-007 Upgrade Kit?
No. The heat-resistant cable cannot be ordered separately from the E4991U-007.

FAQ 2010-07-02

The 4395A with the 41800A Active Probe or the 41802A 1 MΩ Input Adapter: Is any calculation required for converting the data for 50 Ω input?
No, any conversion calculation related to the difference in input impedance (between 1 MΩs and 50 Ωs) is not required. You can directly read the measurement value on the 4395A.

FAQ 2010-07-02

What is input impedance of the 4339B?
Nominal input resistance is 1000 Ω .

FAQ 2010-07-02

Is there any effective way to measure the impedance of a pressure sensitive SMD component (ex. a ferrite bead) with the 16196 series or 16197A test...
In order to measure a pressure sensitive device, the pressure applied to the DUT by the test fixture needs to be carefully controlled.

FAQ 2010-07-02

In the 4395A/4396B NA mode, the "dB" expression is used instead of the "dBm" even when the meas. parameter is set to absolute power amplitude.
Please regard the displayed "dB" as "dBm".

FAQ 2010-07-02

How can I connect a test fixture to the measurement terminals of the E4980A when the stopper at the rear of the fixture disturbs the connection?
Remove the stopper from the test fixture by removing a screw at the center of the plastic stopper. Otherwise, remove the front rubber guide from the E4980A.

FAQ 2010-07-02

Why does the DC resistance measurement function of the 4287A require to be calibrated at the same time with Open/Short/Load calibration?
The specified accuracy for the DC resistance measurement is applied when the Open/Short/Load calibration for the DC resistance measurement is performed.

FAQ 2010-07-02

Why cannot I control TEST SET ATTEN PT1 and PT2 functions in ATTENUATOR MENU when the 87511A S-parameter test set is used with the 4395A?
The TEST SET ATTEN PT1 and TEST SET ATTEN PT2 functions cannot be controlled because the 87511A is not equipped with input attenuators.

FAQ 2010-07-02

使用 Keysight 16085B 4 终端对至 7mm (APC-7) 适配器时,应使用夹具补偿标准件还是同轴校准标准件?

FAQ 2010-07-02

为什么 E4991A 和 4287A 没有负载补偿功能?
除开路/短路补偿以外,执行负载补偿相当于在测试夹具的被测件接触点上执行开路/短路/负载校准(通过使用工作标准器件)。由于在被测件接触点上的开路/短路/负载校准可以完全替代开路/短路/负载补偿,因此 E4991A 和 4287A 没有提供负载补偿功能。 当需要进行负载补偿时,可以使用开路/短路/负载校准功能来替代开路/短路/负载补偿。

FAQ 2010-07-02

Does typical permittivity measurement accuracy includes all the uncertainties due to the E4991A with opt 002, 16453A and MUT insertion conditions?
Yes. All the uncertainties are included in the typical measurement accuracy.

FAQ 2010-07-02

The 4294A displays a caution "Reduce OSC level" or "Bridge Unbalanced" in Fixture COMP [Short] with 1V OSC level. Is the compensation still valid?
No, the SHORT COMPEN value is invalid. The 4294A cannot measure DUT impedance below 48 ohms at OSC level setting over 500 mV.

FAQ 2010-07-02

Why is there a step (discontinuity) on the trace of noise floor around 10 MHz in 4395A's SA mode even when no signal is input into the test port?
This phenomenon is caused by a change in circuit operation of the 4395A at 10 MHz.

FAQ 2010-07-02

How is measurement accuracy calculated when the 42841A is used with the 4284A, 4285A or E4980A?
The measurement accuracy is the sum of the measurement instrument accuracy and additional error produced when the instrument is used with the 42841A and bias current test fixture.

FAQ 2010-07-02

Can the cylindrical insulator reduce the effect of magnetic coupling between the inductive DUT and the outer conductor of the 16196A/B/C/D fixtures...
Yes, but the effect of reducing the magnetic coupling effect is not sufficient and depends on the DUT.

FAQ 2010-07-02

How can I replace the contact tip of the 16334A?
The replacement contact tip is orderable by part number 16334-09002.

FAQ 2010-07-02

当所有频率点上的开路/短路修正都设置为关闭时,E4980A 能否在用户指定的标定频率点上执行开路/短路/负载修正?
不能,只有当所有频率点上的开路/短路修正都设置为打开时,用户指定的标定频率点上的开路/短路/负载修正才能被激活。

FAQ 2010-07-02

Can I control the E4980A functions by operation on Web Browser?
Yes, you can control the E4980A over Web Browser by connecting it to your PC by LAN.

FAQ 2010-07-02

How should I define or select the residual inductance values of Shorting Bars when performing Short compensation on the E4991A or the 4287A?
Nowadays, the authorized standards stipulate the dimensions of shorting devices and the Short Compensation method which uses the defined inductance values of the shorting devices. It is recommended to consider these authorized standards.

FAQ 2010-07-02

The marker list function in the NA mode of the 4395A/4396B displays "EXTRA" value in the list below Smith chart. What does this value stand for?
It stands for equivalent capacitance or inductance.

FAQ 2010-07-02

以前 1 2 3 4 5 6 7 8 9 10 ... 下一页