您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

1-25 / 1728

排序:
Signal & Spectrum Analyzer Benchtop/Modular/Handheld Firmware Update Center
To access the most recent version of firmware or software for signal and spectrum analyzer - benchtop and handheld models.

FAQ 2019-08-30

What is Keysight's Windows 7 to Windows 10 Migration Schedule?
We are beginning the transition of our Windows based instruments from Windows Embedded Standard 7 to Windows 10 IoT Enterprise. Click on the link for additional information.

FAQ 2019-08-28

M8000 系列軟體 30 天免費試用授權
M8000 產品系列適用的軟體之試用授權頁面與連結。

FAQ 2019-05-21

FlexDCA: What Licenses Do I Have, And What Features Do They Enable?
FlexDCA: What Licenses Do I Have, And What Features Do They Enable?

FAQ 2018-12-10

What Information Should I Collect From FlexDCA Before Asking Keysight For Help?
What Information Should I Collect From FlexDCA Before Asking Keysight For Help?

FAQ 2018-12-10

Does Keysight offer teaching courseware on Industry 4.0 and IoT?
Keysight U380xA IoT Applied Courseware series offers a ready-to-teach package that includes hands-on industry relevant experiences and real-world applications such as Smart Home, Smart City, Smart Automobile and Industry 4.0. Click to find out more.

FAQ 2018-10-25

建議用於 200GAUI-4 和 400GAUI-8 C2M 接收器測試設定的儀器配置
建議用於 200GAUI-4 和 400GAUI-8 C2M 接收器測試設定的儀器配置(配件未列出)

FAQ 2018-10-25

What upgrade options are needed to update my Windows operating system, processor board or solid state drive on my X-Series signal analyzer?
Details about X-Series signal analyzer operation system, processor and solid state drive dependencies

FAQ 2018-08-13

x6000 End of Support
End of Support - x6000 Automated X-Ray Inspection system

FAQ 2018-08-07

How do I remove the root login password on the U3800A Intel Edison?
If the password is misplaced or lost, you will need to reflash Intel Edison firmware. Otherwise, you can remove the password from Edison’s system file.

FAQ 2018-07-25

How do I get replacement parts for individual items in the training kit?
Here are the parts that need to be purchased from Keysight at www.keysight.com/find/parts

FAQ 2018-02-26

IO Libraries Suite: What is the latest version? IO Libraries Suite 2018 Update 0.2
IO Libraries Suite 2018 Update 0.2, available online.

FAQ 2018-01-31

How do I downgrade my Infiniium oscilloscope from Windows 10 to Windows 7?
If you bought an Infiniium oscilloscope running Windows 10 and you want to run Windows 7 instead, this document explains how to do so.

FAQ 2017-12-14

Can the state of channel be stored while it is still being actively monitored?
No. The instrument can store the configuration for all channels only while monitoring is OFF. Only measurement attributes of the currently-selected functions (range, resolution, etc) will be preserved in the stored states. If channel monitoring is ON during store / auto-recall execution, the instrument will not function correctly. To restore the instrument back to its initial working state, all modules slotted into the instrument must be removed and the auto-recall function turned OFF. Please refer to the user manual / service manual regarding the usage of the store/auto-recall function.

FAQ 2017-11-13

Signal Analyzer IVI and MATLAB Instrument Drivers
Supported models: N9000A, N9010A, N9020A, N9030A, N9038A, E4406A, E4440A, E4443A, E4445A, E4446A, E4448A, N8201A, E4447A, E4401B, E4402B, E4403B, E4404B, E4405B, E4407B, E4408B, E4411B, E7401A, E7402A, E7403A, E7404A, E7405A, M9290A, N9040B, N9038A, M9420A, N9000B, N9010B, N9020B, N9030B, N9040B, M9290A, M9420A, M9421A, SPN9026A, SPN9003A, N9041B, M90XA

FAQ 2017-09-21

What are the recommended power supplies used for U9391C/F/G?
Power supply

FAQ 2017-08-07

Is there a 3D model of the InfiniiVision 1000 X-Series oscilloscopes?
Yes, see the IGES, SAP, Step, and PKG format file downloads.

FAQ 2017-07-28

What are the Keysight equivalent model numbers for Centellax BERT products and test accessories?
Click on the question for full details of the equivalent model numbers.

FAQ 2017-07-13

How many carriers can the MXG support in Carrier Aggregation mode?
One MXG can support one instance of the Carrier Aggregation mode. One instance of the Carrier Aggregation mode supports 5 component carriers.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced TDD?
The X-Series upgrade path to LTE-Advanced TDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced FDD?
The X-Series upgrade path to LTE-Advanced FDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

If we use external clocks for both the Pattern Generator and Error Detector parts, can we run them at different data rates?
It would be more straight-forward to provide the PG (TX) with a 10 GHz clock (for 10 Gb/s data) and then use the 1:4 demux and provide the ED (RX) with a 2.5 GHz clock (measuring 2.5 Gb/s data). Click on the question for additional information.

FAQ 2017-06-28

How do I send the UXM Error Logs to Keysight?
You can use the UXM’s Export Logs function to send the UXM platform log files to the Keysight support team. Click on the question for additional information.

FAQ 2017-06-28

How do I display the mixer conversion loss of M1970 Series or M1971 Series Harmonic Mixer on an X-Series Signal Analyzer?
There is no way to display the conversion loss values from these mixers on screen. There is a hard copy of the conversion loss data supplied with each mixer that can be referenced.

FAQ 2017-06-28

What is the raw jitter tolerance for the N4960A/N4952A?
There is no CDR in the N4960A, so by itself, the JTOL plot will be a flat line somewhere below 1 UI. An external CDR can be used. Click on the question for additional information.

FAQ 2017-06-28

1 2 3 4 5 6 7 8 9 10 ... 下一頁