Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

1-25 из 28

Упорядочить:
Four Tips Protect Against Power -Related Damage
High power devices that store energy or contain reactive components are notorious for damaging themselves and the surrounding equipment. Get four tips to help protect your devices and equipment. The first tip provides a way to not only protect against over-power, and not just overvoltage or overcurrent. The second tip helps protect your supply when working with more than one power source. To reduce inrush current, tip 3 provides a method to slow the rate of output voltage change. Lastly, some devices can handle a tremendous surge of current and tip four addresses how to keep the power supply active during a surge.

Электронная книга 2019-11-20

PDF PDF 5.11 MB
Implantable Medical Devices Customer
A Keysight application engineer worked with the design engineering team at an implantable medical device manufacturer to recommend a solution consisting of hardware and software for battery drain analysis. The key solution components are the N6705C DC Power Analyzer, the N6781A 2-quadrant SMU for battery drain analysis and Keysight's 14585A control and analysis software.

Пример реального применения 2019-10-16

PDF PDF 2.79 MB
Keysight Translator for QDART Test
Keysight Translator software for QDART

Статья 2019-09-03

Protecting Government Wireless Systems with Detailed Signal Emulation and Interference Analysis
Agency researchers were asked to investigate signal interference and spectral coexistence related to the performance of government systems in the presence of commercial wireless signals. Much of the work was to be completed in a laboratory setting, and this suggested the use of an advanced solution for signal creation, emulation, measurement and analysis.

Пример реального применения 2018-11-14

PDF PDF 4.48 MB
Water Meter Manufacturer Reduces Development Cycle by Two Months - Case Study
Using the X8712A IoT Device Battery Life Optimization Solution, one large water meter manufacturer in China was able to shave two months off their development and test time, and improved their design, extending battery life to over 10 years. This case study explained how the manufacturer was able to achieve their design excellence.

Пример реального применения 2018-10-17

PDF PDF 3.57 MB
A Leading AR/VR Solution Provider Saves 60% of Time While Optimizing Battery Life
Case study reveals how a leading provider saved 60% of test development and testing time during design validation and significantly improved battery life, solving the issue with the heavy battery pack.

Пример реального применения 2018-09-19

PDF PDF 2.64 MB
4 More Ways to Build Your Power Supply Skill Set: Part 2
Today's designs place higher demands on the systems that power them, and more design problems are being caused by these power systems. This eBook supplements the first set of power skills and provides four additional tips to build your power supply skill set.

Электронная книга 2018-08-28

PDF PDF 2.89 MB
5 Tips for Getting the Most out of Your Function Generator - eBook
Today’s function generators can do much more than their predecessors, but many engineers are not aware of these advanced capabilities. This eBook will introduce you to five advanced waveform capabilities that can help improve testing and save you time in the lab.

Электронная книга 2018-07-18

PDF PDF 6.65 MB
DC-DC Converter Testing - Case Study
Manufacturer of automotive DC-DC converters slashes test time by 95 percent.

Пример реального применения 2018-07-17

PDF PDF 4.49 MB
Automotive & Energy Solutions - eBook
Automotive electronics is the underlying platform for all operations and diagnostics, convenience and comfort, safety and security, and main support for the three areas of innovation: e-mobility, autonomous driving, connected car.

Электронная книга 2018-06-19

PDF PDF 4.31 MB
4 Ways to Build Your Power Supply Skill Set
Get four quick tips to help you get more from your power supply and build your power supply skill set.

Электронная книга 2018-05-03

PDF PDF 2.95 MB
4 Ways to Efficiently Generate Complex Waveforms - ebook
Get four simple tips to help you more efficiently generate complex waveforms.

Электронная книга 2017-09-26

PDF PDF 1.65 MB
HUAWEI demonstrates 112 Gb/s PAM-4 optical signal transmission with M8196A AWG
112 Gb/s PAM-4 Optical Signal Transmission over 100-m OM4 Multimode Fiber for High-Capacity Data-Center

Статья 2016-12-05

Practical, Efficient and Safe Power Device Thermal Characterization with B1506A - Article Reprint
The B1506A has standard solution for power device thermal test and offers fast and safe solution to customers. This white paper reports the actual implementation of thermal test with B1506A.

Статья 2016-03-18

PDF PDF 616 KB
PCI Express Receiver Testing Responds To New Challenges - Article
PCI Express Receiver Testing Responds To New Challenges

Статья 2015-03-24

AWG article - MWJ product feature
AWG article - MWJ product feature

Статья 2014-10-14

2014 Global PXI Instrumentation Growth Excellence Leadership Award - Article Reprint
Frost & Sullivan honors Keysight as a growth leader in the PXI modular instrumentation market in 2014.

Статья 2014-05-22

PDF PDF 598 KB
Enhancing microwave spectroscopy in astrophysics applications – Article
An arbitrary waveform generator is the key element in this faster and more accurate method.

Статья 2013-11-15

A new approach for multi-emitter test signal generation – Article
A new capture and playback approach generates multi-emitter test signals using a combination of COTS test equipment and simulation software.

Статья 2013-11-15

Meeting satellite testing challenges - Article
Satellites are now a critical part of the infrastructure supporting the incredible growth in demand for broadband data.

Статья 2013-11-13

Increasing range of vehicle measurements - Article
From Serial Buses to Powertrains, today’s automobiles present a variety of test-and-measurement challenges.

Статья 2013-11-13

Success Story at a major sewing machine company - Case Study
The case study shows how the B1505A power device analyzer/curve tracer is used to make sure of reliable product development and production at JUKI Corporation

Пример реального применения 2013-09-05

PDF PDF 180 KB
Automating Communications Measurement - Article
This article demonstrates how you can automate measurements, control instruments, develop GUI-based applications, and generate reports for the Keysight 33220A waveform generator using MATLAB software.

Статья 2013-02-07

Using Base Station and MIMO Channel Emulators for Mobile WiMAX Devices
This article describes how a channel emulator can be used to characterize the performance of a MIMO receiver. The testing was done in stages of increasing complexity, namely testing under AWGN conditions, MIMO testing with known static channels, and finally testing with channels chosen to represent “real world” behavior.

Статья 2009-01-11

PDF PDF 1.37 MB
DME uses Keysight N6700 power supplies to help military test radios in the field
Success story tells how defense electronics firm DME Corporation built a test system, known as the Advanced Tactical Agile Communications Test Set, or ATACTS, for testing military radios in the field.

Пример реального применения 2007-03-15

PDF PDF 191 KB

1 2 Следующие